General help: Run the command line executable without arguments to get usage help. ------------- Tips: Check the return status of the program. Return code of 0 is success. Any other return code indicates that programming failed. The program may output error messages before the serial number of the transceiver is displayed. Ignore all errors upto the Serial number if the serial number is printed. Rely on the return code from the program. The printed warnings/errors are intended to help debug and fix the issue that caused the failure. Ignore printed errors if the program returns 0 (success) unless special conditions are to be handled. -------------