General notes ------------------------------------------ 1. Limitations: Recommended display resolution 1920x1080 with maximum 125% scaling. The GUI may not show password fields and buttons may be moved out of the visible area of screen when display scaling is used. 2. Limitations: Disconnect all EV2400 and *unused* EV2300 / MKST-3P-ALT-EV2300 / MKS-SAI-001 from the PC. All connected EV2300 / MKST-3P-ALT-EV2300 / MKS-SAI-001 will need to be used by the tool. bqProduction SBB v1.0.16 ------------------------------- 11/15/2022 Added support for MKST-3P-ALT-EV2300 / MKS-SAI-001 EV2300 may not be supported. Use previous versions for EV2300 support. bqProduction SBB v1.0.15 ------------------------------- 11/13/2017 Add support for bq27z561 with I2C communications Add application lock so only one instance of bqProduction can be running on computer. bqProduction SBB v1.0.14 ------------------------------- 07/06/2017 Reduce memory leak causing Java out of memory failure after 200 runs depending on system memory. It is recommended that bqProduction is closed and reopened on a 4GB RAM system after 1000 runs to free memory. bqProduction SBB v1.0.13 ------------------------------- 02/03/2017 Added SHA1 key programming support for the bq40z50-R2 (bq9000) bqProduction SBB v1.0.12 ------------------------------- 01/26/2017 Added SHA1 key programming support for the bq27750 bqProduction SBB v1.0.9 ------------------------------- 03/29/2016 Added 9E34_0_01-bq4050.bqz bqProduction SBB v1.0.9 ------------------------------- 10/2/2015 Add support for bq78z100 using HPA495A Mtester board over I2C. Configuration screen device configuration is now dependent on bqz Container configuration file. bqProduction SBB v1.0.8 ------------------------------- 12/15/2014 Add support for devices bq34z100G1 using HPA495A and bq40320 bqProduction SBB v1.0.6 ------------------------------- 5/2/2014 VTI Dialog will only allow Station entries for adapters that have connected boards and marked for use. Settling time preferences range is now checked. VTI Update is disabled during testing. Reference Gain now longer accepts 0. Added 100msec delay after I2C VOUT is set to 5 volts before an attempt is made to send commands to the board. Configuration view now takes more space on screen to prevent scrolling on normal screen sizes Reduced min size requirement for configuration view to fit in samller space Created new splash image for bqProduction startup Added bqProduction help plugin Removed data flash srec creation from top menu bqProduction SBB v1.0.5 ------------------------------- 3/31/2014 Add support for bq28z610 version 0.11 Remove menu extracting data flash from device. Use golden srecord generated from Battery Management Studio. Complete srecord or data flash only can now be programmed from a golden image. Fix random "Command Channel not found errors" during testing. Add support for reading bqz targetinfo.xml Add online help system. Fix only last station writing to log file. Allow entry and use of VTI measurements for each individual station. Require VTI measurement entry before executing tester. Use updated station name in entire tool if name is changed. Add new splash screen. Enable voltage and current supplies on each board during VTI entry. bqProduction SBB v1.0.4 ------------------------------- Changes from v1.0.3 Bugfixes : Login options(menu items) should remain same if login attempt fails bqProduction SBB v1.0.3 ------------------------------- Changes from v1.0.1 Added 100 ms delay between retries for serial no, date & manufac info bqProduction SBB v1.0.1 ------------------------------- Changes from v1.0.0 Added EV2300 name support Added authentication screen for VTI update bqProduction SBB Version 1.0.0 ------------------------------- Initial Version Devices Supported : bq40320