|
AM263x MCU+ SDK
11.01.00
|
|
Go to the documentation of this file.
55 #ifndef INCLUDE_SDL_UTILS_H_
56 #define INCLUDE_SDL_UTILS_H_
63 #include <sdl/include/sdl_types.h>
156 typedef struct SDL_MPU_staticReg_read
uint32_t accessPermission
Definition: sdl_r5_utils.h:169
uint32_t CONTEXTIDR
Definition: sdl_r5_utils.h:107
MPU Static Registers structure.
Definition: sdl_r5_utils.h:157
uint32_t SDL_UTILS_getCONTEXTIDR(void)
uint32_t nVALIRQSET
Definition: sdl_r5_utils.h:109
uint32_t PMCR
Definition: sdl_r5_utils.h:137
void SDL_R5MPU_readStaticRegisters(SDL_R5MPU_staticRegs *pMPUStaticRegs, uint32_t regionNum)
MPU API to Read the Static Registers. This function reads the values of the static registers such as ...
uint32_t SDL_UTILS_getPMCR(void)
uint32_t size
Definition: sdl_r5_utils.h:167
uint32_t SDL_UTILS_getnVALIRQSET(void)
uint32_t BTCMRegionR
Definition: sdl_r5_utils.h:101
uint32_t mpuTypeReg
Definition: sdl_r5_utils.h:160
uint32_t SDL_UTILS_getnVALDEBUGCLEAR(void)
uint32_t SDL_UTILS_getPinOptionR(void)
uint32_t nVALDEBUGSET
Definition: sdl_r5_utils.h:115
uint32_t PinOptionR
Definition: sdl_r5_utils.h:129
uint32_t ACTLR
Definition: sdl_r5_utils.h:95
uint32_t SDL_UTILS_getBuildOption1R(void)
uint32_t SDL_UTILS_getSlavePortControlR(void)
uint32_t AHBRR
Definition: sdl_r5_utils.h:135
Structure containing R5F CPU Static Registers.
Definition: sdl_r5_utils.h:92
uint32_t nVALIRQCLEAR
Definition: sdl_r5_utils.h:117
uint32_t nVALRESETSET
Definition: sdl_r5_utils.h:113
uint32_t SDL_UTILS_getnVALRESETSET(void)
uint32_t SDL_UTILS_getADFSR(void)
uint32_t SDL_UTILS_getnVALFIQSET(void)
uint32_t SlavePortControlR
Definition: sdl_r5_utils.h:105
uint32_t SDL_UTILS_getLLPPvirtualAXIRR(void)
void SDL_UTILS_enable_cache_event_bus(void)
uint32_t SDL_UTILS_getnVALFIQCLEAR(void)
uint32_t baseAddr
Definition: sdl_r5_utils.h:165
uint32_t SDL_UTILS_getnVALIRQCLEAR(void)
uint32_t PMCNTENSET
Definition: sdl_r5_utils.h:139
int32_t SDL_CPU_staticRegisterRead(SDL_R5FCPU_StaticRegs *pCPUStaticRegs)
This API is used to get the value of static registers for R5F CPU.
uint32_t SDL_UTILS_getIFAR(void)
uint32_t SDL_UTILS_getBuildOption2R(void)
uint32_t SDL_UTILS_getSCTLR(void)
uint32_t sysControlReg
Definition: sdl_r5_utils.h:158
uint32_t SDL_UTILS_getCFLR(void)
uint32_t ATCMRegionR
Definition: sdl_r5_utils.h:103
uint32_t nVALRESETCLEAR
Definition: sdl_r5_utils.h:121
uint32_t SDL_UTILS_getSecondaryACTLR(void)
uint32_t PMINTENCLR
Definition: sdl_r5_utils.h:145
uint32_t SDL_UTILS_getAIFSR(void)
uint32_t nVALFIQCLEAR
Definition: sdl_r5_utils.h:119
uint32_t SDL_UTILS_getAHBRR(void)
uint32_t SDL_UTILS_getDFAR(void)
uint32_t PMUSERENR
Definition: sdl_r5_utils.h:141
uint32_t SDL_UTILS_getPMINTENCLR(void)
void SDL_UTILS_enable_event_bus(void)
uint32_t SDL_UTILS_getATCMRegionR(void)
uint32_t SDL_UTILS_getIFSR(void)
uint32_t SDL_UTILS_getnVALDEBUGSET(void)
uint32_t SDL_UTILS_getLLPPnormalAXIRR(void)
uint32_t nVALDEBUGCLEAR
Definition: sdl_r5_utils.h:123
uint32_t regionId
Definition: sdl_r5_utils.h:162
uint32_t SDL_UTILS_getPMINTENSET(void)
uint32_t SDL_UTILS_getnVALRESETCLEAR(void)
uint32_t LLPPnormalAXIRR
Definition: sdl_r5_utils.h:131
uint32_t SDL_UTILS_getACTLR(void)
uint32_t SDL_UTILS_getDFSR(void)
uint32_t SDL_UTILS_getPMUSERENR(void)
uint32_t nVALFIQSET
Definition: sdl_r5_utils.h:111
uint32_t SDL_UTILS_getPMOVSR(void)
uint32_t BuildOption2R
Definition: sdl_r5_utils.h:127
uint32_t CPACR
Definition: sdl_r5_utils.h:99
uint32_t SDL_UTILS_getBTCMRegionR(void)
uint32_t SDL_UTILS_getCPACR(void)
uint32_t LLPPvirtualAXIRR
Definition: sdl_r5_utils.h:133
uint32_t BuildOption1R
Definition: sdl_r5_utils.h:125
uint32_t SDL_UTILS_getPMCNTENSET(void)
uint32_t SecondaryACTLR
Definition: sdl_r5_utils.h:97
uint32_t SCTLR
Definition: sdl_r5_utils.h:93
uint32_t PMINTENSET
Definition: sdl_r5_utils.h:143