AM263x MCU+ SDK  11.01.00
Release Notes 10.01.00

Attention
1. Also refer to individual module pages for more details on each feature, unsupported features, important usage guidelines.
2. Multi Core ELF image format support has been added (Understanding Multicore ELF image format). RPRC format will be deprecated from SDK 11.0.
3. Test report is not uploaded in SDK due to an issue with the report generation tool.
Note
The examples will show usage of SW modules and APIs on a specific CPU instance and OS combination.
Unless explicitly noted otherwise, the SW modules would work in both FreeRTOS and no-RTOS environment.
Unless explicitly noted otherwise, the SW modules would work on any of the R5F's present on the SOC.

New in this Release

Feature Module
SBL over Ethernet Bootloader
Pinmux CSV Generation support in SysCfg Pinmux
FreeRTOS FAT Example support FreeRTOS
FSI LLD Support FSI
FreeRTOS Kernel migrated to 11.1.0 LTS FreeRTOS

Device and Validation Information

SOC Supported CPUs EVM Host PC
AM263x R5F AM263x ControlCard Revision E2 (referred to as am263x-cc in code).
Windows 10 64b or Ubuntu 18.04 64b
AM263x R5F AM263x LaunchPad Revision E2 (referred to as am263x-lp in code) Windows 10 64b or Ubuntu 18.04 64b

Dependent Tools and Compiler Information

Tools Supported CPUs Version
Code Composer Studio R5F 12.8.1
SysConfig R5F 1.21.2 build, build 3837
TI ARM CLANG R5F 4.0.1.LTS
FreeRTOS Kernel R5F 11.1.0
LwIP R5F STABLE-2_2_0_RELEASE
Mbed-TLS R5F 2.13.1

Key Features

Experimental Features

Attention
Features listed below are early versions and should be considered as "experimental".
Users can evaluate the feature, however the feature is not fully tested at TI side.
TI would not support these feature on public e2e.
Experimental features will be enabled with limited examples and SW modules.
Feature Module
Ether-ring Implementation Networking

OS Kernel

OS Supported CPUs SysConfig Support Key features tested Key features not tested / NOT supported
FreeRTOS Kernel R5F NA Task, Task notification, interrupts, semaphores, mutexs, timers Task load measurement using FreeRTOS run time statistics APIs. Limited support for ROV features.
FreeRTOS POSIX R5F NA pthread, mqueue, semaphore, clock -
NO RTOS R5F NA See Driver Porting Layer (DPL) below -

Driver Porting Layer (DPL)

Module Supported CPUs SysConfig Support OS support Key features tested Key features not tested / NOT supported
Cache R5F YES FreeRTOS, NORTOS Cache write back, invalidate, enable/disable -
Clock R5F YES FreeRTOS, NORTOS Tick timer at user specified resolution, timeouts and delays -
CpuId R5F NA FreeRTOS, NORTOS Verify Core ID and Cluster ID that application is currently running on -
CycleCounter R5F NA FreeRTOS, NORTOS Measure CPU cycles using CPU specific internal counters -
Debug R5F YES FreeRTOS, NORTOS Logging and assert to any combo of: UART, CCS, shared memory -
Heap R5F NA FreeRTOS, NORTOS Create arbitrary heaps in user defined memory segments -
Hwi R5F YES FreeRTOS, NORTOS Interrupt register, enable/disable/restore, Interrupt prioritization -
MPU R5F YES FreeRTOS, NORTOS Setup MPU and control access to address space -
Semaphore R5F NA FreeRTOS, NORTOS Binary, Counting Semaphore, recursive mutexs with timeout -
Task R5F NA FreeRTOS Create, delete tasks -
Timer R5F YES FreeRTOS, NORTOS Configure arbitrary timers -

Secondary Bootloader (SBL)

Module Supported CPUs SysConfig Support OS support Key features tested Key features not tested / NOT supported
Bootloader R5FSS0-0 YES NORTOS Boot modes: QSPI, UART. All R5F's. RPRC, MCELF, multi-core image format Force Dual Core Mode, Disable Dual Core Switch and R5SS1 only not tested

SOC Device Drivers

Peripheral Supported CPUs SysConfig Support DMA Supported Key features tested Key features not tested / NOT supported
ADC R5F YES Yes. Example: adc_soc_continuous_dma Single software triggered conversion, Multiple ADC trigger using PWM, Result read using DMA, EPWM trip through PPB limit, PPB features, Burst mode, Single and Differential mode, Interrupt with Offset from Aquisition Window, EPWM/ECAP/RTI triggered conversions -
Bootloader R5F YES Yes. DMA enabled for SBL QSPI Boot modes: QSPI, UART. All R5F's -
CMPSS R5F YES NA Asynchronous PWM trip, Digital Filter, Calibration, -
CPSW R5F YES No MAC loopback, PHY loopback, LWIP: Getting IP, Ping, Iperf, Layer 2 MAC, Layer 2 PTP Timestamping and Ethernet CPSW Switch support, TSN stack RMII, MII mode
DAC R5F YES Yes. Example: dac_sine_dma Constant voltage, Square wave generation, Sine wave generation with and without DMA, Ramp wave generation, Random Voltage generation -
ECAP R5F YES yes. Example : ecap_edma ECAP APWM mode, PWM capture, DMA trigger in both APWM and Capture Modes -
EDMA R5F YES NA DMA transfer using interrupt and polling mode, QDMA Transfer, Channel Chaining, PaRAM Linking -
EPWM R5F YES Yes. Example: epwm_dma PWM outputs A and B in up-down count mode, Trip zone, Update PWM using EDMA, Valley switching, High resolution time period adjustment, type5 feature -
EQEP R5F YES NA Speed and Position measurement. Frequency Measurement, Speed and Direction Measurement, cw-ccw modes -
FSI R5F YES Yes. Example: fsi_loopback_dma RX, TX, polling, interrupt mode, Dma, single lane loopback. - FSI Spi Mode
GPIO R5F YES NA Output, Input and Interrupt functionality -
I2C R5F YES No Controller mode, basic read/write -
IPC Notify R5F YES NA Mailbox functionality, IPC between RTOS/NORTOS CPUs M4F core
IPC Rpmsg R5F YES NA RPMessage protocol based IPC M4F core
LIN R5F YES YES RX, TX, polling, interrupt, DMA mode. -
MCAN R5F YES No RX, TX, interrupt and polling mode, Corrupt Message Transmission Prevention, Error Passive state, Bus Off State, Bus Monitoring Mode -
MCSPI R5F YES Yes. Example: mcspi_loopback_dma Controller/Peripheral mode, basic read/write, polling, interrupt and DMA mode -
MDIO R5F YES NA Register read/write, link status and link interrupt enable API -
MPU Firewall R5F YES NA Only compiled (Works only on HS-SE device) -
MMCSD R5F YES NA MMCSD 4bit, Raw read/write - file IO, eMMC

PINMUX | R5F | YES | NA | Tested with multiple peripheral pinmuxes PMU | R5F | NO | NA | Tested various PMU events | Counter overflow detection is not enabled | - PRUICSS | R5F | YES | NA | Tested with Ethercat FW HAL | - QSPI | R5F | YES | Yes. Example: qspi_flash_dma_transfer | Read direct, Write indirect, Read/Write commands, DMA for read | - RTI | R5F | YES | No | Counter read, timebase selction, comparator setup for Interrupt, DMA requests | Capture feature, fast enabling/disabling of events not tested SDFM | R5F | YES | Yes. Example: sdfm_filter_sync_dmaread| Filter data read from CPU, Filter data read with PWM sync | - SOC | R5F | YES | NA | Lock/unlock MMRs, clock enable, set Hz, Xbar configuration, SW Warm Reset, Address Translation | - SPINLOCK | R5F | NA | NA | Lock, unlock HW spinlocks | - UART | R5F | YES | Yes. Example: uart_echo_dma | Basic read/write at baud rate 115200, polling, interrupt mode | HW flow control not tested, DMA mode not supported WATCHDOG | R5F | YES | NA | Reset mode, Interrupt mode | -

Board Device Drivers

Peripheral Supported CPUs SysConfig Support Key features tested Key features not tested
EEPROM R5F YES Only compiled -
ETHPHY R5F YES Tested with ethercat_slave_beckhoff_ssc_demo example -
FLASH R5F YES QSPI Flash -
LED R5F YES GPIO -

CMSIS

Module Supported CPUs SysConfig Support OS Support Key features tested Key features not tested
- - - - - -

Ethernet and Networking

Module Supported CPUs SysConfig Support OS Support Key features tested Key features not tested
Time-Sensitive Networking(gPTP-IEEE 802.1AS) R5F NO FreeRTOS gPTP IEEE 802.1 AS-2020 compliant gPTP stack, End Nodes and Bridge mode support, YANG data model configuration Multi-Clock Domain
LwIP R5F YES FreeRTOS TCP/UDP IP networking stack with and without checksum offload enabled, TCP/UDP IP networking stack with server and client functionality, basic Socket APIs, netconn APIs and raw APIs, DHCP, ping, TCP iperf, scatter-gather, DSCP priority mapping Other LwIP features
Ethernet driver (ENET) R5F YES FreeRTOS Ethernet as port using CPSW, MAC loopback and PHY loopback, Layer 2 MAC, Packet Timestamping, CPSW Switch, CPSW EST, interrupt pacing, Policer and Classifier, MDIO Manual Mode, Credit Based Shaper (IEEE 802.1Qav), Strapped PHY (Early Ethernet) RMII, MII mode
ICSS-EMAC R5F YES FreeRTOS Switch and MAC features, Storm Prevention (MAC), Host Statistics, Multicast Filtering Promiscuous Mode
Mbed-TLS R5F NO FreeRTOS Tested software cryptography after porting, used mbedTLS with LwIP to implement HTTPS server Hardware offloaded cryptography
Ether-ring Implementation R5F NO FreeRTOS EDuplicate Rejection, Ring termination and Packet Duplication Latency measurement, Performance KPIs

Demos

Module Supported CPUs SysConfig Support OS Support Key features tested Key features not tested
- - - - - -

Safety Diagnostic Library

Module Supported CPUs SysConfig Support OS support Key features tested Key features not tested / NOT supported
MCRC R5F NA NORTOS Full CPU, Auto CPU Mode and Semi CPU Auto Mode -
DCC R5F NA NORTOS Single Shot and Continuous modes -
PBIST R5F NA NORTOS Memories supported by MSS PBIST controller. -
ESM R5F NA NORTOS Tested in combination with RTI, DCC -
RTI R5F NA NORTOS WINDOWSIZE_100_PERCENT, WINDOWSIZE_50_PERCENT ,Latency/Propagation timing error(early)(50% window),Latency/Propagation timing error(late)(50% window) -
ECC R5F NA NORTOS ECC of MSS_L2, R5F TCM, MCAN, VIM, ICSSM, TPTC R5F data Cache(DED)
ECC Bus Safety R5F NA NORTOS AHB, AXI, TPTC -
CCM R5F NA NORTOS CCM Self Test Mode,Error Forcing Mode and Self Test Error Forcing Mode. -
R5F STC(LBIST), Static Register Read R5F NA NORTOS STC of R5F, R5F CPU Static Register Read -
Integrated Example R5F NA FreeRTOS Integrated example with all the SDL modules integrated in to one example. ECC Bu Safety and STC.

Fixed Issues

ID Head Line Module Applicable Releases Applicable Devices Resolution/Comments
PROC_SDL-7615 ECC example fails for SEC and DED for TPTC memories. SDL 09.00.00 Onwards AM263x, AM263Px Fixed the example.
PROC_SDL-8393 In ECC bus safety, error injection test writes to address 0x0. SDL 09.01.00 Onwards AM263x, AM263Px Fixed the source code and example.
PROC_SDL-8518 Integrated example should have checked ECC for TPTC, ATCM, BTCM memories. SDL 10.00.00 onwards AM263x None.
PROC_SDL-8393 In ECC bus safety, error injection test writes to address 0x0. SDL 08.06.00 onwards AM263x, AM263Px None
MCUSDK-13821 ADC reference monitor instance doesn't match the reference buffer instance ADC 10.00.00 AM263x, AM263Px Update the monitor instances.
MCUSDK-12262 EPWM deadband example failure EPWM 09.02.00 AM263x, AM263Px removed sync between the epwms and used the global tbclksync to synchronize the EPWMs
MCUSDK-13164 AM26x: EPWM DeadBand example failure EPWM 10.00.00 onwards phase shift adds a tbclk delay. added another EPWM instance to sync.
MCUSDK-13634 EPWM: Remove eventsUsed from Action Qualifier Syscfg. EPWM 10.00.00 onwards removed unused eventUsed element from the examples syscfg
MCUSDK-13670 SDFM ECAP loopback example used explicit HW_REG_RD SDFM 10.00.00 onwards updated the register read with corresponding API.
MCUSDK-13641, CODEGEN-12832 Increased build time for examples using Link Time Optimization (-flto) with TI-ARM-CLANG 4.0.0 LTS Build 10.00.00 onwards Issue fixed in latest 4.0.1 LTS compiler release.
MCUSDK-13647 Unable to select 3pin/4pin mode when McSPI is configured as Single Peripheral McSPI 10.00.00 onwards Issue fixed in latest 4.0.1 LTS compiler release.
MCUSDK-13145 UART: Incorrect API used to catch UART TX DMA Event miss McSPI 10.00.00 onwards Update driver with correct API.

Known Issues

ID Head Line Module Reported in release Workaround
MCUSDK-13865 HRPWM Deadband sfo example has 1ns jitter EPWM 10.00.00 onwards -
MCUSDK-13201 HRPWM waveform not generating (in updwon count) when prescaler is non-zero and HRPE is enabled EPWM 10.00.01 onwards None
MCUSDK-13834 EQEP: EQEP frequency measurement example is not working as expected EQEP 10.00.01 onwards None
MCUSDK-14051 EQEP : CW CCW example doesn't use polling or interrupt EQEP 10.00.01 None
MCUSDK-13702 am263x-lp: sbl sd not working for multicore appimages MMCSD, SBL 10.00.00 -
MCUSDK-13164 AM263x: EPWM deadband example failure EPWM 09.02.00 remove sync between the epwms and use the global tbclksync to synchronize the EPWMs
MCUSDK-7319 CONTROLSS-SDFM: Two Back-to-Back Writes to SDCPARMx Register Bit Fields CEVT1SEL, CEVT2SEL, and HZEN Within Three SD-Modulator Clock Cycles can Corrupt SDFM State Machine, Resulting in Spurious Comparator Events SDFM 08.04.00 onwards Avoid back-to-back writes within three SD-modulator clock cycles or have the SDCPARMx register bit fields configured in one register write.
MCUSDK-9082 MbedTLS - RSA exploit by kernel-privileged cache side-channel attackers Mbed-TLS 08.06.00 onwards -
MCUSDK-11730 A wrong counter is used for Event 2 in PMU configuration PMU 09.00.00 onwards -
MCUSDK-13111 Memory Configurator/syscfg auto-linker generator doesn't support reordering Build 09.01.00 onwards -
MCUSDK-13109 RTI Interrupt req is pulse type and not level type RTI 09.01.00 onwards -
MCUSDK-13014 The memory read feature of uniflash erases the memory Flash 09.01.00 onwards -
MCUSDK-13011 Multicore Empty project not working properly FreeRTOS 09.01.00 onwards -
MCUSDK-12986 FreeRTOS: Barrier instructions missing in Interrupt Disable/Enable API's FreeRTOS 09.01.00 onwards -
PINDSW-7715 Dual EMAC instance not working with both ports together for icss_emac_lwip example ICSS-EMAC 09.02.00 onwards None
PINDSW-7746 icss_emac_lwip example having low iperf values in TCP and UDP ICSS-EMAC 09.02.00 onwards None
PINDSW-8118 Enabling DHCP mode in icss_emac_lwip example causes assert ICSS-EMAC 09.02.00 onwards None
MCUSDK-12756 MbedTLS - Timing side channel attack in RSA private operation exposing plaintext. Mbed-TLS 08.06.00 onwards None
MCUSDK-13164 AM263x: epwm deadband example validation failure EPWM 09.01.00 onwards The Waveform of the EPWM is correct and is as expected.
MCUSDK-13202 Frame drops are seen in PRU GPIO based SENT decoder example while sending frames in burst format PRU-IO 09.00.00 onwards None
PROC_SDL-8392 In ECC bus safety example, ECC error is not properly cleared at the source. SDL 08.06.00 onwards None
PROC_SDL-8519 In ECC for R5F data cache only, double bit test is not supported. SDL 10.00.00 onwards ECC test for single bit injection on R5F data cache, release profile binary is showing some inconsistency on result.
PROC_SDL-8857 SDL integrated example does not support ECC Bus Safety. SDL 10.01.00 onwards Use standalone example.
PROC_SDL-8864 D-tag and D-data ECC examples fail in release profile. SDL 10.00.00 onwards None.
MCUSDK-13466 UART Transfer fails in 10MHz Auto Baud mode UART 10.00.00 onwards Use different mode for 10MHz clock
MCUSDK-13193 SBL SD transfer time increased w.r.t SDK 9.2 SBL 10.00.00 onwards None.
MCUSDK-13511 MPU region count incorrect in SysCfg MPU Firewall 09.02.00 onwards None.
MCUSDK-13473 UART uniflash script fails with large images ( > 1MB) SBL 10.00.00 onwards Use JTAG based flashing
MCUSDK-11730 A wrong counter is used for Event 2 in PMU configuration PMU 10.00.00 onwards Comment out the code in PMU_init() whcih configures Cycle Counter.
MCUSDK-13630 Cache should not be enabled at L2 Bank boundaries Cache Cache should not be enabled at last 32Bytes of L2 Bank Create MPU configurations for end of each L2 Bank with Non Cached attribute
MCUSDK-13165 SBL QSPI flow has incorrect addressing for Secure Boot flow SBL, QSPI SBL QSPI flow has incorrect addressing for Secure Boot flow since it expects MEMMAP configuration Use MCELF Image format
MCUSDK-13652 Readelf throws warning while parsing RS note SBL, QSPI Readelf command throws error when trying to read the RS note segment from an mcelf file. -
MCUSDK-14110 Error building examples in CCS in mac Infra Example build fails in CCS only in MAC Machines Use makefile based build

Errata

ID Head Line Module SDK Status
i2311 USART: Spurious DMA Interrupts UART Implemented
i2313 GPMC: Sub-32-bit read issue with NAND and FPGA/FIFO GPMC Not supported in SDK
i2324 No synchronizer present between GCM and GCD status signals Common Implemented
i2345 CPSW: Ethernet Packet corruption occurs if CPDMA fetches a packet which spans across memory banks CPSW Implemented
i2350 McSPI data transfer using EDMA in 'ABSYNC' mode stops after 32 bits transfer McSPI Implemented
i2354 SDFM: Two Back-to-Back Writes to SDCPARMx Register Bit Fields CEVT1SEL, CEVT2SEL, and HZEN Within Three SD-Modulator Clock Cycles can Corrupt SDFM State Machine, Resulting in Spurious Comparator Events SDFM Open
i2355 ADC: DMA Read of Stale Result ADC Implemented
i2356 ADC: Interrupts may Stop if INTxCONT (Continue-to-Interrupt Mode) is not Set ADC Implemented
i2375 SDFM module event flags (SDIFLG.FLTx_FLG_CEVTx) do not get set again if the comparator event is still active and digital filter path (using SDCOMPxCTL.CEVTxDIGFILTSEL) is being selected SDFM Open
i2392 Race condition in capture registers resulting in events miss Common Open
i2394 Race condition in interrupt and error aggregator capture registers resulting in events miss Common Open
i2401 CPSW: Host Timestamps Cause CPSW Port to Lock up CPSW Open
i2402 CPSW: Ethernet to Host Checksum Offload does not work CPSW Open
i2404 Race condition in mailbox registers resulting in events miss IPC Implemented
i2405 CONTROLSS: Race condition OUTPUT_XBAR and PWM_XBAR resulting in event miss XBAR Open

Limitations

ID Head Line Module Reported in release Workaround
MCUSDK-9471 Ethernet CPSW CPDMA stuck with SOF overrun when TCP/DUP checksum offload is enabled. Ethernet CPSW 08.05.00 onwards Disable TCPUDP checksum offload in receive (THOST) direction.
MCUSDK-13630 Cache should not be enabled at L2 Bank boundaries Cache 09.02.00 onwards Create MPU configurations for end of each L2 Bank with Non Cached attribute
MCUSDK-13220 Multi Core Elf format has few limitations documented at Understanding Multicore ELF image format Infra 10.00.00 onwards -

Upgrade and Compatibility Information

Compiler Options

Module Affected API Change Additional Remarks

SOC Device Drivers

Module Affected API Change Additional Remarks

Ethernet and Networking

Module Affected API Change Additional Remarks
Networking Networking examples and syscfg Moved the examples from mcu_plus_sdk/examples/networking to mcu_plus_sdk/source/networking/enet/core/examples -