AM263x MCU+ SDK  11.01.00
Release Notes 09.01.00

Attention
Also refer to individual module pages for more details on each feature, unsupported features, important usage guidelines.
Note
The examples will show usage of SW modules and APIs on a specific CPU instance and OS combination.
Unless explicitly noted otherwise, the SW modules would work in both FreeRTOS and no-RTOS environment.
Unless explicitly noted otherwise, the SW modules would work on any of the R5F's present on the SOC.
Attention
Klockwork Static Analysis report is not updated for this release

New in this Release

Feature Module
Memory Configurator (SysConfig based Linker generation) (Memory Configurator) Common
Coremark and Dhrystone benchmark (Coremark Benchmark, Dhrystone Benchmark) Common
GPMC PSRAM support (without DMA) (GPMC) GPMC
McSPI LLD driver support (MCSPI Low Level Driver) McSPI
UART LLD driver support (UART Low Level Driver) UART
HW Spinlock example (Spinlock Example) Spinlock
SafeIPC support (IPC SafeIPC Echo) IPC
ECAP-ADC & ECAP-EDMA example (ADC SOC ECAP) (ECAP EDMA Example) ECAP
EPWM Synchronization example (EPWM Synchronization) EPWM
Uniflash tool support (TI Uniflash Tool) Uniflash
LwIP stack is upgraded to 2.2.0 version Ethernet and Networking
YANG data model based configuration support for IET/Frame Preemption(IEEE 802.1Qbu), Credit Based Shaper(IEEE 802.1Qav), Enhancements for Scheduled Traffic(IEEE 802.1Qbv) and other TSN features Ethernet and Networking
Ethernet Switch management through standard Link Layer Discovery Protocol(IEEE 802.1AB) for CPSW peripheral Ethernet and Networking
Multi-time domain gPTP(IEEE 802.1AS) support enabled in TSN stack Ethernet and Networking
Example to showcase the simultaneous execution of Time-Sensitive Networking and LwIP stack Ethernet and Networking
Syscfg and documentation update for static IP configuration, custom MAC address and other ethernet related configurations Ethernet and Networking

Device and Validation Information

SOC Supported CPUs EVM Host PC
AM263x R5F AM263x ControlCard Revision E2 (referred to as am263x-cc in code).
Windows 10 64b or Ubuntu 18.04 64b
AM263x R5F AM263x LaunchPad Revision E2 (referred to as am263x-lp in code) Windows 10 64b or Ubuntu 18.04 64b

Dependent Tools and Compiler Information

Tools Supported CPUs Version
Code Composer Studio R5F 12.5.0
SysConfig R5F 1.18.0 build, build 3266
TI ARM CLANG R5F 3.2.0.LTS
FreeRTOS Kernel R5F 10.4.3
LwIP R5F STABLE-2_2_0_RELEASE
Mbed-TLS R5F mbedtls-2.13.1

Key Features

Experimental Features

Attention
Features listed below are early versions and should be considered as "experimental".
Users can evaluate the feature, however the feature is not fully tested at TI side.
TI would not support these feature on public e2e.
Experimental features will be enabled with limited examples and SW modules.
Feature Module
SENT Encoder Example PRU_IO
SENT Decoder Example PRU_IO
Empty PRU firmware Example PRU_IO
GUI for UART Uniflash Tool Bootloader
GUI for UART Uniflash Tool Bootloader

OS Kernel

OS Supported CPUs SysConfig Support Key features tested Key features not tested / NOT supported
FreeRTOS Kernel R5F NA Task, Task notification, interrupts, semaphores, mutexs, timers Task load measurement using FreeRTOS run time statistics APIs. Limited support for ROV features.
FreeRTOS POSIX R5F NA pthread, mqueue, semaphore, clock -
NO RTOS R5F NA See Driver Porting Layer (DPL) below -

Driver Porting Layer (DPL)

Module Supported CPUs SysConfig Support OS support Key features tested Key features not tested / NOT supported
Cache R5F YES FreeRTOS, NORTOS Cache write back, invalidate, enable/disable -
Clock R5F YES FreeRTOS, NORTOS Tick timer at user specified resolution, timeouts and delays -
CpuId R5F NA FreeRTOS, NORTOS Verify Core ID and Cluster ID that application is currently running on -
CycleCounter R5F NA FreeRTOS, NORTOS Measure CPU cycles using CPU specific internal counters -
Debug R5F YES FreeRTOS, NORTOS Logging and assert to any combo of: UART, CCS, shared memory -
Heap R5F NA FreeRTOS, NORTOS Create arbitrary heaps in user defined memory segments -
Hwi R5F YES FreeRTOS, NORTOS Interrupt register, enable/disable/restore, Interrupt prioritization -
MPU R5F YES FreeRTOS, NORTOS Setup MPU and control access to address space -
Semaphore R5F NA FreeRTOS, NORTOS Binary, Counting Semaphore, recursive mutexs with timeout -
Task R5F NA FreeRTOS Create, delete tasks -
Timer R5F YES FreeRTOS, NORTOS Configure arbitrary timers -

Secondary Bootloader (SBL)

Module Supported CPUs SysConfig Support OS support Key features tested Key features not tested / NOT supported
Bootloader R5FSS0-0 YES NORTOS Boot modes: QSPI, UART. All R5F's. RPRC, multi-core image format Force Dual Core Mode, Disable Dual Core Switch and R5SS1 only not tested

SOC Device Drivers

Peripheral Supported CPUs SysConfig Support DMA Supported Key features tested Key features not tested / NOT supported
ADC R5F YES Yes. Example: adc_soc_continuous_dma Single software triggered conversion, Multiple ADC trigger using PWM, Result read using DMA, EPWM trip through PPB limit, PPB limits, PPB offsets, burst mode oversampling, differential mode, Offset, EPWM triggered conversion -
Bootloader R5F YES Yes. DMA enabled for SBL QSPI Boot modes: QSPI, UART. All R5F's -
CMPSS R5F YES NA Asynchronous PWM trip -
CPSW R5F YES No MAC loopback, PHY loopback, LWIP: Getting IP, Ping, Iperf, Layer 2 MAC, Layer 2 PTP Timestamping and Ethernet CPSW Switch support, TSN stack RMII, MII mode
DAC R5F YES Yes. Example: dac_sine_dma Constant voltage, Square wave generation, Sine wave generation with and without DMA, Ramp wave generation, Random Voltage generation -
ECAP R5F YES No ECAP APWM mode, PWM capture -
EDMA R5F YES NA DMA transfer using interrupt and polling mode, QDMA Transfer, Channel Chaining, PaRAM Linking -
EPWM R5F YES Yes. Example: epwm_dma PWM outputs A and B in up-down count mode, Trip zone, Update PWM using EDMA, Valley switching, High resolution time period adjustment, type5 feature -
EQEP R5F YES NA Speed and Position measurement. Frequency Measurement -
FSI R5F YES Yes. Example: fsi_loopback_dma RX, TX, polling, interrupt mode, Dma, single lane loopback. - FSI Spi Mode
GPIO R5F YES NA Output, Input and Interrupt functionality -
I2C R5F YES No Controller mode, basic read/write -
IPC Notify R5F YES NA Mailbox functionality, IPC between RTOS/NORTOS CPUs M4F core
IPC Rpmsg R5F YES NA RPMessage protocol based IPC M4F core
MCAN R5F YES No RX, TX, interrupt and polling mode, Corrupt Message Transmission Prevention, Error Passive state, Bus Off State, Bus Monitoring Mode -
MCSPI R5F YES Yes. Example: mcspi_loopback_dma Controller/Peripheral mode, basic read/write, polling, interrupt and DMA mode -
MDIO R5F YES NA Register read/write, link status and link interrupt enable API -
MPU Firewall R5F YES NA Only compiled (Works only on HS-SE device) -
MMCSD R5F YES NA MMCSD 4bit, Raw read/write - file IO, eMMC

PINMUX | R5F | YES | NA | Tested with multiple peripheral pinmuxes PMU | R5F | NO | NA | Tested various PMU events | Counter overflow detection is not enabled | - PRUICSS | R5F | YES | NA | Tested with Ethercat FW HAL | - QSPI | R5F | YES | Yes. Example: qspi_flash_dma_transfer | Read direct, Write indirect, Read/Write commands, DMA for read | - RTI | R5F | YES | No | Counter read, timebase selction, comparator setup for Interrupt, DMA requests | Capture feature, fast enabling/disabling of events not tested SDFM | R5F | YES | No | Filter data read from CPU, Filter data read with PWM sync | - SOC | R5F | YES | NA | Lock/unlock MMRs, clock enable, set Hz, Xbar configuration, SW Warm Reset, Address Translation | - SPINLOCK | R5F | NA | NA | Lock, unlock HW spinlocks | - UART | R5F | YES | Yes. Example: uart_echo_dma | Basic read/write at baud rate 115200, polling, interrupt mode | HW flow control not tested, DMA mode not supported WATCHDOG | R5F | YES | NA | Reset mode, Interrupt mode | -

Board Device Drivers

Peripheral Supported CPUs SysConfig Support Key features tested Key features not tested
EEPROM R5F YES Only compiled -
ETHPHY R5F YES Tested with ethercat_slave_beckhoff_ssc_demo example -
FLASH R5F YES QSPI Flash -
LED R5F YES GPIO -

CMSIS

Module Supported CPUs SysConfig Support OS Support Key features tested Key features not tested
- - - - - -

Industrial Communications Toolkit

Module Supported CPUs SysConfig Support OS Support Key features tested Key features not tested
EtherCAT SubDevice FWHAL R5F NO FreeRTOS Tested with ethercat_slave_beckhoff_ssc_demo example Reset isolation

Motor Control

Module Supported CPUs SysConfig Support OS Support Key features tested Key features not tested
- - - - - -

Ethernet and Networking

Module Supported CPUs SysConfig Support OS Support Key features tested Key features not tested
Time-Sensitive Networking(gPTP-IEEE 802.1AS) R5F NO FreeRTOS gPTP IEEE 802.1 AS-2020 compliant gPTP stack, End Nodes and Bridge mode support, YANG data model configuration Multi-Clock Domain
LwIP R5F YES FreeRTOS TCP/UDP IP networking stack with and without checksum offload enabled, TCP/UDP IP networking stack with server and client functionality, basic Socket APIs, netconn APIs and raw APIs, DHCP, ping, TCP iperf, scatter-gather, DSCP priority mapping Other LwIP features
Ethernet driver (ENET) R5F YES FreeRTOS Ethernet as port using CPSW, MAC loopback and PHY loopback, Layer 2 MAC, Packet Timestamping, CPSW Switch, CPSW EST, interrupt pacing, Policer and Classifier, MDIO Manual Mode, Credit Based Shaper (IEEE 802.1Qav), Strapped PHY (Early Ethernet) RMII, MII mode
ICSS-EMAC R5F YES FreeRTOS Only compiled Not tested
Mbed-TLS R5F NO FreeRTOS Tested software cryptography after porting, used mbedTLS with LwIP to implement HTTPS server Hardware offloaded cryptography

Demos

Module Supported CPUs SysConfig Support OS Support Key features tested Key features not tested
- - - - - -

Safety Diagnostic Library

Module Supported CPUs SysConfig Support OS support Key features tested Key features not tested / NOT supported
MCRC R5F NA NORTOS Full CPU, Auto CPU Mode and Semi CPU Auto Mode -
DCC R5F NA NORTOS Single Shot and Continuous modes -
PBIST R5F NA NORTOS Memories supported by MSS PBIST controller. -
ESM R5F NA NORTOS Tested in combination with RTI, DCC -
RTI R5F NA NORTOS WINDOWSIZE_100_PERCENT, WINDOWSIZE_50_PERCENT ,Latency/Propagation timing error(early)(50% window),Latency/Propagation timing error(late)(50% window) -
ECC R5F NA NORTOS ECC of MSS_L2, R5F TCM, MCAN, VIM, ICSSM, TPTC R5F Cache
ECC Bus Safety R5F NA NORTOS AHB, AXI, TPTC -
CCM R5F NA NORTOS CCM Self Test Mode,Error Forcing Mode and Self Test Error Forcing Mode. -
R5F STC(LBIST), Static Register Read R5F NA NORTOS STC of R5F, R5F CPU Static Register Read -

Fixed Issues

ID Head Line Module Applicable Releases Resolution/Comments
MCUSDK-9309 IPC: Issue when Combination of Notify and RPMsg is enabled in SysCfg. IPC 8.01.00 onwards Use Only Notify or Only Notify+RPMsg on all cores.
MCUSDK-12153 Syscfg Code Duplication in EPWM XCMP configs EPWM 09.00.00 -
MCUSDK-11836 LIN_sendWakeupSignal is not functional as expected LIN 09.00.00 -
MCUSDK-11828 lin_external example does not work if default configuration is disabled LIN 09.00.00 Fix enableParity variable in syscfg template, disable Loopbacks/interrupt if loopback/interrupt is not enabled
MCUSDK-11725 Data Abort on ECAP_getModuloCounterStatus() API ECAP 08.06.00 onwards Unaligned access. Usage of 32 bit read macro to read a 16 bit address location
MCUSDK-11385 RP message send hang issue in case of timeout IPC 08.06.00 onwards RPMsg send invoked IPC Notify send without timeout management

Known Issues

ID Head Line Module Reported in release Workaround
MCUSDK-7319 CONTROLSS-SDFM: Two Back-to-Back Writes to SDCPARMx Register Bit Fields CEVT1SEL, CEVT2SEL, and HZEN Within Three SD-Modulator Clock Cycles can Corrupt SDFM State Machine, Resulting in Spurious Comparator Events SDFM 08.04.00 onwards Avoid back-to-back writes within three SD-modulator clock cycles or have the SDCPARMx register bit fields configured in one register write.
MCUSDK-8073 UART1 not working as expected while configuring two uarts i.e UART0 and UART1 for two different cores UART 08.04.00 onwards UART1 configuration from other core should be done after UART0 is configured and initialized
MCUSDK-9082 MbedTLS - RSA exploit by kernel-privileged cache side-channel attackers Mbed-TLS 08.06.00 onwards -
MCUSDK-9459 UART LLD EDMA Mode not generating interrupt with TX and RX trigger levels greater than 1 UART 09.01.00 onwards -
MCUSDK-10005 UART LLD Write incompatible with data length 5 and 6 UART 09.01.00 onwards Use other data length
MCUSDK-11247 Delay missing after setting FIFO CLEAR bit UART 08.06.00 onwards -
MCUSDK-11462 EPWM: Illegal Combo Logic example fails EPWM 09.00.00 onwards -
MCUSDK-11526 UART LLD does not output readable characters with 16x AUTO BAUD operation mode UART 09.01.00 onwards -
MCUSDK-10626 FSI DMA loopback example TX and RX mismatching on 2nd run FSI 08.06.00 onwards Reset board between 2 runs
MCUSDK-11730 A wrong counter is used for Event 2 in PMU configuration PMU 09.00.00 onwards -
PROC_SDL-5616 ECC Bus Safety SEC and DED Error Injection fails for CPSW. SDL 8.6.0 onwards None.
PROC_SDL-5617 ECC Bus Safety SEC and DED Error Injection fails for MSS_L2. SDL 8.6.0 onwards None.
PROC_SDL-4749 ECC Bus Safety DED Error Injection fails for AXI. SDL 8.5.0 onwards None.
PROC_SDL-5979 R5F Cache ECC diagnostics are not supported. SDL 8.5.0 onwards None.

Errata

ID Head Line Module SDK Status
i2311 USART: Spurious DMA Interrupts UART Implemented
i2313 GPMC: Sub-32-bit read issue with NAND and FPGA/FIFO GPMC Not supported in SDK
i2324 No synchronizer present between GCM and GCD status signals Common Open
i2345 CPSW: Ethernet Packet corruption occurs if CPDMA fetches a packet which spans across memory banks CPSW Implemented
i2350 McSPI data transfer using EDMA in 'ABSYNC' mode stops after 32 bits transfer McSPI Implemented
i2354 SDFM: Two Back-to-Back Writes to SDCPARMx Register Bit Fields CEVT1SEL, CEVT2SEL, and HZEN Within Three SD-Modulator Clock Cycles can Corrupt SDFM State Machine, Resulting in Spurious Comparator Events SDFM Open
i2355 ADC: DMA Read of Stale Result ADC Implemented
i2356 ADC: Interrupts may Stop if INTxCONT (Continue-to-Interrupt Mode) is not Set ADC Implemented
i2375 SDFM module event flags (SDIFLG.FLTx_FLG_CEVTx) do not get set again if the comparator event is still active and digital filter path (using SDCOMPxCTL.CEVTxDIGFILTSEL) is being selected SDFM Open
i2392 Race condition in capture registers resulting in events miss Common Open
i2394 Race condition in interrupt and error aggregator capture registers resulting in events miss Common Open
i2401 CPSW: Host Timestamps Cause CPSW Port to Lock up CPSW Open
i2402 CPSW: Ethernet to Host Checksum Offload does not work CPSW Open
i2404 Race condition in mailbox registers resulting in events miss IPC Implemented
i2405 CONTROLSS: Race condition OUTPUT_XBAR and PWM_XBAR resulting in event miss XBAR Open

Limitations

ID Head Line Module Reported in release Workaround
MCUSDK-9471 Ethernet CPSW CPDMA stuck with SOF overrun when TCP/DUP checksum offload is enabled. Ethernet CPSW 08.05.00 onwards Disable TCPUDP checksum offload in receive (THOST) direction.

Upgrade and Compatibility Information

Compiler Options

Module Affected API Change Additional Remarks

SOC Device Drivers

Module Affected API Change Additional Remarks
Linker Default linker in SDK SDK is moved to support sysconfig based linker generation Older is removed from core project ti-arm-clang folder and syconfig will generate the new linker under generated folder during sysconfig file generation step of compilation refer Memory Configurator. Customer project created earlier can continue to use the existing linker if they don't want to move to syscofnig based linker.

Ethernet and Networking

Module Affected API Change Additional Remarks
LwIP TCP/IP stack None Upgraded to 2.2.0 version Please refer to Lightweight IP (LwIP) 'Upgrade' section