AM263x MCU+ SDK  11.01.00
Release Notes 09.00.00

Attention
Also refer to individual module pages for more details on each feature, unsupported features, important usage guidelines.
Note
The examples will show usage of SW modules and APIs on a specific CPU instance and OS combination.
Unless explicitly noted otherwise, the SW modules would work in both FreeRTOS and no-RTOS environment.
Unless explicitly noted otherwise, the SW modules would work on any of the R5F's present on the SOC.

New in this Release

Feature Module
SFO calibration library and examples EPWM
Optimized IRQ handler and low latency interrupt example DPL
Standby (WFI) mode support DPL noRTOS DPL
EDMA example to transfer between different memories EDMA
SysConfig option to enable pBIST for SBL SBL
Interrupt profiling support and example DPL
Support for loading HS-FS firmware view CCS load script Common
MbedTLS MQTT example Networking
Support added for Single Packet reception from DMA Networking
Smart placement support Common
IEC60730 Support added. R5F CPU static register read diagnoctic and example added. SDL
SDL is safety certified from TuV for ISO26262/IEC61508 for MCU PLUS SDK version 8.6.0. SDL

Device and Validation Information

SOC Supported CPUs EVM Host PC
AM263x R5F AM263x ControlCard Revision E1 (referred to as am263x-cc in code).
Windows 10 64b or Ubuntu 18.04 64b
AM263x R5F AM263x LaunchPad Revision E2 (referred to as am263x-lp in code) Windows 10 64b or Ubuntu 18.04 64b

Dependent Tools and Compiler Information

Tools Supported CPUs Version
Code Composer Studio R5F 12.4.0
SysConfig R5F 1.17.0 build, build 3128
TI ARM CLANG R5F 2.1.3.LTS
FreeRTOS Kernel R5F 10.4.3
LwIP R5F STABLE-2_1_2_RELEASE
Mbed-TLS R5F mbedtls-2.13.1
Attention
TI ARM CLANG 2.1.3.LTS is not part of CCS by default, Follow steps at TI CLANG Compiler Toolchain to install the compiler

Key Features

Experimental Features

Attention
Features listed below are early versions and should be considered as "experimental".
Users can evaluate the feature, however the feature is not fully tested at TI side.
TI would not support these feature on public e2e.
Experimental features will be enabled with limited examples and SW modules.
Feature Module
SENT Encoder Example PRU_IO
SENT Decoder Example PRU_IO
Empty PRU firmware Example PRU_IO
GUI for UART Uniflash Tool Bootloader
GUI for UART Uniflash Tool Bootloader

OS Kernel

OS Supported CPUs SysConfig Support Key features tested Key features not tested / NOT supported
FreeRTOS Kernel R5F NA Task, Task notification, interrupts, semaphores, mutexs, timers Task load measurement using FreeRTOS run time statistics APIs. Limited support for ROV features.
FreeRTOS POSIX R5F NA pthread, mqueue, semaphore, clock -
NO RTOS R5F NA See Driver Porting Layer (DPL) below -

Driver Porting Layer (DPL)

Module Supported CPUs SysConfig Support OS support Key features tested Key features not tested / NOT supported
Cache R5F YES FreeRTOS, NORTOS Cache write back, invalidate, enable/disable -
Clock R5F YES FreeRTOS, NORTOS Tick timer at user specified resolution, timeouts and delays -
CpuId R5F NA FreeRTOS, NORTOS Verify Core ID and Cluster ID that application is currently running on -
CycleCounter R5F NA FreeRTOS, NORTOS Measure CPU cycles using CPU specific internal counters -
Debug R5F YES FreeRTOS, NORTOS Logging and assert to any combo of: UART, CCS, shared memory -
Heap R5F NA FreeRTOS, NORTOS Create arbitrary heaps in user defined memory segments -
Hwi R5F YES FreeRTOS, NORTOS Interrupt register, enable/disable/restore, Interrupt prioritization -
MPU R5F YES FreeRTOS, NORTOS Setup MPU and control access to address space -
Semaphore R5F NA FreeRTOS, NORTOS Binary, Counting Semaphore, recursive mutexs with timeout -
Task R5F NA FreeRTOS Create, delete tasks -
Timer R5F YES FreeRTOS, NORTOS Configure arbitrary timers -

Secondary Bootloader (SBL)

Module Supported CPUs SysConfig Support OS support Key features tested Key features not tested / NOT supported
Bootloader R5FSS0-0 YES NORTOS Boot modes: QSPI, UART. All R5F's. RPRC, multi-core image format Force Dual Core Mode, Disable Dual Core Switch and R5SS1 only not tested

SOC Device Drivers

Peripheral Supported CPUs SysConfig Support DMA Supported Key features tested Key features not tested / NOT supported
ADC R5F YES Yes. Example: adc_soc_continuous_dma Single software triggered conversion, Multiple ADC trigger using PWM, Result read using DMA, EPWM trip through PPB limit, PPB limits, PPB offsets, burst mode oversampling, differential mode, Offset, EPWM triggered conversion -
Bootloader R5F YES Yes. DMA enabled for SBL QSPI Boot modes: QSPI, UART. All R5F's -
CMPSS R5F YES NA Asynchronous PWM trip -
CPSW R5F YES No MAC loopback, PHY loopback, LWIP: Getting IP, Ping, Iperf, Layer 2 MAC, Layer 2 PTP Timestamping and Ethernet CPSW Switch support -
DAC R5F YES Yes. Example: dac_sine_dma Constant voltage, Square wave generation, Sine wave generation with and without DMA, Ramp wave generation, Random Voltage generation -
ECAP R5F YES No ECAP APWM mode, PWM capture -
EDMA R5F YES NA DMA transfer using interrupt and polling mode, QDMA Transfer, Channel Chaining, PaRAM Linking -
EPWM R5F YES Yes. Example: epwm_dma PWM outputs A and B in up-down count mode, Trip zone, Update PWM using EDMA, Valley switching, High resolution time period adjustment, type5 feature -
EQEP R5F YES NA Speed and Position measurement. Frequency Measurement -
FSI R5F YES Yes. Example: fsi_loopback_dma RX, TX, polling, interrupt mode, Dma, single lane loopback. - FSI Spi Mode
GPIO R5F YES NA Output, Input and Interrupt functionality -
I2C R5F YES No Controller mode, basic read/write -
IPC Notify R5F YES NA Mailbox functionality, IPC between RTOS/NORTOS CPUs M4F core
IPC Rpmsg R5F YES NA RPMessage protocol based IPC M4F core
MCAN R5F YES No RX, TX, interrupt and polling mode, Corrupt Message Transmission Prevention, Error Passive state, Bus Off State, Bus Monitoring Mode -
MCSPI R5F YES Yes. Example: mcspi_loopback_dma Controller/Peripheral mode, basic read/write, polling, interrupt and DMA mode -
MDIO R5F YES NA Register read/write, link status and link interrupt enable API -
MPU Firewall R5F YES NA Only compiled (Works only on HS-SE device) -
MMCSD R5F YES NA MMCSD 4bit, Raw read/write - file IO, eMMC

PINMUX | R5F | YES | NA | Tested with multiple peripheral pinmuxes PMU | R5F | NO | NA | Tested various PMU events | Counter overflow detection is not enabled | - PRUICSS | R5F | YES | NA | Tested with Ethercat FW HAL | - QSPI | R5F | YES | Yes. Example: qspi_flash_dma_transfer | Read direct, Write indirect, Read/Write commands, DMA for read | - RTI | R5F | YES | No | Counter read, timebase selction, comparator setup for Interrupt, DMA requests | Capture feature, fast enabling/disabling of events not tested SDFM | R5F | YES | No | Filter data read from CPU, Filter data read with PWM sync | - SOC | R5F | YES | NA | Lock/unlock MMRs, clock enable, set Hz, Xbar configuration, SW Warm Reset, Address Translation | - SPINLOCK | R5F | NA | NA | Lock, unlock HW spinlocks | - UART | R5F | YES | Yes. Example: uart_echo_dma | Basic read/write at baud rate 115200, polling, interrupt mode | HW flow control not tested, DMA mode not supported WATCHDOG | R5F | YES | NA | Reset mode, Interrupt mode | -

Board Device Drivers

Peripheral Supported CPUs SysConfig Support Key features tested Key features not tested
EEPROM R5F YES Only compiled -
ETHPHY R5F YES Tested with ethercat_slave_beckhoff_ssc_demo example -
FLASH R5F YES QSPI Flash -
LED R5F YES GPIO -

CMSIS

Module Supported CPUs SysConfig Support OS Support Key features tested Key features not tested
- - - - - -

Industrial Communications Toolkit

Module Supported CPUs SysConfig Support OS Support Key features tested Key features not tested
EtherCAT SubDevice FWHAL R5F NO FreeRTOS Tested with ethercat_slave_beckhoff_ssc_demo example Reset isolation

Motor Control

Module Supported CPUs SysConfig Support OS Support Key features tested Key features not tested
- - - - - -

Networking

Module Supported CPUs SysConfig Support OS Support Key features tested Key features not tested
LwIP R5F YES FreeRTOS TCP/UDP IP networking stack with and without checksum offload enabled, TCP/UDP IP networking stack with server and client functionality, basic Socket APIs, netconn APIs and raw APIs, DHCP, ping, TCP iperf, scatter-gather, DSCP priority mapping Other LwIP features
Ethernet driver (ENET) R5F YES FreeRTOS Ethernet as port using CPSW, MAC loopback and PHY loopback, Layer 2 MAC, Packet Timestamping, CPSW Switch, CPSW EST, interrupt pacing, Policer and Classifier, MDIO Manual Mode, CBS (IEEE 802.1Qav), Strapped PHY (Early Ethernet) RMII mode
ICSS-EMAC R5F YES FreeRTOS Only compiled Not tested
Mbed-TLS R5F NO FreeRTOS Tested software cryptography after porting, used mbedTLS with LwIP to implement HTTPS server Hardware offloaded cryptography

Demos

Module Supported CPUs SysConfig Support OS Support Key features tested Key features not tested
- - - - - -

Safety Diagnostic Library

Module Supported CPUs SysConfig Support OS support Key features tested Key features not tested / NOT supported
MCRC R5F NA NORTOS Full CPU, Auto CPU Mode and Semi CPU Auto Mode -
DCC R5F NA NORTOS Single Shot and Continuous modes -
PBIST R5F NA NORTOS Memories supported by MSS PBIST controller. -
ESM R5F NA NORTOS Tested in combination with RTI, DCC -
RTI R5F NA NORTOS WINDOWSIZE_100_PERCENT, WINDOWSIZE_50_PERCENT ,Latency/Propagation timing error(early)(50% window),Latency/Propagation timing error(late)(50% window) -
ECC R5F NA NORTOS ECC of MSS_L2, R5F TCM, MCAN, VIM, ICSSM, TPTC R5F Cache
ECC Bus Safety R5F NA NORTOS AHB, AXI, TPTC -
CCM R5F NA NORTOS CCM Self Test Mode,Error Forcing Mode and Self Test Error Forcing Mode. -
R5F STC(LBIST), Static Register Read R5F NA NORTOS STC of R5F, R5F CPU Static Register Read -

Fixed Issues

ID Head Line Module Applicable Releases Applicable Devices Resolution/Comments
MCUSDK-8526 SBL examples should be calling Bootloader_loadSelfCpu for R5_0-0 core SBL 8.4.0 onwards -
MCUSDK-9662 QSPI LLD EDMA Transfer fails for size (Unaligned) > MAX EDMA CNT QSPI 8.4.0 onwards Initiate trasfer with aligned data
MCUSDK-9811 IPC Notify unregister client always returns success IPC 8.05.00 onwards Added status variable check
MCUSDK-9835 SBL should support HS-SE device build via CCS SBL 8.05.00 onwards Added devconfig for CCS build
MCUSDK-10102 Trip Zone example not working EPWM 8.6.0 Gpio changes needed on E1 to E2 migration
MCUSDK-10119 MCAN External read write example fails for multirun MCAN 8.5.0 onwards Interrupt reset is required during init in example
MCUSDK-10144 RTI driver Up Counter calculation in driver is incorrect Timer 8.06.00 onwards Updated calculation to subtract reload value by one
MCUSDK-10167 All the system project are made based on AM2631 CCS 8.6.0 Updated to CCS12.4 and latest CSP
MCUSDK-10295 ECAP : driver : Flags read doesn't include the Signal Monitoring errors ECAP 8.5.0 onwards -
MCUSDK-10550 Global Strobe Load Signal from EPWMs is not taking effect on ECAP Signal Monitoring ECAP 8.5.0 onwards -
MCUSDK-10712 GPIO_Input_Interrupt Example not working GPIO 8.6.0 Added Interrupt config call in template
MCUSDK-10713 Interrupt registration fixed in the IPC Driver code IPC 8.5.0 onwards Added Sysconfig based interrupt registration
MCUSDK-10841 SBL needs to copy the vector table for self core right before the self-core reset release SBL 8.06.00 onwards Move the image load for self core just before the release reset instead of doing it early
MCUSDK-11290 EPWM: High Resolution DeadBand APIs does not write to registers properly EPWM 8.6.0 -
MCUSDK-11354 EPWM_clearTripZoneFlag() function in the SDK does not clear the CAPEVT signal EPWM 8.6.0 Updated EPWM_clearTripZoneFlag API to accept CAPEVT as input
MCUSDK-11401 Mailbox memory needs to be cleared after HSMRt load SBL 8.6.0 -
MCUSDK-11207 Incorrect IOCTL params for CPSW ENET_TIMESYNC_IOCTL_SET_TIMESTAMP Networking 8.5.0 -
MCUSDK-10775 Example build failing on enabling External Phy Management Networking 8.6.0 -
PROC_SDL-5981 SDL does not handle CCM callback of R5FSS1. SDL 8.5.0 onwards -

Known Issues

ID Head Line Module Reported in release Workaround
MCUSDK-4234 FSI RX Generic Trigger Test is not working FSI 8.3.0 -
SITARAAPPS-2040 Dual Core configuration issue with CSP 1.1.3 (Sitara MCU Device Support) on AM263x CSP Gel Scripts 8.2.1 Edit gel file as mentioned in Prerequisites while running multi core applications.
MCUSDK-7030 Interrupt nesting is not functional as expected when you have 2 or more interrupts with different priorities MCAN 8.4.0 Keep the interrupt priority same in system
MCUSDK-7319 CONTROLSS-SDFM: Two Back-to-Back Writes to SDCPARMx Register Bit Fields CEVT1SEL, CEVT2SEL, and HZEN Within Three SD-Modulator Clock Cycles can Corrupt SDFM State Machine, Resulting in Spurious Comparator Events SDFM 8.4.0 Avoid back-to-back writes within three SD-modulator clock cycles or have the SDCPARMx register bit fields configured in one register write.
MCUSDK-8073 UART1 not working as expected while configuring two uarts i.e UART0 and UART1 for two different cores UART 8.4.0 onwards UART1 configuration from other core should be done after UART0 is configured and initialized
MCUSDK-9082 MbedTLS - RSA exploit by kernel-privileged cache side-channel attackers Mbed-TLS 8.6.0 -
MCUSDK-10626 FSI DMA loopback example TX and RX mismatching on 2nd run FSI 8.6.0 Reset board between 2 runs
MCUSDK-11462 EPWM: Illegal Combo Logic example fails EPWM 9.0.0 -
PROC_SDL-5616 ECC Bus Safety SEC and DED Error Injection fails for CPSW. SDL 8.6.0 onwards None.
PROC_SDL-5617 ECC Bus Safety SEC and DED Error Injection fails for MSS_L2. SDL 8.6.0 onwards None.
PROC_SDL-4749 ECC Bus Safety DED Error Injection fails for AXI. SDL 8.5.0 onwards None.
MCUSDK-11506 ENET: CPDMA Goes To Lockup State. CPSW 8.5.0 onwards Disable THOST checksum Offload.
MCUSDK-11507 ENET: CPSW MAC port is stuck forever and dropping all the Rx/Tx packets with reception of corrupts preamble. CPSW 8.2.0 onwards Disable hostRxTimestampEn flag in CPSW CPST configuration. This does not impact the CPTS Rx or Tx Timestamp Events for PTP packets and is orthogonal feature.
MCUSDK-10978 CCS build doesn't support for HS appimages generation CCS 09.00.00 Use make/gmake based build for HS-SE
PROC_SDL-5979 R5F Cache ECC diagnostics are not supported. SDL 8.5.0 onwards None.
MCUSDK-9309 IPC: Issue when Combination of Notify and RPMsg is enabled in SysCfg. IPC 8.01.00 onwards Use Only Notify or Only Notify+RPMsg on all cores.

Errata

ID Head Line Module SDK Status
i2311 USART: Spurious DMA Interrupts UART Implemented
i2354 SDFM: Two Back-to-Back Writes to SDCPARMx Register Bit Fields CEVT1SEL, CEVT2SEL, and HZEN Within Three SD-Modulator Clock Cycles can Corrupt SDFM State Machine, Resulting in Spurious Comparator Events SDFM Open
i2355 ADC: DMA Read of Stale Result ADC Implemented
i2345 CPSW: Ethernet Packet corruption occurs if CPDMA fetches a packet which spans across memory banks CPSW Implemented
i2350 McSPI data transfer using EDMA in 'ABSYNC' mode stops after 32 bits transfer McSPI Open
i2356 ADC: Interrupts may Stop if INTxCONT (Continue-to-Interrupt Mode) is not Set ADC Implemented
i2324 No synchronizer present between GCM and GCD status signals Common Open
i2375 SDFM module event flags (SDIFLG.FLTx_FLG_CEVTx) do not get set again if the comparator event is still active and digital filter path (using SDCOMPxCTL.CEVTxDIGFILTSEL) is being selected SDFM Open
i2313 GPMC: Sub-32-bit read issue with NAND and FPGA/FIFO GPMC Open

Limitations

ID Head Line Module Reported in release Workaround
MCUSDK-9471 Ethernet CPSW CPDMA stuck with SOF overrun when TCP/DUP checksum offload is enabled. Ethernet CPSW 08.05.00 onwards Disable TCPUDP checksum offload in receive (THOST) direction.

Upgrade and Compatibility Information

Compiler Options

Module Affected API Change Additional Remarks

SOC Device Drivers

Module Affected API Change Additional Remarks
IPC Notify IpcNotify_init IntrPriority added as an element in IpcNotify_Params structure to make interrupt priority configurable. This field is automatically updated by sysconfig
ClockP ClockP_init IntrPriority added as an element in ClockP_Params structure to make Tick interrupt priority configurable. This field is automatically updated by sysconfig
Module Affected API Change Additional Remarks

Networking

Module Affected API Change Additional Remarks