AM263x MCU+ SDK  11.01.00
EVM Revision E2 support

Note
AM263x MCU+ SDK release supports ControlCard Revision E1 and LaunchPad Revision E2.
Limited testing is done for ControlCard E2 revision with this release and not all example may work out of box from SDK on E2 revision ControlCard.
This page has information about using SDK release with E2 revision of ControlCard and lists down SDK examples which require update to run on E2 revision ControlCard.

ControlCard

LaunchPad

Pins for DAC and ADC on CC E2 are as follows

DAC Instance HSEC PIN
DAC 9 (ADC1_MUX_SEL signal LOW)
ADC Instance ADC channel HSEC PIN
ADC0 ADC0_AIN0 9 (ADC1_MUX_SEL signal HIGH)
ADC0 ADC0_AIN1 11 (ADC1_MUX_SEL signal HIGH)
ADC0 ADC0_AIN2 15
ADC0 ADC0_AIN3 17
ADC0 ADC0_AIN4 21
ADC0 ADC0_AIN5 23
ADC1 ADC1_AIN0 12
ADC1 ADC1_AIN1 14
ADC1 ADC1_AIN2 18
ADC1 ADC1_AIN3 20
ADC1 ADC1_AIN4 24
ADC1 ADC1_AIN5 26
ADC2 ADC2_AIN0 31
ADC2 ADC2_AIN1 33
ADC2 ADC2_AIN2 37
ADC2 ADC2_AIN3 39
ADC2 ADC2_AIN4 -
ADC2 ADC2_AIN5 -
ADC3 ADC3_AIN0 28
ADC3 ADC3_AIN1 30
ADC3 ADC3_AIN2 34
ADC3 ADC3_AIN3 36
ADC3 ADC3_AIN4 40
ADC3 ADC3_AIN5 42
ADC4 ADC4_AIN0 25 (ADC2_MUX_SEL signal HIGH)
ADC4 ADC4_AIN1 27 (ADC2_MUX_SEL signal HIGH)
ADC4 ADC4_AIN2 -
ADC4 ADC4_AIN3 -
ADC4 ADC4_AIN4 -
ADC4 ADC4_AIN5 -

Note

The following changes are required to run the examples on AM263x CC E2 version, and are applicable for releases 08.03.00 through 08.06.00.

CMPSS Asynchronous Trip

CMPSS Asynchronous trip

Changes required

  • Change the CMPSS instance from CMPSS0 to say CMPSS1
  • Change the neccessary trip signal routing

Description

A CMPSS example that enables the CMPSS High comparator and feeds the asynchronous output to GPIO and EPWM

This example enables the CMPSSA0 CMPSSA1 COMPH comparator and feeds the asynchronous CTRIPOUTH signal to the XBAROUT0 pin and CTRIPH to EPWM0B.

CMPSS is configured to generate trip signals to trip the EPWM signals. CMPIN1P is used to give positive input and internal DAC is configured to provide the negative input. Internal DAC is configured to provide a signal at VDD/2. An EPWM signal is generated at EPWM0B and is configured to be tripped by CTRIPOUTH.

When a low input(VSS) is provided to CMPIN1P,

  • Trip signal(XBAROUT0) output is low
  • EPWM0B gives a PWM signal

When a high input(higher than VDD/2) is provided to CMPIN1P,

  • Trip signal(XBAROUT0) output turns high
  • EPWM0B gets tripped and outputs as high

External Connections

  • Give input on CMPIN1P (ControlCard HSEC Pin 15)
  • Outputs can be observed on
    • XBAROUT0 (SOC pin QSPI0_CSN1. USER_LED1 on ControlCard)
    • and EPWM0B (ControlCard HSEC pin 51) using an oscilloscope

Images

CMPSS_INSTANCE_CHANGE

CMPSS_EPWM_XBAR

CMPSS_OUTPUT_XBAR

ADC Burst Mode Oversampling

ADC Burst Mode Oversampling

Changes required

  • Change the ADC0 instance to a different ADC instance, say, ADC1.
  • Change the necessary interrupt routing

Description

This example sets up ePWM0 to periodically trigger a set of conversions (SOC0,1,12,13,14,15) on ADC0 ADC1 for conversion of inputs on ADC_AIN0, ADC_AIN1 and burst mode conversion on ADC_AIN3.

This demonstrates a batch of conversion on ADC0 ADC1 (inputs on ADC_AIN0 and ADC_AIN1) and burst mode conversion on ADC0 ADC1 (input ADC_AIN3)

ADC0 ADC1 Interrupt ISR is used to read results of ADC0 ADC1 (i.e. digital representations of inputs ADC_AIN0, ADC_AIN1 and average of oversampled ADC_AIN3)

The below watch variables can be used to view ADC conversion results.

Watch Variables gAdc0Result0 - Digital representation of the voltage on pin ADC0_AIN0 ADC1_AIN0 gAdc0result1 - Digital representation of the voltage on pin ADC0_AIN1 ADC1_AIN1 gadc0Result2 - Digital representation of the voltage on pin ADC0_AIN3 ADC1_AIN3

External Connections

ADC0_AIN0 ADC1_AIN0, ADC0_AIN1 ADC1_AIN1, ADC0_AIN3 ADC1_AIN3 pins should be connected to signals to be converted.

Check example.syscfg

Images

ADC_instance_change

ADC_INT_XBAR change

ADC Differential Mode

ADC Differential Mode

Changes required

  • Change the ADC0 instance to a different ADC instance, say, ADC1.
  • Change the necessary interrupt routing

Description

This example sets up ePWM0 to periodically trigger a set of conversions (SOC0,1) on ADC0 ADC1 for conversion of inputs on ADC_AIN0, ADC_AIN1 in differential modes (ADC_AIN0 - ADC_AIN1) on SOC0 and (ADC_AIN1 - ADC_AIN0) on SOC1. Note: In differential mode, the outputs are symmetric across "2112 or 0x840" i.e., if there is a 1v on differential input, expected output should be around 2752 or 0xAC0. if there is a -1v on differential input, expected output should be around 1472 or 0x5C0. Expect overflow if the readings are above 4224 ADC0 ADC1 Interrupt ISR is used to read results of ADC0 ADC1 (i.e. digital representations of inputs ADC_AIN0, ADC_AIN1 and average of oversampled ADC_AIN3) The below watch variables can be used to view ADC conversion results. Watch Variables gAdc0Result0 - Digital representation of the differential voltage on pins ADC0_AIN0 - ADC0_AIN1 ADC1_AIN0 - ADC1_AIN1 gAdc0result1 - Digital representation of the differential voltage on pins ADC0_AIN1 - ADC0_AIN0 ADC1_AIN1 - ADC1_AIN0 External Connections ADC0_AIN0 ADC1_AIN0, ADC0_AIN1 ADC1_AIN1 pins should be connected to signals to be converted. Check example.syscfg

Images

ADC_instance_change

ADC_INT_XBAR change

ADC Multiple SOC EPWM

ADC Multiple SOC EPWM

Changes required

  • Change the ADC0 instance to a different ADC instance, say, ADC2.
  • Change the necessary interrupt routing

Description

This example sets up ePWM0 to periodically trigger a set of conversions (SOC0,1,2) on ADC0 ADC2 and ADC1. This demonstrates multiple ADCs working together to process a batch of conversions using the available parallelism across multiple ADCs. ADC0 ADC2 Interrupt ISR is used to read results of both ADC0 ADC2 and ADC1. The below watch variables can be used to view ADC conversion results. External Connections ADC0_AIN0 ADC2_AIN0, ADC0_AIN1 ADC2_AIN1, ADC0_AIN2 ADC2_AIN2 and ADC1_AIN0, ADC1_AIN1, ADC1_AIN2 pins should be connected to signals to be converted. Watch Variables gAdc0Result0 - Digital representation of the voltage on pin ADC0_AIN0 ADC2_AIN0 gAdc0result1 - Digital representation of the voltage on pin ADC0_AIN1 ADC2_AIN1 adc0Result2 - Digital representation of the voltage on pin ADC0_AIN2 ADC2_AIN2 adc1Result0 - Digital representation of the voltage on pin ADC1_AIN0 adc1Result1 - Digital representation of the voltage on pin ADC1_AIN1 adc1Result2 - Digital representation of the voltage on pin ADC1_AIN2

Images

ADC_instance_change

ADC_INT_XBAR change

ADC PPB EPWM Trip

ADC PPB EPWM Trip

Changes required

  • Change the ADC0 instance to a different ADC instance, say, ADC1.
  • Change the necessary interrupt routing

Description

This example uses the ADC Post Processing Block to trip a ePWM in case of out of bound input.

ADCINT1 is configured to periodically trigger the ADC. Initially ADC is triggered through software.

Limit detection Post processing block is configured and if ADC results are outside the defined range, the PPB will generate an ADCxEVTy event. This signal is configured as trip source for EPWM0, 1 and 2.

This example showcases one-shot, cycle-by-cycle and direct tripping of PWMs.

  • EPWM0 is configured for One Shot trip.
  • EPWM1 is configured for Cycle by Cycle trip.
  • EPWM2 is configured for Direct trip via Digital compare submodule.

External Connections ADC0_AIN2 ADC1_AIN2 pin should be connected to DAC output pin. EPWM0A, EPWM0B, EPWM1A, EPWM1B, EPWM2A, EPWM2B can be connected to an oscilloscope to validate tripping.

Watch Variables adc0Result2 - Digital representation of the voltage on pin ADC0_AIN2 ADC1_AIN2

Images

ADC_instance_change

ADC_INT_XBAR change

ADC_EPWM_XBAR change

ADC SOC Continuous DMA

ADC SOC Continuous DMA

Changes required

  • Change the ADC0 instance to a different ADC instance, say, ADC2.
  • Change the necessary interrupt routing

Description

This example sets up two ADC channels to convert simultaneously. The results will be transferred by DMA into a buffer in RAM.

It configures ePWM0 to trigger SOC0 on ADC0 ADC2 and ADC1. EPWM is only used to trigger the first ADC conversion. INT0 of ADC0 ADC2 is configured to generate interrupt after first conversion and will then disable EPWM SOC generation. INT1 of both ADC's is configured to enable continuous conversion.

DMA channel 0 is triggered at EOC0 of ADC0 ADC2 and will copy conversion result to a buffer in RAM. DMA channel 1 is triggered at EOC0 of ADC1 and will copy conversion result to another buffer in RAM. DMA will generate interrupt after the buffer is filled and will stop conversion on both ADC's.

The below watch variables can be used to view ADC conversion results.

External Connections ADC0_AIN0 ADC2_AIN0 and ADC1_AIN0 pins should be connected to signals to be converted.

Watch Variables gAdc0DataBuffer - Buffers which stores conversion results from ADC0 gAdc1DataBuffer - Buffers which stores conversion results from ADC1

Images

ADC_instance_change

ADC_INT_XBAR change

EDMA_CHANNEL_TRIGGER_SELECT change

ADC SOC software

ADC SOC software

Changes required

  • Change the ADC0 instance to a different ADC instance, say, ADC1.
  • Change the necessary interrupt routing

Description

This example uses the ADC module to perform an ADC SOC conversion triggered by software.

In this example ADC0 ADC1 is used to convert the SOC, the user can also select a different one.

This example also showcases how to configure and use the ADC module.

Images

ADC_instance_change