AM263x MCU+ SDK  11.01.00
Release Notes 07.03.05

Attention
Also refer to individual module pages for more details on each feature, unsupported features, important usage guidelines.
Note
The examples will show usage of SW modules and APIs on a specific CPU instance and OS combination.
Unless explicitly noted otherwise, the SW modules would work in both FreeRTOS and no-RTOS environment.
Unless explicitly noted otherwise, the SW modules would work on any of the R5F's present on the SOC.

Device and Validation Information

SOC Supported CPUs EVM Host PC
AM263x R5F - Windows 10 64b or Ubuntu 18.04 64b

Dependent Tools and Compiler Information

Tools Supported CPUs Version
Code Composer Studio R5F 11.1.0
SysConfig R5F 1.11.0 build, build 2255
TI ARM CLANG R5F 1.3.0.LTS
FreeRTOS Kernel R5F 10.4.3

Key Features

OS Kernel

OS Supported CPUs SysConfig Support Key features tested Key features not tested / NOT supported
FreeRTOS Kernel R5F NA Task, Task notification, interrupts, semaphores, mutexs, timers Task load measurement using FreeRTOS run time statistics APIs. Limited support for ROV features.
FreeRTOS POSIX R5F NA pthread, mqueue, semaphore, clock -
NO RTOS R5F NA See Driver Porting Layer (DPL) below -

Driver Porting Layer (DPL)

Module Supported CPUs SysConfig Support OS support Key features tested Key features not tested / NOT supported
Cache R5F YES FreeRTOS, NORTOS Cache write back, invalidate, enable/disable -
Clock R5F YES FreeRTOS, NORTOS Tick timer at user specified resolution, timeouts and delays -
CycleCounter R5F NA FreeRTOS, NORTOS Measure CPU cycles using CPU specific internal counters -
Debug R5F YES FreeRTOS, NORTOS Logging and assert to any combo of: UART, CCS, shared memory -
Heap R5F NA FreeRTOS, NORTOS Create arbitrary heaps in user defined memory segments -
Hwi R5F YES FreeRTOS, NORTOS Interrupt register, enable/disable/restore -
MPU R5F YES FreeRTOS, NORTOS Setup MPU and control access to address space -
Semaphore R5F NA FreeRTOS, NORTOS Binary, Counting Semaphore, recursive mutexs with timeout -
Task R5F NA FreeRTOS Create, delete tasks -
Timer R5F YES FreeRTOS, NORTOS Configure arbitrary timers -

Secondary Bootloader (SBL)

Module Supported CPUs SysConfig Support OS support Key features tested Key features not tested / NOT supported
- - - - - -

SOC Device Drivers

Peripheral Supported CPUs SysConfig Support Key features tested Key features not tested / NOT supported
ADC R5F YES Software triggered conversion -
Bootloader R5F YES Only compiled -
CMPSS R5F YES Only compiled -
DAC R5F YES Constant voltage and square wave generation -
ECAP R5F YES ECAP APWM generation mode -
EDMA R5F YES DMA transfer using interrupt and polling mode, QDMA Transfer, Channel Chaining, PaRAM Linking -
EPWM R5F YES Different Frequency, Duty cycle, interrupt mode -
EQEP R5F YES Frequency measurement -
FSI R5F YES Only compiled -
GPIO R5F YES Only compiled -
I2C R5F YES Controller mode, basic read/write -
IPC Notify R5F YES Low latency IPC between RTOS/NORTOS CPUs -
IPC Rpmsg R5F YES RPMessage protocol based IPC, All R5F cores M4F core
MCAN R5F YES Only compiled -
MCSPI R5F YES Only compiled -
MDIO R5F YES Only compiled -
MPU Firewall R5F YES Only compiled -
PINMUX R5F YES Only compiled -
PRUICSS R5F YES Only compiled -
QSPI R5F YES Read direct, Write indirect, Read/Write commands, DMA for read -
SDFM R5F YES Only compiled -
SOC R5F YES lock/unlock MMRs, get CPU name, clock enable, set Hz -
SPINLOCK R5F NA Lock, unlock HW spinlocks -
UART R5F YES Basic read/write, polling, interrupt mode HW flow control not tested, DMA mode not supported
WATCHDOG R5F YES Only compiled -

Board Device Drivers

Peripheral Supported CPUs SysConfig Support Key features tested Key features not tested
EEPROM R5F YES Only compiled -
ETHPHY R5F YES Only compiled -
FLASH R5F YES Only compiled -
LED R5F YES Only compiled -

CMSIS

Module Supported CPUs SysConfig Support OS Support Key features tested Key features not tested
- - - - - -

Motor Control

Module Supported CPUs SysConfig Support OS Support Key features tested Key features not tested
- - - - - -

Networking

Module Supported CPUs SysConfig Support OS Support Key features tested Key features not tested
- - - - - -

Demos

Module Supported CPUs SysConfig Support OS Support Key features tested Key features not tested
- - - - - -

Fixed Issues

NA

Known Issues

ID Head Line Module Reported in release Workaround
- - - -

-

Limitations

ID Head Line Module Reported in release Workaround
- - - - -

Upgrade and Compatibility Information

Not Applicable

SOC Device Drivers

Module Affected API Change Additional Remarks
- - - -