AM263x MCU+ SDK  11.01.00
MMCSD RAW IO EMMC LLD

Introduction

This example uses the LLD driver to demonstrates basic read write operations to the eMMC device in polling mode. The MMC instance and the media connected to it are selectable via Sysconfig.

The example writes known data to a particular offset in the media and then reads it back. The read data is then compared with the written known data. When both the comparisons match, test result is passed otherwise failed.

Supported Combinations

Parameter Value
CPU + OS r5fss0-0 nortos
Toolchain ti-arm-clang
Board am263x-cc
Example folder examples/drivers/mmcsd/mmcsd_raw_io_emmc_lld

Steps to Run the Example

See Also

MMCSD

Sample Output

[MMCSD] eMMC Polling LLD Starting...
Data Matched !!
All tests have passed!!