AM263x MCU+ SDK  11.01.00
ADC Early Interrupt Offset

Introduction

The early interrupt feature allows generation (or setting) of INT flag right before the Conversion starts, but after the sample and hold (acquisition) window. This is to facilitate the early updation to the system that the ADC result could be expected. The configurability of offset for the early interrupt allows even more flexibility as of after how many sysclk cycles from the Sample and hold windw should the interrupt be generated.

Diagram showcasing Early Interrupt and Offset feature of ADC

Example Description

This example demonstrates the early interrupt feature and its offset configurability for the ADC. SOC 1 is set to be triggered when ADC1_INT1 is set, which in turn is set for EOC/SOC0. Hence, SOC1 are supposed to happen at EOC0. The ADC1_INT1 is set as an early interrupt and the offset is varied. which delays the triggering of the SOC1. Although triggered, the SOC1 should wait until the conversion of SOC0 is complete. hence a delay from trigger to acquisition is present in SOC1. This can be obtained by setting the PPB (Post Processing Block) to the SOC1. So, by reading the varied delay against offset value, the example records the offset configurability of the early interrupt.

  • Note :
    • The PPB Delay reads minimum of 2 sysclk cycles even for immediate conversion.
    • ADC Clock is set to prescale factore of 3.

SOC Configurations

  • SOC 0 :
    1. Trigger is set to software.
    2. Sample window : 16
    3. Samples on Channel 0 (arbitrary)
  • SOC 1 :
    1. Trigger is set to software, ADC1_INT1.
    2. Sample window : 16
    3. Samples on Channel 0 (arbitrary)

PPB Configurations

  1. PPB 1 is set for SOC 1

Interrupt Configurations

INT xbar0 is set for ADC 1 INT 2.

  • ADC 1 INT 1 :
    1. triggered by EOC/SOC0
  • ADC 1 INT 2 :
    1. triggered by EOC/SOC1
    2. triggers ISR App_adcISR()

ISR configurations

  • App_adcISR0 :
    • reads the delays in SOC1.
    • clears the INT 1, 2 flags

External Connections

AM263Px-CC E2 or AM263x-CC E2 or AM261x-SOM E1

Feed analog inputs to channels ADC1_AIN0 - HSEC Pin 12

AM263x-CC E1

Feed analog inputs to channels ADC1_AIN0 - HSEC Pin 18

AM263Px-LP or AM263x-LP or AM261X-LP

Feed analog inputs to channels ADC1_AIN0 - J1/3 Pin 24

Watch Variables

gAdc1soc1Delay[] - holds the delay values for ADC1_SOC1

Supported Combinations

Parameter Value
CPU + OS r5fss0-0 nortos
Toolchain ti-arm-clang
Board am263x-cc, am263x-lp
Example folder examples/drivers/adc/adc_early_interrupt_offset/

Steps to Run the Example

  • When using CCS projects to build, import the CCS project for the required combination and build it using the CCS project menu (see Using SDK with CCS Projects).
  • When using makefiles to build, note the required combination and build using make command (see Using SDK with Makefiles)
  • (optional) Establish connections as mentioned in External Connections section.
  • Launch a CCS debug session and run the executable, see CCS Launch, Load and Run
  • Using the watch variables, view the ADC conversion results.
  • View the ADC conversion results in UART console logs

See Also

ADC

Sample Output

Shown below is a sample output when the application is run,

ADC Early Interrupt and Configurable Offset Test Started
Offset Delay
0 31
1 30
2 29
3 28
4 27
5 26
6 25
7 24
8 23
9 22
10 21
11 20
12 19
13 18
14 17
15 16
16 15
17 14
18 13
19 12
20 11
21 10
22 9
23 8
24 7
25 6
26 5
27 4
28 3
29 2
30 2
31 2
ADC Early Interrupt and Configurable Offset Test Passed
All tests have passed!!