AM263x MCU+ SDK  11.00.00
Bootloader_socCoreOpModeConfig Struct Reference

Detailed Description

Data structure containing information about the operating mode specific to the SOC.

This structure is used to store the data about Lock step or Stand alone mode as provided by the user in the syscfg.

Data Fields

uint32_t r5fss0_opMode
 
uint32_t r5fss1_opMode
 

Field Documentation

◆ r5fss0_opMode

uint32_t Bootloader_socCoreOpModeConfig::r5fss0_opMode

[IN] Operating mode for first R5 subsystem

◆ r5fss1_opMode

uint32_t Bootloader_socCoreOpModeConfig::r5fss1_opMode

[IN] Operating mode for second R5 subsystem