AM263x MCU+ SDK  11.00.00
R5F CPU Static Register Read Functions

Introduction

Functions

int32_t SDL_CPU_staticRegisterRead (SDL_R5FCPU_StaticRegs *pCPUStaticRegs)
 This API is used to get the value of static registers for R5F CPU. More...
 
void SDL_R5MPU_readStaticRegisters (SDL_R5MPU_staticRegs *pMPUStaticRegs, uint32_t regionNum)
 MPU API to Read the Static Registers. This function reads the values of the static registers such as System Control Register, MPU Type Register and MPU Region Number Register. More...
 

Function Documentation

◆ SDL_CPU_staticRegisterRead()

int32_t SDL_CPU_staticRegisterRead ( SDL_R5FCPU_StaticRegs pCPUStaticRegs)

This API is used to get the value of static registers for R5F CPU.

Parameters
pCPUStaticRegsPointer to the SDL_R5FCPU_StaticRegs structure.

◆ SDL_R5MPU_readStaticRegisters()

void SDL_R5MPU_readStaticRegisters ( SDL_R5MPU_staticRegs pMPUStaticRegs,
uint32_t  regionNum 
)

MPU API to Read the Static Registers. This function reads the values of the static registers such as System Control Register, MPU Type Register and MPU Region Number Register.

Parameters
pMPUStaticRegs[IN] Pointer to the static registers structure
regionNum[IN] Region number