AM263x MCU+ SDK  11.00.00
fsi/v0/fsi.h
Go to the documentation of this file.
1 /*
2  * Copyright (C) 2021 Texas Instruments Incorporated
3  *
4  * Redistribution and use in source and binary forms, with or without
5  * modification, are permitted provided that the following conditions
6  * are met:
7  *
8  * Redistributions of source code must retain the above copyright
9  * notice, this list of conditions and the following disclaimer.
10  *
11  * Redistributions in binary form must reproduce the above copyright
12  * notice, this list of conditions and the following disclaimer in the
13  * documentation and/or other materials provided with the
14  * distribution.
15  *
16  * Neither the name of Texas Instruments Incorporated nor the names of
17  * its contributors may be used to endorse or promote products derived
18  * from this software without specific prior written permission.
19  *
20  * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS
21  * "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT
22  * LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR
23  * A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT
24  * OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL,
25  * SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT
26  * LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE,
27  * DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY
28  * THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT
29  * (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE
30  * OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
31  */
32 
49 #ifndef FSI_V0_H_
50 #define FSI_V0_H_
51 
52 /* ========================================================================== */
53 /* Include Files */
54 /* ========================================================================== */
55 
56 #include <drivers/hw_include/cslr.h>
57 
58 #ifdef __cplusplus
59 extern "C" {
60 #endif
61 
62 /* ========================================================================== */
63 /* Macros & Typedefs */
64 /* ========================================================================== */
65 
66 /* Common defines for both FSI TX and RX */
67 
71 #define FSI_MAX_LEN_NWORDS_DATA ((uint16_t)0xFU)
72 
76 #define FSI_MAX_VALUE_USERDATA ((uint16_t)0xFFU)
77 
81 #define FSI_MAX_VALUE_BUF_PTR_OFF ((uint16_t)0xFU)
82 
86 #define FSI_CTRL_REG_KEY ((uint16_t)0xA5U)
87 
88 
97 typedef uint32_t FSI_DataWidth;
98 #define FSI_DATA_WIDTH_1_LANE ((uint32_t)0x0U)
99 
100 #define FSI_DATA_WIDTH_2_LANE ((uint32_t)0x1U)
101 
104 #define FSI_PINGTIMEOUT_ON_HWSWINIT_PING_FRAME ((uint32_t)0x1U)
105 
117 typedef uint32_t FSI_ECCComputeWidth;
118 
119 #define FSI_32BIT_ECC_COMPUTE ((uint32_t)0x0U)
120 
121 #define FSI_16BIT_ECC_COMPUTE ((uint32_t)0x1U)
122 
136 typedef uint32_t FSI_InterruptNum;
137 
138 #define FSI_INT1 ((uint32_t)0x0U)
139 
140 #define FSI_INT2 ((uint32_t)0x1U)
141 
163 typedef uint32_t FSI_FrameType;
164 
165 #define FSI_FRAME_TYPE_PING ((uint32_t)0x0U)
166 
167 #define FSI_FRAME_TYPE_ERROR ((uint32_t)0xFU)
168 
169 #define FSI_FRAME_TYPE_1WORD_DATA ((uint32_t)0x4U)
170 
171 #define FSI_FRAME_TYPE_2WORD_DATA ((uint32_t)0x5U)
172 
173 #define FSI_FRAME_TYPE_4WORD_DATA ((uint32_t)0x6U)
174 
175 #define FSI_FRAME_TYPE_6WORD_DATA ((uint32_t)0x7U)
176 
177 #define FSI_FRAME_TYPE_NWORD_DATA ((uint32_t)0x3U)
178 
190 typedef uint32_t FSI_PingTimeoutMode;
191 
196 #define FSI_PINGTIMEOUT_ON_HWINIT_PING_FRAME ((uint32_t)0x0U)
197 
198 #ifdef __cplusplus
199 }
200 #endif
201 
202 #endif /* #ifndef FSI_V0_H_ */
203 
FSI_InterruptNum
uint32_t FSI_InterruptNum
Interrupt lines supported in FSI.
Definition: fsi/v0/fsi.h:136
FSI_PingTimeoutMode
uint32_t FSI_PingTimeoutMode
FSI ping timeout mode.
Definition: fsi/v0/fsi.h:190
FSI_FrameType
uint32_t FSI_FrameType
FSI frame type.
Definition: fsi/v0/fsi.h:163
FSI_ECCComputeWidth
uint32_t FSI_ECCComputeWidth
ECC Computation width - 16 bit or 32 bit.
Definition: fsi/v0/fsi.h:117
FSI_DataWidth
uint32_t FSI_DataWidth
Data lines used for transmit/receive operation.
Definition: fsi/v0/fsi.h:97