AM263x MCU+ SDK  11.00.00
enet_mod_mdio.h
Go to the documentation of this file.
1 /*
2  * Copyright (c) Texas Instruments Incorporated 2020
3  *
4  * Redistribution and use in source and binary forms, with or without
5  * modification, are permitted provided that the following conditions
6  * are met:
7  *
8  * Redistributions of source code must retain the above copyright
9  * notice, this list of conditions and the following disclaimer.
10  *
11  * Redistributions in binary form must reproduce the above copyright
12  * notice, this list of conditions and the following disclaimer in the
13  * documentation and/or other materials provided with the
14  * distribution.
15  *
16  * Neither the name of Texas Instruments Incorporated nor the names of
17  * its contributors may be used to endorse or promote products derived
18  * from this software without specific prior written permission.
19  *
20  * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS
21  * "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT
22  * LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR
23  * A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT
24  * OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL,
25  * SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT
26  * LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE,
27  * DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY
28  * THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT
29  * (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE
30  * OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
31  */
32 
47 #ifndef ENET_MOD_MDIO_H_
48 #define ENET_MOD_MDIO_H_
49 
50 /* ========================================================================== */
51 /* Include Files */
52 /* ========================================================================== */
53 
54 #include <stdint.h>
57 
58 #ifdef __cplusplus
59 extern "C" {
60 #endif
61 
62 /* ========================================================================== */
63 /* Macros */
64 /* ========================================================================== */
65 
67 #define ENET_MDIO_FEAT_CLAUSE45 (ENET_BIT(0U))
68 
70 #define ENET_MDIO_FEAT_PHY_MONITOR (ENET_BIT(1U))
71 
73 #define ENET_MDIO_PUBLIC_IOCTL(x) (ENET_IOCTL_TYPE_PUBLIC | \
74  ENET_IOCTL_MDIO_BASE | \
75  ENET_IOCTL_MIN(x))
76 
78 #define ENET_MDIO_PRIVATE_IOCTL(x) (ENET_IOCTL_TYPE_PRIVATE | \
79  ENET_IOCTL_MDIO_BASE | \
80  ENET_IOCTL_MIN(x))
81 
83 #define ENET_MDIO_PHY_ADDR_MASK(addr) (ENET_BIT(addr))
84 
86 #define ENET_MDIO_IS_PHY_ADDR_SET(mask, addr) (((mask) & ENET_BIT(addr)) != 0U)
87 
89 #define ENET_MDIO_PHY_ADDR_MASK_NONE (0x00000000U)
90 
92 #define ENET_MDIO_PHY_ADDR_MASK_ALL (0xFFFFFFFFU)
93 
95 #define ENET_MDIO_PHY_CNT_MAX (31U)
96 
97 /* ========================================================================== */
98 /* Structures and Enums */
99 /* ========================================================================== */
100 
104 typedef enum EnetMdio_Ioctl_e
105 {
114 
123 
132 
141 
153 
162 
171 
180 
189 
198 
207 
216 
225 
234 
243 
252 
261 
276 
278 
282 typedef enum EnetMdio_Group_e
283 {
286 
289 
293 
297 typedef enum EnetMdio_FrameFmt_s
298 {
301 
305 
309 typedef enum EnetMdio_C45Mmd_e
310 {
313 
316 
319 
322 
325 
328 
332 
338 typedef struct EnetMdio_C22ReadInArgs_s
339 {
345 
347  uint32_t phyAddr;
348 
350  uint16_t reg;
352 
358 typedef struct EnetMdio_C45ReadInArgs_s
359 {
365 
367  uint32_t phyAddr;
368 
371 
373  uint16_t reg;
375 
381 typedef struct EnetMdio_C22WriteInArgs_s
382 {
388 
390  uint32_t phyAddr;
391 
393  uint16_t reg;
394 
396  uint16_t val;
398 
404 typedef struct EnetMdio_C45WriteInArgs_s
405 {
411 
413  uint32_t phyAddr;
414 
417 
419  uint16_t reg;
420 
422  uint16_t val;
424 
425 /* ========================================================================== */
426 /* Global Variables Declarations */
427 /* ========================================================================== */
428 
429 /* None */
430 
431 /* ========================================================================== */
432 /* Function Declarations */
433 /* ========================================================================== */
434 
435 /* None */
436 
437 /* ========================================================================== */
438 /* Deprecated Function Declarations */
439 /* ========================================================================== */
440 
441 /* None */
442 
443 /* ========================================================================== */
444 /* Static Function Definitions */
445 /* ========================================================================== */
446 
447 /* None */
448 
449 #ifdef __cplusplus
450 }
451 #endif
452 
453 #endif /* ENET_MOD_MDIO_H_ */
454 
ENET_MDIO_GROUP_NUM
@ ENET_MDIO_GROUP_NUM
Definition: enet_mod_mdio.h:291
ENET_MDIO_IOCTL_IS_POLL_ENABLED
@ ENET_MDIO_IOCTL_IS_POLL_ENABLED
Get link state change poll enable status.
Definition: enet_mod_mdio.h:152
EnetMdio_C45WriteInArgs::phyAddr
uint32_t phyAddr
Definition: enet_mod_mdio.h:413
EnetMdio_C45WriteInArgs::mmd
EnetMdio_C45Mmd mmd
Definition: enet_mod_mdio.h:416
ENET_MDIO_IOCTL_PRINT_REGS
@ ENET_MDIO_IOCTL_PRINT_REGS
Print MDIO registers.
Definition: enet_mod_mdio.h:122
EnetMdio_C22WriteInArgs::val
uint16_t val
Definition: enet_mod_mdio.h:396
ENET_MDIO_IOCTL_C22_ASYNC_READ_TRIGGER
@ ENET_MDIO_IOCTL_C22_ASYNC_READ_TRIGGER
Trigger Asynchronous read to PHY register.
Definition: enet_mod_mdio.h:197
enet_types.h
This file contains the basic types using across the Enet driver.
ENET_MDIO_IOCTL_C45_ASYNC_WRITE_TRIGGER
@ ENET_MDIO_IOCTL_C45_ASYNC_WRITE_TRIGGER
Trigger Asynchronous Write to PHY register using clause-45 frame.
Definition: enet_mod_mdio.h:251
ENET_MDIO_IOCTL_C45_ASYNC_READ_COMPLETE
@ ENET_MDIO_IOCTL_C45_ASYNC_READ_COMPLETE
Checks for async Read completion to PHY register using clause-45 frame.
Definition: enet_mod_mdio.h:242
ENET_MDIO_IOCTL_C45_READ
@ ENET_MDIO_IOCTL_C45_READ
Read a PHY register using clause-45 frame.
Definition: enet_mod_mdio.h:179
EnetMdio_C22WriteInArgs::reg
uint16_t reg
Definition: enet_mod_mdio.h:393
enet_ioctl.h
This file contains the type definitions and helper macros for the Enet IOCTL interface.
ENET_MDIO_IOCTL_C22_ASYNC_WRITE_COMPLETE
@ ENET_MDIO_IOCTL_C22_ASYNC_WRITE_COMPLETE
Checks for async Write completion to PHY register.
Definition: enet_mod_mdio.h:224
EnetMdio_C45WriteInArgs::val
uint16_t val
Definition: enet_mod_mdio.h:422
ENET_MDIO_IOCTL_C45_ASYNC_WRITE_COMPLETE
@ ENET_MDIO_IOCTL_C45_ASYNC_WRITE_COMPLETE
Checks for async Write completion to PHY register using clause-45 frame.
Definition: enet_mod_mdio.h:260
ENET_MDIO_MMD_VENDOR_1
@ ENET_MDIO_MMD_VENDOR_1
Definition: enet_mod_mdio.h:327
ENET_MDIO_MMD_VENDOR_2
@ ENET_MDIO_MMD_VENDOR_2
Definition: enet_mod_mdio.h:330
EnetMdio_C45ReadInArgs::reg
uint16_t reg
Definition: enet_mod_mdio.h:373
ENET_MDIO_MMD_WIS
@ ENET_MDIO_MMD_WIS
Definition: enet_mod_mdio.h:315
EnetMdio_C22WriteInArgs
Input args for ENET_MDIO_IOCTL_C22_WRITE command.
Definition: enet_mod_mdio.h:382
ENET_MDIO_IOCTL_ENABLE_STATE_MACHINE
@ ENET_MDIO_IOCTL_ENABLE_STATE_MACHINE
Enable MDIO state machine. Use.
Definition: enet_mod_mdio.h:275
EnetMdio_C45ReadInArgs::mmd
EnetMdio_C45Mmd mmd
Definition: enet_mod_mdio.h:370
EnetMdio_Ioctl
EnetMdio_Ioctl
MDIO IOCTL commands.
Definition: enet_mod_mdio.h:105
ENET_MDIO_MMD_PHY_XS
@ ENET_MDIO_MMD_PHY_XS
Definition: enet_mod_mdio.h:321
ENET_MDIO_GROUP_1
@ ENET_MDIO_GROUP_1
Definition: enet_mod_mdio.h:288
EnetMdio_C22ReadInArgs
Input args for ENET_MDIO_IOCTL_C22_READ command.
Definition: enet_mod_mdio.h:339
ENET_MDIO_IOCTL_C45_ASYNC_READ_TRIGGER
@ ENET_MDIO_IOCTL_C45_ASYNC_READ_TRIGGER
Trigger Asynchronous Read to PHY register using clause-45 frame.
Definition: enet_mod_mdio.h:233
ENET_MDIO_IOCTL_IS_ALIVE
@ ENET_MDIO_IOCTL_IS_ALIVE
Get PHY alive status.
Definition: enet_mod_mdio.h:131
EnetMdio_C45ReadInArgs
Input args for ENET_MDIO_IOCTL_C45_READ command.
Definition: enet_mod_mdio.h:359
EnetMdio_C45WriteInArgs
Input args for ENET_MDIO_IOCTL_C45_WRITE command.
Definition: enet_mod_mdio.h:405
ENET_MDIO_MMD_DTE_XS
@ ENET_MDIO_MMD_DTE_XS
Definition: enet_mod_mdio.h:324
EnetMdio_C45WriteInArgs::group
EnetMdio_Group group
Definition: enet_mod_mdio.h:410
ENET_MDIO_FRAME_FMT_C45
@ ENET_MDIO_FRAME_FMT_C45
Definition: enet_mod_mdio.h:303
ENET_MDIO_MMD_PCS
@ ENET_MDIO_MMD_PCS
Definition: enet_mod_mdio.h:318
ENET_MDIO_MMD_PMA_PMD
@ ENET_MDIO_MMD_PMA_PMD
Definition: enet_mod_mdio.h:312
ENET_MDIO_IOCTL_C22_ASYNC_READ_COMPLETE
@ ENET_MDIO_IOCTL_C22_ASYNC_READ_COMPLETE
Checks for async read completion to PHY register.
Definition: enet_mod_mdio.h:206
ENET_MDIO_IOCTL_IS_LINKED
@ ENET_MDIO_IOCTL_IS_LINKED
Get PHY link status.
Definition: enet_mod_mdio.h:140
ENET_MDIO_IOCTL_GET_VERSION
@ ENET_MDIO_IOCTL_GET_VERSION
Get the hardware version of the MDIO module.
Definition: enet_mod_mdio.h:113
EnetMdio_C22ReadInArgs::group
EnetMdio_Group group
Definition: enet_mod_mdio.h:344
ENET_MDIO_PUBLIC_IOCTL
#define ENET_MDIO_PUBLIC_IOCTL(x)
Helper macro to create IOCTL commands for MDIO module.
Definition: enet_mod_mdio.h:73
ENET_MDIO_IOCTL_C22_READ
@ ENET_MDIO_IOCTL_C22_READ
Read a PHY register using clause-22 frame.
Definition: enet_mod_mdio.h:161
EnetMdio_FrameFmt
EnetMdio_FrameFmt
Frame format.
Definition: enet_mod_mdio.h:298
EnetMdio_C45WriteInArgs::reg
uint16_t reg
Definition: enet_mod_mdio.h:419
ENET_MDIO_IOCTL_C22_WRITE
@ ENET_MDIO_IOCTL_C22_WRITE
Write a PHY register using clause-22 frame.
Definition: enet_mod_mdio.h:170
EnetMdio_C45ReadInArgs::group
EnetMdio_Group group
Definition: enet_mod_mdio.h:364
EnetMdio_Group
EnetMdio_Group
MDIO user group.
Definition: enet_mod_mdio.h:283
ENET_MDIO_FRAME_FMT_C22
@ ENET_MDIO_FRAME_FMT_C22
Definition: enet_mod_mdio.h:300
EnetMdio_C45ReadInArgs::phyAddr
uint32_t phyAddr
Definition: enet_mod_mdio.h:367
EnetMdio_C22WriteInArgs::phyAddr
uint32_t phyAddr
Definition: enet_mod_mdio.h:390
ENET_MDIO_GROUP_0
@ ENET_MDIO_GROUP_0
Definition: enet_mod_mdio.h:285
ENET_MDIO_IOCTL_C45_WRITE
@ ENET_MDIO_IOCTL_C45_WRITE
Write a PHY register using clause-45 frame.
Definition: enet_mod_mdio.h:188
EnetMdio_C22ReadInArgs::reg
uint16_t reg
Definition: enet_mod_mdio.h:350
EnetMdio_C22ReadInArgs::phyAddr
uint32_t phyAddr
Definition: enet_mod_mdio.h:347
ENET_MDIO_IOCTL_C22_ASYNC_WRITE_TRIGGER
@ ENET_MDIO_IOCTL_C22_ASYNC_WRITE_TRIGGER
Trigger Asynchronous Write to PHY register.
Definition: enet_mod_mdio.h:215
EnetMdio_C22WriteInArgs::group
EnetMdio_Group group
Definition: enet_mod_mdio.h:387
EnetMdio_C45Mmd
EnetMdio_C45Mmd
Clause-45 MDIO Manageable Device (MMD) addresses.
Definition: enet_mod_mdio.h:310