AM263x MCU+ SDK  11.00.00
Release Notes 08.04.00

Attention
Also refer to individual module pages for more details on each feature, unsupported features, important usage guidelines.
Note
The examples will show usage of SW modules and APIs on a specific CPU instance and OS combination.
Unless explicitly noted otherwise, the SW modules would work in both FreeRTOS and no-RTOS environment.
Unless explicitly noted otherwise, the SW modules would work on any of the R5F's present on the SOC.

New in this Release

Feature Module
Syconfig support and flash driver redesign to enable new flash configuration OSPI
Optimized trigonometric funtion support on R5 core Common
McSPI Driver update for performance improvement McSPI
LIN driver and example support LIN
EPWM: PWM protection and latency example using PRU EPWM
SBL support to configure R5 in lockstep or dualcore mode SBL
Syncronization support for 2 SDFM instances SDFM
High sampling rate examples for burst mode ADC
TCP/IP Checksum offload to hardware support enabled in ethernet CPSW driver CPSW
Simplified LwIP CPSW examples added for reference CPSW
CPSW Scatter-Gather and Interrupt pacing is enabled in enet driver and in reference example CPSW
CPSW driver memory footprint reduced by more than 40% CPSW
CPSW Layer-2 performance is benchmarked and added a reference example CPSW
CPSW driver support added for MDIO manual mode CPSW
CPSW ALE congurations are moved to SysConfig GUI CPSW
CPSW DSCP Priority mapping and Policer usecase is added in the CPSW example CPSW
Multi-core (R5) support added for CPSW driver CPSW

Device and Validation Information

SOC Supported CPUs EVM Host PC
AM263x R5F AM263x ControlCard Revision E1 (referred to as am263x-cc in code).
Windows 10 64b or Ubuntu 18.04 64b
AM263x R5F AM263x LaunchPad Revision E1 (referred to as am263x-lp in code) Windows 10 64b or Ubuntu 18.04 64b

Dependent Tools and Compiler Information

Tools Supported CPUs Version
Code Composer Studio R5F 12.0.0
SysConfig R5F 1.13.0 build, build 2553
TI ARM CLANG R5F 2.1.1.LTS
FreeRTOS Kernel R5F 10.4.3
LwIP R5F STABLE-2_1_2_RELEASE
Attention
TI ARM CLANG 2.1.1.LTS is not part of CCS by default, Follow steps at TI CLANG Compiler Toolchain to install the compiler

Key Features

Experimental Features

Attention
Features listed below are early versions and should be considered as "experimental".
Users can evaluate the feature, however the feature is not fully tested at TI side.
TI would not support these feature on public e2e.
Experimental features will be enabled with limited examples and SW modules.
Feature Module
GUI for UART Uniflash Tool Bootloader

OS Kernel

OS Supported CPUs SysConfig Support Key features tested Key features not tested / NOT supported
FreeRTOS Kernel R5F NA Task, Task notification, interrupts, semaphores, mutexs, timers Task load measurement using FreeRTOS run time statistics APIs. Limited support for ROV features.
FreeRTOS POSIX R5F NA pthread, mqueue, semaphore, clock -
NO RTOS R5F NA See Driver Porting Layer (DPL) below -

Driver Porting Layer (DPL)

Module Supported CPUs SysConfig Support OS support Key features tested Key features not tested / NOT supported
Cache R5F YES FreeRTOS, NORTOS Cache write back, invalidate, enable/disable -
Clock R5F YES FreeRTOS, NORTOS Tick timer at user specified resolution, timeouts and delays -
CpuId R5F NA FreeRTOS, NORTOS Verify Core ID and Cluster ID that application is currently running on -
CycleCounter R5F NA FreeRTOS, NORTOS Measure CPU cycles using CPU specific internal counters -
Debug R5F YES FreeRTOS, NORTOS Logging and assert to any combo of: UART, CCS, shared memory -
Heap R5F NA FreeRTOS, NORTOS Create arbitrary heaps in user defined memory segments -
Hwi R5F YES FreeRTOS, NORTOS Interrupt register, enable/disable/restore, Interrupt prioritization -
MPU R5F YES FreeRTOS, NORTOS Setup MPU and control access to address space -
Semaphore R5F NA FreeRTOS, NORTOS Binary, Counting Semaphore, recursive mutexs with timeout -
Task R5F NA FreeRTOS Create, delete tasks -
Timer R5F YES FreeRTOS, NORTOS Configure arbitrary timers -

Secondary Bootloader (SBL)

Module Supported CPUs SysConfig Support OS support Key features tested Key features not tested / NOT supported
Bootloader R5FSS0-0 YES NORTOS Boot modes: QSPI, UART. All R5F's. RPRC, multi-core image format Force Dual Core Mode, Disable Dual Core Switch and R5SS1 only not tested

SOC Device Drivers

Peripheral Supported CPUs SysConfig Support DMA Supported Key features tested Key features not tested / NOT supported
ADC R5F YES Yes. Example: adc_soc_continuous_dma Single software triggered conversion, Multiple ADC trigger using PWM, Result read using DMA, EPWM trip through PPB limit, burst mode oversampling, differential mode -
Bootloader R5F YES Yes. DMA enabled for SBL QSPI Boot modes: QSPI, UART. All R5F's -
CMPSS R5F YES NA Asynchronous PWM trip -
CPSW R5F YES No MAC loopback, PHY loopback, LWIP: Getting IP, Ping, Iperf, Layer 2 MAC, Layer 2 PTP Timestamping and CPSW Switch support -
DAC R5F YES Yes. Example: dac_sine_dma Constant voltage, Square wave generation, Sine wave generation with and without DMA, Ramp wave generation, Random Voltage generation -
ECAP R5F YES No ECAP APWM mode, PWM capture -
EDMA R5F YES NA DMA transfer using interrupt and polling mode, QDMA Transfer, Channel Chaining, PaRAM Linking -
EPWM R5F YES Yes. Example: epwm_dma PWM outputs A and B in up-down count mode, Trip zone, Update PWM using EDMA, Valley switching, High resolution time period adjustment, type5 feature -
EQEP R5F YES NA Speed and Position measurement. Frequency Measurement not tested
FSI R5F YES Yes. Example: fsi_loopback_dma RX, TX, polling, interrupt mode, Dma, single lane loopback. - FSI Spi Mode
GPIO R5F YES NA Output, Input and Interrupt functionality -
I2C R5F YES No Controller mode, basic read/write -
IPC Notify R5F YES NA Mailbox functionality, IPC between RTOS/NORTOS CPUs M4F core
IPC Rpmsg R5F YES NA RPMessage protocol based IPC M4F core
MCAN R5F YES No RX, TX, interrupt and polling mode, Corrupt Message Transmission Prevention, Error Passive state, Bus Off State, Bus Monitoring Mode -
MCSPI R5F YES Yes. Example: mcspi_loopback_dma Controller/Peripheral mode, basic read/write, polling, interrupt and DMA mode -
MDIO R5F YES NA Register read/write, link status and link interrupt enable API -
MPU Firewall R5F YES NA Only compiled (Works only on HS-SE device) -
PINMUX R5F YES NA Tested with multiple peripheral pinmuxes -
PRUICSS R5F YES NA Tested with Ethercat FW HAL -
QSPI R5F YES Yes. Example: qspi_flash_dma_transfer Read direct, Write indirect, Read/Write commands, DMA for read -
RTI R5F YES No Counter read, timebase selction, comparator setup for Interrupt, DMA requests Capture feature, fast enabling/disabling of events not tested
SDFM R5F YES No Filter data read from CPU, Filter data read with PWM sync -
SOC R5F YES NA Lock/unlock MMRs, clock enable, set Hz, Xbar configuration, SW Warm Reset, Address Translation -
SPINLOCK R5F NA NA Lock, unlock HW spinlocks -
UART R5F YES Yes. Example: uart_echo_dma Basic read/write at baud rate 115200, polling, interrupt mode HW flow control not tested, DMA mode not supported
WATCHDOG R5F YES NA Reset mode Interrupt mode

Board Device Drivers

Peripheral Supported CPUs SysConfig Support Key features tested Key features not tested
EEPROM R5F YES Only compiled -
ETHPHY R5F YES Tested with ethercat_peripheral_beckhoff_ssc_demo example -
FLASH R5F YES QSPI Flash -
LED R5F YES GPIO -

CMSIS

Module Supported CPUs SysConfig Support OS Support Key features tested Key features not tested
- - - - - -

Industrial Communications Toolkit

Module Supported CPUs SysConfig Support OS Support Key features tested Key features not tested
EtherCAT Peripheral FWHAL R5F NO FreeRTOS Tested with ethercat_peripheral_beckhoff_ssc_demo example Reset isolation

Motor Control

Module Supported CPUs SysConfig Support OS Support Key features tested Key features not tested
- - - - - -

Networking

Module Supported CPUs SysConfig Support OS Support Key features tested Key features not tested
LwIP R5F YES FreeRTOS TCP/UDP IP networking stack with and without checksum offload enabled,, TCP/UDP IP networking stack, DHCP, ping, TCP iperf, TCP/UDP IP, scatter-gather Other LwIP features, checksum offload with VLAN_Tag, more robustness tests pending
Ethernet driver (ENET) R5F YES FreeRTOS Ethernet as port using CPSW and ICSS,Layer 2 MAC, Layer 2 PTP Timestamping, CPSW Switch, CPSW EST, interrupt pacing, Policer, MDIO Manual Mode -
ICSS-EMAC R5F YES FreeRTOS Only compiled Not tested

Demos

Module Supported CPUs SysConfig Support OS Support Key features tested Key features not tested
- - - - - -

Fixed Issues

ID Head Line Module Applicable Releases Applicable Devices Resolution/Comments
MCUSDK-4050 Long CS assert/deassert delay before and after the MCSPI data transfer McSPI 8.2.0 onwards AM263x Fixed
MCUSDK-4190 Fixed MAC address is hard-coded for CPDMA devices, this will cause issue when two boards are connected in the same network Enet 8.2.0 onwards AM263x Fixed
MCUSDK-4345 EDMA: Region interrupt not triggered if Channel Id and TCC are not equal EDMA 8.2.0 onwards AM263x Fixed
MCUSDK-4357 hw_types.h should include <stdint.h> to resolve dependent includes Common 8.2.0 onwards AM263x Fixed
MCUSDK-4538 [SBL] sbl qspi incorrect core number displayed for R5FSS1-0 SBL 8.3.0 onwards AM263x Fixed
MCUSDK-6263 ADC interrupt are not cleared properly in ADC_soc_continuous_dma example ADC 8.3.0 onwards AM263x Fixed
MCUSDK-7303 MCAN_getTxBufCancellationIntrEnable is misnamed MCAN 8.3.0 onwards AM263x Fixed
MCUSDK-7304 CPSW: LWIP example doesn't work on port 2 CPSW 8.3.0 onwards AM263x Fixed
MCUSDK-7308 Multiple RTI instances selection leads to duplicates variable declaration in auto generated files RTI & Sysconfig 8.3.0 onwards AM263x Fixed
MCUSDK-7322 ADC: minimum Acquistion window should be 16 ADC 8.3.0 onwards AM263x Fixed
MCUSDK-7342 Unable to add more than one instance of Output XBAR in sysconfig Sysconfig 8.3.0 onwards AM263x Fixed
MCUSDK-7813 ADC: Interrupts may Stop if INTxCONT (Continue-to-Interrupt Mode) is not Set ADC 8.3.0 onwards AM263x Fixed
MCUSDK-7827 CMPSS: Hysteresis APIs overwrite other register fields CMPSS 8.3.0 onwards AM263x Fixed
MCUSDK-7833 CMPSS: Invalid macros supported for input parameters to CMPSS_configLowComparator API CMPSS 8.3.0 onwards AM263x Fixed
MCUSDK-7834 CMPSS sysconfig: COMPL does not show configurable positive input source CMPSS 8.3.0 onwards AM263x Fixed
MCUSDK-7835 CMPSS sysconfig: CMPSSB shows invalid configurables CMPSS 8.3.0 onwards AM263x Fixed
MCUSDK-7838 CMPSS sysconfig: Incorrect the PWM sync source range and Blanking source range CMPSS 8.3.0 onwards AM263x Fixed
MCUSDK-7946 Invalid interrupt source configuration for burst mode oversampling, differential mode ADC example ADC 8.3.0 onwards AM263x Fixed
MCUSDK-8039 CPSW: Syscfg should not have two instances of CPSW for enabling both RGMIIs CPSW 8.3.0 onwards AM263x Fixed
MCUSDK-6207 A53x, Linux references in documentation Common 8.3.0 onwards Fixed
MCUSDK-7333 DEV_ID and Core IDs table is not mentioned in documentation Common 8.3.0 onwards Fixed
MCUSDK-7363 [enet] Documentation of file name incorrect in sysconfig generated file Enet 8.3.0 onwards Fixed
MCUSDK-8115 HRPWM_getHiResTimeBasePeriod() API function doesn't return correct value EPWM 8.2.0 onwards Fixed
MCUSDK-8116 HRPWM_getCounterCompareValue() API function doesn't return correct value EPWM 8.2.0 onwards Fixed
MCUSDK-8117 HRPWM_getHiResCounterCompareValueOnly() API function doesn't return correct value EPWM 8.2.0 onwards Fixed

Known Issues

ID Head Line Module Reported in release Workaround
MCUSDK-1016 Semaphore does not function as expected when "post" call is present in multiple ISRs at different priorities DPL, FreeRTOS 8.0.0 Disable interrupt nesting
MCUSDK-2294 GPIO Pin Direction GPIO. GPIO Pin Direction not getting automatically configured. 8.0.0 Use GPIO_setDirMode to set pin direction for GPIO pin.
MCUSDK-2557 eqep_frequency_measurement example is failing SBL 8.2.0 -
MCUSDK-4059 AM263x: FSI first frame transmitted is incorrect in DMA mode FSI 8.3.0 Please refer fsi_loopback_dma example.
MCUSDK-4234 FSI RX Generic Trigger Test is not working FSI 8.3.0 -
SITARAAPPS-2040 Dual Core configuration issue with CSP 1.1.3 (Sitara MCU Device Support) on AM263x CSP Gel Scripts 8.2.1 Edit gel file as mentioned in Prerequisites while running multi core applications.
MCUSDK-6909 EPWM: Emulation mode doesn't work EPWM 8.4.0 -
MCUSDK-7030 [NORTOS]Interrupt nesting is not functional as expected when you have 2 or more interrupts with different priorities MCAN 8.4.0 Keep the interrupt priority same in system
MCUSDK-7319 CONTROLSS-SDFM: Two Back-to-Back Writes to SDCPARMx Register Bit Fields CEVT1SEL, CEVT2SEL, and HZEN Within Three SD-Modulator Clock Cycles can Corrupt SDFM State Machine, Resulting in Spurious Comparator Events SDFM 8.4.0 Avoid back-to-back writes within three SD-modulator clock cycles or have the SDCPARMx register bit fields configured in one register write.
MCUSDK-7811 CPSW: Ethernet Packet corruption occurs if CPDMA fetches a packet which spans across memory banks CPSW 8.3.0 onwards Ensure from application side single ethernet packet does not span across memory banks.
MCUSDK-7915 SDFM: EPWM filter sync example does not configure and check the PWM synchronization SDFM 8.3.0 onwards None
MCUSDK-8072 [Enet] EnetBoard_setupPorts does not provide config option to enable internal delay for RGMII Enet 8.4.0 onwards None
MCUSDK-8073 UART1 not working as expected while configuring two uarts i.e UART0 and UART1 for two different cores UART 8.4.0 onwards UART1 configuration from other core should be done after UART0 is configured and initialized
MCUSDK-8079 EDMA: Aggregated interrupt used instead of Region interrupt EDMA 8.4.0 onwards None
MCUSDK-8235 AM263x LP: CMPSS: Example fails - PWM not tripped CMPSS 8.4.0 onwards None
MCUSDK-8348 EnetDma_initPktInfo does not initialized chkSumInfo member Enet 8.4.0 onwards All L2 based applications need to explicitly set EnetDma_initPktInfo.chkSumInfo = 0

Limitations

ID Head Line Module Reported in release Workaround
- - - - -

Upgrade and Compatibility Information

Compiler Options

Module Affected API Change Additional Remarks
- - Enabled copmpiler option -Oz and -flto for release mode build These option are enabled for Code size and performance optimization

SOC Device Drivers

Module Affected API Change Additional Remarks
MCSPI MCSPI_chConfig Added parameter for trigger level configuration txFifoTrigLvl, rxFifoTrigLvl in MCSPI_ChConfig Allows configuring tragger level through sys config. Regenerate the sys config files
MCAN MCAN_getTxBufCancellationIntrEnable Name changed from MCAN_getTxBufCancellationIntrEnable to MCAN_txBufCancellationIntrEnable. MCAN_getTxBufCancellationIntrEnable function sets (does not get). So renamed to MCAN_txBufCancellationIntrEnable.
CMPSS CMPSS_configLowComparator Values (macros) that can be passed to CMPSS_configLowComparator() Changed from CMPSS_INSRC_DAC, CMPSS_INSRC_PIN to CMPSS_INSRC_PIN_INL and CMPSS_INSRC_PIN_INH
CMPSS sysconfig lowCompPositive In CMPSSA 'Low Comparator Configuration', 'Negative Input Source' changed to 'Positive Input Source'. Valid values changed to CMPSS_INSRC_PIN_INL and CMPSS_INSRC_PIN_INH CMPSSA low comparator does not have configurable negative input source. Low comparator Positive input source is configurable between pin INL and pin INH
CMPSS sysconfig CMPSSB highCompNegative and CMPSSB lowCompPositive In CMPSSB 'High Comparator Configuration' -> 'Negative Input Source' and 'Low Comparator Configuration' -> 'Positive Input Source' are removed. CMPSSB high comparator and low comparator does not have configurable positive/negative input source.
SBL Bootloader_socCpuPowerOnReset Added argument to configure the R5 sub system to lockstep or dualcore mode

Function Bootloader_socCpuPowerOnReset() requires 2 arguments, cpuID and cpu operating mode