Introduction
The Single Edge Nibble Transmission protocol is a unidirectional communications method that connects the sensor/transmitting device and the controller/receiving device without the use of a coordination signal from the controller/receiving device. It is intended for usage in situations where high-resolution data must be transferred from a sensor to an engine control unit (ECU). It serves as a simpler, less expensive alternative to CAN, LIN, or PSI5 as well as a replacement for lesser resolution techniques such as traditional sensors that provide analog output voltage and PWM. Automotive applications for SENT-compatible sensor devices include applications for pedal sensing, mass airflow sensing, pressure sensing, temperature sensing, humidity sensing, and many others.
SENT Signal
The SENT decoder Example is a reference for software based implementation of SAE J2716. PRU ICSS firmware enables SENT decoder interface on TI Sitara AM263x processor. This example does following: configures pin mux, sets soc mux to enable gpio mode for ICSS, initializes PRU, DMEM and PRU INTC module, downloads crc look up table in PRU Data RAM, and extracts sent decoded signal to UART terminal.
Supported Combinations
| Parameter | Value |
| ICSSM | ICSSM |
| Toolchain | pru-cgt |
| Board | am263x-cc |
| Example folder | examples/pru_io/sent/decoder_pruicss_iep_ecap/example |
HW Setup
Encoder setup
Decoder setup
Encoder+Decoder Setup
Connect the folowing pins while using PRUICSS IEP ECAP Example
PR0_PRU0_GPIO0 (GPIO93) -> PR0_PRU0_GPIO0 (Pin no. 125)
PR0_PRU0_GPIO1 (GPIO94) -> PR0_PRU0_GPIO1 (Pin no. 126)
PR0_PRU0_GPIO2 (GPIO95) -> PR0_PRU0_GPIO2 (Pin no. 127)
PR0_PRU0_GPIO3 (GPIO96) -> PR0_PRU0_GPIO3 (Pin no. 128)
PR0_PRU0_GPIO4 (GPIO92) -> PR0_PRU0_GPIO4 (Pin no. 124)
PR0_PRU0_GPIO5 (GPIO87) -> PR0_PRU0_GPIO5 (Pin no. 108)
Ground Pin(Any) -> Ground Pin(Any) [To Make sure both boards are having common ground]
HW setup
Steps to Run the Example
- When using CCS projects to build, Import sent_decoder_r5f project from the above mentioned Example folder path.
- Build the projects.
- Load R5F project, run it. Decoder setup is now ready.
- We will be validating decoder demo using SENT encoder example. Next step is to setup sent encoder follow the steps mentioned in SENT Encoder Example.
- Note
- Prerequisite: PRU-CGT-2-3 (ti-pru-cgt) should be installed at:
C:/ti/
Sample Output
******************SENT DECODER Application**********************
SENT PRU-ICSS firmware loaded and running
******************CHANNEL0 SENT DATA**********************
Number of Frames received: 9
Channel0 calculated tick period: 538 ns
channel0 StatusComm Data: 08
Channel0: Data0 Data1 Data2 Data3 Data4 Data5 CRC
Value: 07 04 08 07 04 08 03
**********************************************************
******************CHANNEL1 SENT DATA**********************
Number of Frames received: 9
Channel0 calculated tick period: 538 ns
channel0 StatusComm Data: 08
Channel0: Data0 Data1 Data2 Data3 Data4 Data5 CRC
Value: 07 04 08 07 04 08 03
**********************************************************
******************CHANNEL2 SENT DATA**********************
Number of Frames received: 9
Channel0 calculated tick period: 538 ns
channel0 StatusComm Data: 08
Channel0: Data0 Data1 Data2 Data3 Data4 Data5 CRC
Value: 07 04 08 07 04 08 03
**********************************************************
******************CHANNEL3 SENT DATA**********************
Number of Frames received: 9
Channel0 calculated tick period: 538 ns
channel0 StatusComm Data: 08
Channel0: Data0 Data1 Data2 Data3 Data4 Data5 CRC
Value: 07 04 08 07 04 08 03
**********************************************************
******************CHANNEL4 SENT DATA**********************
Number of Frames received: 9
Channel0 calculated tick period: 538 ns
channel0 StatusComm Data: 08
Channel0: Data0 Data1 Data2 Data3 Data4 Data5 CRC
Value: 07 04 08 07 04 08 03
**********************************************************
******************CHANNEL5 SENT DATA**********************
Number of Frames received: 9
Channel0 calculated tick period: 538 ns
channel0 StatusComm Data: 08
Channel0: Data0 Data1 Data2 Data3 Data4 Data5 CRC
Value: 07 04 08 07 04 08 03
**********************************************************
- Note
- See list supported firmware design and list of supported feature : SENT
Steps to modify SENT decoder PRU Firmware
Modification supported: Change hardcoded tick period in firmware. Current release supports only 1us tick period support in firmware. In order to modify it:
- When using CCS projects to build, Import decoder_pru1_fw project from the above mentioned Example folder path.
- In
main.asm file modify ch0_ticktime to desired value(1000 to 3000) and accordingly modify ch0_syncpulse_min_dur = (0.8*ch0_ticktime)*56 and ch0_syncpulse_max_dur = (1.2*ch0_ticktime)*56. For example for 500ns tick period.
- Rebuild examples\pru_io\sent\decoder_pruicss_iep_ecap\decoder_pru0_fw project
- Rebuild examples\pru_io\sent\decoder_pruicss_iep_ecap\decoder_example
- Load R5F updated binary, run it.
ch0_ticktime .set 500
ch0_syncpulse_min_dur .set 400*56
ch0_syncpulse_max_dur .set 600*56