AM263x MCU+ SDK  11.00.00
SDL R5F ECC DTAG

Introduction

The example shows how to setup and use the ECC Safety Diagnostic operation on d-tag cache momory of R5F core. Shows the generation of SEC error on R5F ECC Aggregator for DTAG cache moemories.

Use Cases

Use Case Description
UC-1 Single bit error injection.
UC-2 Double bit error injection.

Supported Combinations

Parameter Value
CPU + OS r5fss0-0 nortos
r5fss1-0 nortos
Toolchain ti-arm-clang
Board am263x-cc
Example folder examples/sdl/ecc/sdl_ecc_r5_d-tag/

Steps to Run the Example

See Also

ECC : Error Correcting Code

Sample Output

Shown below is a sample output when the application is run,

ECC Example Application
ECC UC-1 and UC-2 Test
ECC_Test_init: Exception init complete
ESM_Test_init: Init MSS ESM complete
ECC_Test_init: R5FSS0 ECC initialization is completed
Starting Tests for Dtag cache - single error correction
Waiting for ESM Interrupt
Injected error and got ESM Interrupt for ram_Id = 8
Waiting for ESM Interrupt
Injected error and got ESM Interrupt for ram_Id = 9
Waiting for ESM Interrupt
Injected error and got ESM Interrupt for ram_Id = 10
Waiting for ESM Interrupt
Injected error and got ESM Interrupt for ram_Id = 11
Starting Tests for Dtag cache - double error detection
Waiting for ESM Interrupt
Injected error and got ESM Interrupt for ram_Id = 8
Waiting for ESM Interrupt
Injected error and got ESM Interrupt for ram_Id = 9
Waiting for ESM Interrupt
Injected error and got ESM Interrupt for ram_Id = 10
Waiting for ESM Interrupt
Injected error and got ESM Interrupt for ram_Id = 11
All tests have passed.