AM263x MCU+ SDK  11.00.00
UART HLD LLD External loopback

Introduction

This example demonstrates the UART RX and TX operation from both hld and lld driver APIs by looping the Tx & Rx externally in polling mode of operation.

External Connections :

AM263x-CC E2 :

Connect Jumper wires between the following HSEC pins

  • UART1_RXD(L3) J24 PIN-19 --— UART4_TXD(C12) J21 PIN-26
  • UART1_TXD(M3) J25 PIN-20 --— UART4_RXD(D11) J21 PIN-27

AM263x-LP :

Connect Jumper wires between the following pins

  • UART1_RXD(L3) J1/J3 PIN-3 --— UART4_TXD(C9) J6/J8 PIN-58
  • UART1_TXD(M3) J1/J3 PIN-4 --— UART4_RXD(A10) J5/J7 PIN-47

Supported Combinations

Parameter Value
CPU + OS r5fss0-0 nortos
Toolchain ti-arm-clang
Boards am263x-cc, am263x-lp
Example folder examples/drivers/uart/uart_hld_lld_external_loopback

Steps to Run the Example

See Also

UART

Sample Output

Shown below is a sample output when the application is run, Please note that application prints in CCS console.

CCS Console:

[UART] example started ...
This is uart test with HLD-LLD instances
All tests have passed!!