Introduction
This example demonstrates setting of multiple LED at the same time connected to the same I2C controller. The application will blink all the I2C controlled LED in the EVM.
Application blinks leds for 3 loops in interrupt mode and 3 loops in polling mode. Application exits after 6 iterations.
Supported Combinations
| Parameter | Value |
| CPU + OS | r5fss0-0 nortos |
| Toolchain | ti-arm-clang |
| Boards | am263x-cc, am263x-lp |
| Example folder | examples/drivers/i2c/i2c_led_blink |
AM263X-CC
- Watch out for LEDs LD2, LD3, LD4, LD5, LD6, LD7, LD8, LD9, LD10, LD11 on the CC to blink which is controlled by I2C2.
AM263X-LP
- Watch out for LED D7, D8, D9, D10, D11, D12, D13, D14 on the LP to blink which is controlled by I2C1.
Steps to Run the Example
See Also
I2C Low Level Driver
Sample Output
Shown below is a sample output when the application is run,
[I2C] LED Read Write Test Started ...
LED will Blink for 3 loop in polling Mode ...
LED will Blink for 3 loop in interrupt Mode ...
All tests have passed!!