Introduction
This example configures a GPIO pin connected to an LED on the EVM in output mode. The application toggles the LED on/off for 10 seconds and exits.
Supported Combinations
| Parameter | Value |
| CPU + OS | r5fss0-0 nortos |
| Toolchain | ti-arm-clang |
| Board | am263x-cc, am263x-lp |
| Example folder | examples/drivers/gpio/gpio_led_blink/ |
Steps to Run the Example
AM263X-CC
- Watch out for LED LD13 on the CC to blink which is controlled by GPIO0_1.
AM263X-LP
- Watch out for LED DS2 on the LP to blink which is controlled by GPIO0_26.
See Also
GPIO
Sample Output
Shown below is a sample output when the application is run,
GPIO LED Blink Test Started ...
LED will Blink for 10 seconds ...
GPIO LED Blink Test Passed!!
All tests have passed!!