Introduction
This example demonstrates EPWM tripping through ADC limit detection PPB block. ADC0INT1 is configured to periodically trigger the ADC0 channel 2 post initial software forced trigger. The limit detection post-processing block(PPB) is configured and if the ADC results are outside of the defined range, the post-processing block will generate an ADCxEVTy event. This event is configured as EPWM trip source through configuring EPWM XBAR and corresponding EPWM’s trip zone and digital compare sub-modules. The example showcases one-shot, cycle-by-cycle and direct tripping of PWMs through ADCAEVT1 source via Digital compare submodule. DAC is configured to generate a ramp waveform and its output is connected as ADC input. PWM tripping is validated by reading different trip flags.
- Note
- The ADC EVT routing the Outputxbar in AM263x is missing. Hence in order to bring the ADC EVT to GPIO, we can follow other routes such as routing.
- ADC EVT is typically paired usage with Tripping the EPWMs. We can route the ADC EVT to PWMxbar, to DCEVT(A/B)(1/2) to Trip Zone TripOut to Outputxbar. Note that it can be a OST or CBC, but then the ADCEVT is now latched instead of its actual status. So, forward the DCEVT(A/B)(1/2) as is to the tripzone. The example showcases this routing.
Module Block diagram
The example does the below
- Configures SOC0 of ADC0 to read from Channel 2 and ADC0INT1 to periodically trigger conversions after the initial software forced trigger.
- ADC PPB is configured to generate ADC EVT1 if ADC results are outside the range.
- ADC Event is configured as EPWM trip source through EPWM XBAR.
- Trip Zone and Digital Compare submodule are configured to enable different trip combinations.
- EPWM0 (EPWM2 in case of AM261x-LP) is configured for One Shot trip.
- EPWM1 (EPWM3 in case of AM261x-LP) is configured for Cycle by Cycle trip.
- EPWM2 (EPWM4 in case of AM261x-LP) is configured for Direct trip via Digital compare submodule.
- The ramp waveform on DAC output is routed to ADC input.
- The watch variables storing ADC conversion outputs can be used to view the results.
- ADC EVT is routed via OutputXbar to GPIO
Watch Variables
- adc0Result2 - Digital representation of the voltage on pin ADC0_AIN2
External Connections
- ADC0_AIN2 pin should be connected to DAC output pin.
- EPWM0A, EPWM0B, EPWM1A, EPWM1B, EPWM2A, EPWM2B can be connected to an oscilloscope to validate tripping.
- In case of AM261x-LP, these are EPWM 2A/B, 3A/B, 4A/B respectively
AM263PX-CC E2
When using AM263Px-CC with TMDSHSECDOCK (HSEC180 controlCARD Baseboard Docking Station)
- Connect HSEC Pin 15 (ADC input) to HSEC Pin 9 (DAC out)
- Capture and analyze waveforms at HSEC Pin 49, HSEC Pin 51, HSEC Pin 53, HSEC Pin 55, HSEC Pin 50, HSEC Pin 52
- Observe ADC EVT via Output Xbar on HSEC Pin 85
AM263X-CC E2 or AM263X-CC E1 or AM261X-SOM E1
When using AM263x-CC with TMDSHSECDOCK (HSEC180 controlCARD Baseboard Docking Station)
- Connect HSEC Pin 15 (ADC input) to HSEC Pin 9 (DAC out)
- Capture and analyze waveforms at HSEC Pin 49, HSEC Pin 51, HSEC Pin 53, HSEC Pin 55, HSEC Pin 50, HSEC Pin 52
- Observe ADC EVT via PWMXbar - DCEVT - Output Xbar on HSEC Pin 85
AM263PX-LP
When using AM263Px-LP
- Connect booster pack header J5/J7 pin 66 (ADC input) to J1/J3 pin 30 (DAC out)
- Capture and analyze waveforms at booster pack header J2/J4 pin 11, J6/J8 pin 59, J2/J4 pin 37, J2/J4 pin 38, J2/J4 pin 39, J2/J4 pin 40.
- Observe ADC EVT via Output Xbar on J5.50
AM263X-LP
When using AM263x-LP
- Connect booster pack header J5/J7 pin 66 (ADC input) to J1/J3 pin 30 (DAC out)
- Capture and analyze waveforms at booster pack header J2/J4 pin 11, J6/J8 pin 59, J2/J4 pin 37, J2/J4 pin 38, J2/J4 pin 39, J2/J4 pin 40.
- Observe ADC EVT via PWMXbar - DCEVT - Output Xbar on J5.58
AM261X-LP
When using AM261x-LP
- Connect booster pack header J7 pin 63 (ADC input) to J3 pin 30 (DAC out) | note for these pins refer to IO Expander configurations on Schematics and syscfg
- Capture and analyze waveforms at booster pack header
- EPWM 2A / 2B J4 pin 40/39
- EPWM 3A / 3B J4 pin 38/37
- EPWM 4A / 4B J4 pin 36/35
- Observe ADC EVT via Output Xbar on J6.51
Supported Combinations
| Parameter | Value |
| CPU + OS | r5fss0-0 nortos |
| Toolchain | ti-arm-clang |
| Board | am263x-cc, am263x-lp |
| Example folder | examples/drivers/adc/adc_ppb_epwm_trip/ |
Steps to Run the Example
- When using CCS projects to build, import the CCS project for the required combination and build it using the CCS project menu (see Using SDK with CCS Projects).
- When using makefiles to build, note the required combination and build using make command (see Using SDK with Makefiles)
- Establish connections as mentioned in External Connections section
- Launch a CCS debug session and run the executable, see CCS Launch, Load and Run
- Using the watch variables, view the ADC conversion results.
- Observe 6 EPWM waveforms. After ADC input voltage exceeds the PPB limit, PWMs get tripped.
See Also
ADC
Sample Output
Shown below is a sample output when the application is run,
ADC PPB ePWM Trip Test Started ...
ADC PPB ePWM Trip Test Passed!!
All tests have passed!!
Sample Output Capture