AM263x MCU+ SDK  11.00.00
MMCSD Low Level Driver

Note
EMMC Flash card is not available in AM263X board.

Multi-Media Card Secure Digital (MMCSD) peripheral is a driver which provides an interface with storage devices which follows MMC/SD/SDIO protocol. The driver supports single bit and four bit data lines to communicate with the connected media. The MMCSD controller provides accessibility to external MMC/SD/SDIO devices using a programmed IO method. There is only one MMCSD module inside the SOC - MMCSD0.

Features Supported

  • 64-bit data, address width System Bus Interface
  • SD command/response sets as defined in the SD Physical Layer specification v2.00
  • Operating voltage range VCC = 3.3 V
  • Default-speed & High-speed MMCSD protocol.

SysConfig Features

Note
It is strongly recommend to use SysConfig where it is available instead of using direct SW API calls. This will help simplify the SW application and also catch common mistakes early in the development cycle.

Features not Supported

  • No integrated DMA Controller Support.
  • MMCSD instance does not support DDR mode.

Usage Overview

API Sequence

To use the MMCSD LLD driver to write/read data to or from a MMC/SD Device, the application calls the following APIs:

Initializing the MMCSD LLD Driver

MMCSD_lld_init() must be called before any other MMCSD APIs. This function uses mmcsd lld handle to initialize each instance.

Calling MMCSD_lld_init() a second time with the same handle previously passed to MMCSD_lld_init() will result in an error. You can, though, re-use the handle if the instance is closed via MMCSD_lld_deInit().

Please note that initializing MMCSD LLD driver is taken care by the SysConfig generated code.

MMCSD Transfer Mode

The MMCSD driver supports two transfer modes of operation: Polling and Interrupt Mode.

In Polling mode transfer can be initiated with all the polling mode APIs.

In Interrupt mode Users have to register the appropriate ISR and assign a callback function before calling the interrupt mode APIs.

DMA can enabled in any mode of operation if enabled.

Example Usage

Include the below file to access the APIs

#include <string.h>
#include <kernel/dpl/MutexArmP.h>
#include <kernel/nortos/dpl/r5/HwiP_armv7r_vim.h>

Instance Open Example

int32_t status = MMCSD_STS_SUCCESS;
gMmcsdLldHandle = (MMCSDLLD_Handle)(&gMmcsdLldObject);
gMmcsdLldHandle->initHandle = (MMCSDLLD_InitHandle)(&gMmcsdLldInitObject);
status = MMCSD_lld_init(gMmcsdLldHandle);

Instance Close Example

int32_t status = MMCSD_STS_SUCCESS;
status = MMCSD_lld_deInit(gMmcsdLldHandle);

Non-Blocking Transfer Example

gMmcsdLldHandle = (MMCSDLLD_Handle)(gMmcsdLldHandle);
intrNum = gMmcsdLldHandle->initHandle->intrNum;
intcBaseAddr = gHwiConfig.intcBaseAddr;
gMmcsdVimStsAddr = intcBaseAddr + (0x404u + (((intrNum)>> 5) & 0xFu)*0x20u);
gMmcsdVimStsClrMask = 0x1u << ((intrNum) & 0x1Fu);
/* Assign Transfer Complete Callback Function */
gMmcsdLldHandle->transferCompleteCallback = MMCSD_lld_transferCompleteCallback_implementation;
/* Register Interrupt */
HwiP_setVecAddr(intrNum, (uintptr_t)&App_MMCSD_ISR);
HwiP_setPri(intrNum, MMCSD_INTERRUPT_PRIORITY);
HwiP_enableInt(intrNum);
int32_t status = MMCSD_STS_SUCCESS;
uint32_t blockSize = MMCSD_lld_getBlockSize(gMmcsdLldHandle);
uint32_t numBlocks = APP_MMCSD_DATA_SIZE / blockSize;
if((APP_MMCSD_DATA_SIZE % blockSize) != 0)
{
numBlocks += 1;
}
/* Fill Write and Read Buffer */
mmcsd_io_fill_buffers();
/* Lock Mutex */
gMMCSDTransferMutex = MUTEX_ARM_LOCKED;
/* Initiate Transfer */
status = MMCSD_lld_write_SD_Intr(gMmcsdLldHandle, gMmcsdTxBuf,
APP_MMCSD_START_BLK, numBlocks);
/* Wait for Mutex to unlock */
while(try_lock_mutex(&gMMCSDTransferMutex) == MUTEX_ARM_LOCKED);

Non-Blocking Example transfer callback

void MMCSD_lld_transferCompleteCallback_implementation (void * args,
int32_t transferStatus)
{
unlock_mutex(&gMMCSDTransferMutex);
}

Non-Blocking Example ISR CALL callback

static __attribute__((__section__(".text.hwi"), noinline, naked, target("arm"), aligned(4))) void App_MMCSD_ISR(void)
{
ISR_CALL_LEVEL_NONFLOAT_REENTRANT(MMCSD_lld_Isr, \
gMmcsdLldHandle, \
intrNum, \
gMmcsdVimStsAddr, \
gMmcsdVimStsClrMask,
intcBaseAddr);
}

API

APIs for MMCSD LLD

args
void * args
Definition: hsmclient_msg.h:4
MMCSD_lld_Isr
void MMCSD_lld_Isr(void *args)
This is the MMCSD Controller ISR and can be used as IRQ handler.
MMCSD_lld_deInit
int32_t MMCSD_lld_deInit(MMCSDLLD_Handle handle)
This API De-Initializes the MMCSD instance.
MMCSD_lld_write_SD_Intr
int32_t MMCSD_lld_write_SD_Intr(MMCSDLLD_Handle handle, uint8_t *buf, uint32_t startBlk, uint32_t numBlks)
Function to perform block writes to the SD media in Interrupt Mode.
__attribute__
struct lld_sockaddr __attribute__
This is the SecureBoot Stream type which holds the data for a specific bootloader to HSM call....
HwiP_enableInt
void HwiP_enableInt(uint32_t intNum)
Enable a specific interrupt.
MMCSDLLD_InitHandle
struct MMCSDLLD_InitObject * MMCSDLLD_InitHandle
MMCSD_lld_init
int32_t MMCSD_lld_init(MMCSDLLD_Handle handle)
This API Initializes the MMCSD instance.
DebugP.h
MMCSDLLD_Handle
struct MMCSDLLD_Object * MMCSDLLD_Handle
MMCSD_lld_getBlockSize
uint32_t MMCSD_lld_getBlockSize(MMCSDLLD_Handle handle)
This function returns the block size of the MMC/SD media connected to the MMCSD controller.
mmcsd.h
MMCSD Driver API/interface file.
MMCSD_STS_SUCCESS
#define MMCSD_STS_SUCCESS
Return status when the API execution was successful.
Definition: mmcsd_lld.h:86
DebugP_assert
#define DebugP_assert(expression)
Function to call for assert check.
Definition: DebugP.h:177