AM263x MCU+ SDK  08.06.00
MMCSD_ioDelayParams Struct Reference

Data Fields

uint32_t deviceType
 
uint32_t transferSpeed
 
uint32_t operatingVoltage
 
uint32_t loopBackType
 

Field Documentation

◆ deviceType

uint32_t MMCSD_ioDelayParams::deviceType

MMC device type

◆ transferSpeed

uint32_t MMCSD_ioDelayParams::transferSpeed

MMC transfer speed

◆ operatingVoltage

uint32_t MMCSD_ioDelayParams::operatingVoltage

MMC peripheral operating voltage

◆ loopBackType

uint32_t MMCSD_ioDelayParams::loopBackType

MMC peripheral loop back type