AM263x MCU+ SDK  08.06.00
EnetPhy_C45WriteRegInArgs Struct Reference

Detailed Description

Input args for ENET_PHY_IOCTL_C45_WRITE_REG command.

Data Fields

Enet_MacPort macPort
 
uint8_t mmd
 
uint16_t reg
 
uint16_t val
 

Field Documentation

◆ macPort

Enet_MacPort EnetPhy_C45WriteRegInArgs::macPort

Port number

◆ mmd

uint8_t EnetPhy_C45WriteRegInArgs::mmd

MMD

◆ reg

uint16_t EnetPhy_C45WriteRegInArgs::reg

Register address

◆ val

uint16_t EnetPhy_C45WriteRegInArgs::val

Value to be written