AM263x MCU+ SDK  08.06.00

Detailed Description

MAC authentication configuration.

Data Fields

bool authModeEn
 
uint32_t macAuthDisMask
 

Field Documentation

◆ authModeEn

bool CpswAle_MacAuthCfg::authModeEn

Enable MAC Authorization mode

◆ macAuthDisMask

uint32_t CpswAle_MacAuthCfg::macAuthDisMask

Disable Port authorization - When set will allow unknown addresses to arrive on a switch in authorization mode. It is intended for device to device network connection on ports which do not require MACSEC encryption