Bootloader driver configuration, these are filled by SysCfg based on the boot media selected.
Data Fields | |
| Bootloader_Fxns * | fxns |
| void * | args |
| uint32_t | bootMedia |
| uint32_t | bootImageSize |
| uint32_t | coresPresentMap |
| uint8_t * | scratchMemPtr |
| void * | socCoreOpMode |
| Bootloader_Fxns* Bootloader_Config::fxns |
| void* Bootloader_Config::args |
| uint32_t Bootloader_Config::bootMedia |
| uint32_t Bootloader_Config::bootImageSize |
| uint32_t Bootloader_Config::coresPresentMap |
| uint8_t* Bootloader_Config::scratchMemPtr |
| void* Bootloader_Config::socCoreOpMode |