AM263x MCU+ SDK  08.06.00
sdl_exception_priv.h
Go to the documentation of this file.
1 /*
2  * SDL EXCEPTION
3  *
4  * Software Diagnostics Library module for handling exceptions
5  *
6  * Copyright (c) Texas Instruments Incorporated 2022
7  *
8  * Redistribution and use in source and binary forms, with or without
9  * modification, are permitted provided that the following conditions
10  * are met:
11  *
12  * Redistributions of source code must retain the above copyright
13  * notice, this list of conditions and the following disclaimer.
14  *
15  * Redistributions in binary form must reproduce the above copyright
16  * notice, this list of conditions and the following disclaimer in the
17  * documentation and/or other materials provided with the
18  * distribution.
19  *
20  * Neither the name of Texas Instruments Incorporated nor the names of
21  * its contributors may be used to endorse or promote products derived
22  * from this software without specific prior written permission.
23  *
24  * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS
25  * "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT
26  * LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR
27  * A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT
28  * OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL,
29  * SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT
30  * LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE,
31  * DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY
32  * THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT
33  * (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE
34  * OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
35  *
36  */
37 
38 #ifndef INCLUDE_SDL_ECC_EXCEPTION_PRIV_H_
39 #define INCLUDE_SDL_ECC_EXCEPTION_PRIV_H_
40 
41 #include <stdint.h>
42 
48 typedef struct SDL_EXCEPTION_Instance_s
49 {
54  void *paramPtr;
57 
58 #endif /* INCLUDE_SDL_ECC_EXCEPTION_PRIV_H_ */
SDL_EXCEPTION_Instance_t::callbackFunctions
SDL_EXCEPTION_CallbackFunctions_t callbackFunctions
Definition: sdl_exception_priv.h:50
SDL_EXCEPTION_Instance_t::paramPtr
void * paramPtr
Definition: sdl_exception_priv.h:54
SDL_EXCEPTION_ECCCallback_t
void(* SDL_EXCEPTION_ECCCallback_t)(uint32_t intSource, uint32_t errorAddr, uint32_t ramId, uint64_t bitErrorOffset, uint32_t bitErrorGroup)
Format of Call back function for ECC error events.
Definition: sdl_exception.h:63
SDL_EXCEPTION_CallbackFunctions_t
Structure of call back functions for various exception events.
Definition: sdl_exception.h:74
SDL_EXCEPTION_Instance_t
Definition: sdl_exception_priv.h:49
SDL_EXCEPTION_Instance_t::ECCCallBackFunction
SDL_EXCEPTION_ECCCallback_t ECCCallBackFunction
Definition: sdl_exception_priv.h:52