This file contains the SDL DPL API's.
Provides the APIs for DPL.
Go to the source code of this file.
Data Structures | |
| struct | SDL_DPL_HwipParams |
| This structure contains the parameters for interrupt registration through the SDL DPL interface. More... | |
| struct | SDL_DPL_Interface |
| This structure contains the pointers for the DPL interfaces provided by the application to SDL_DPL_init. More... | |
Typedefs | |
| typedef void(* | pSDL_DPL_InterruptCallbackFunction) (void *arg) |
| Prototype for the interrupt callback function. More... | |
| typedef void * | pSDL_DPL_HwipHandle |
| typedef int32_t(* | pSDL_DPL_InterruptFunction) (int32_t intNum) |
| Prototype for the interrupt enable/disable functions. More... | |
| typedef pSDL_DPL_HwipHandle(* | pSDL_DPL_RegisterFunction) (SDL_DPL_HwipParams *pParams) |
| Prototype for the interrupt registration function. More... | |
| typedef int32_t(* | pSDL_DPL_DeregisterFunction) (pSDL_DPL_HwipHandle handle) |
| Prototype for the interrupt de-register function. More... | |
| typedef int32_t(* | pSDL_DPL_DelayFunction) (int32_t ndelay) |
| Prototype for the delay function. More... | |
| typedef void *(* | pSDL_DPL_AddrTranslateFunction) (uint64_t addr, uint32_t size) |
| Prototype for address translation function. More... | |
Functions | |
| int32_t | SDL_DPL_init (SDL_DPL_Interface *dplInterface) |
| DPL init. More... | |
| int32_t | SDL_DPL_enableInterrupt (int32_t intNum) |
| DPL enable interrupt. More... | |
| int32_t | SDL_DPL_disableInterrupt (int32_t intNum) |
| DPL disable interrupt. More... | |
| int32_t | SDL_DPL_registerInterrupt (SDL_DPL_HwipParams *pParams, pSDL_DPL_HwipHandle *handle) |
| DPL register interrupt. More... | |
| int32_t | SDL_DPL_deregisterInterrupt (pSDL_DPL_HwipHandle handle) |
| DPL deregister interrupt. More... | |
| int32_t | SDL_DPL_delay (int32_t ndelay) |
| DPL delay. More... | |
| void * | SDL_DPL_addrTranslate (uint64_t addr, uint32_t size) |
| DPL Address translation function. More... | |