AM263x MCU+ SDK  08.06.00
mmcsd/v1/mmcsd.h File Reference

Introduction

MMCSD Driver API/interface file.

Go to the source code of this file.

Data Structures

struct  MMCSD_sysCfg
 Structure holding the hs mmcsd controller system configurations. More...
 
struct  MMCSD_cmd
 Structure for MMCSD command. More...
 
struct  MMCSD_cmdObj
 Structure holding the hs mmcsd controller command object. More...
 
struct  MMCSD_ioDelayParams
 
struct  MMCSD_Params
 
struct  MMCSD_EmmcDeviceData
 eMMC device properties More...
 
struct  MMCSD_SdDeviceData
 SD device properties. More...
 
struct  MMCSD_Transaction
 MMCSD transaction. More...
 
struct  MMCSD_Attrs
 MMCSD instance attributes - used during init time. More...
 
struct  MMCSD_Object
 MMCSD driver object. More...
 
struct  MMCSD_Config
 

Macros

#define MMCSD_CARD_SD   (0U)
 Determines the type of card is SD. More...
 
#define MMCSD_CARD_MMC   (1U)
 Determines the type of card is MMC. More...
 
#define MMCSD_CARD_EMMC   (2U)
 Determines the type of card is MMC. More...
 
#define MMCSD_CARD_TYPE_NO_DEVICE   (3U)
 
#define MMCSD_CMD_SETBUSWIDTH   (MMCSD_CMD_RESERVED + 0U)
 Set bus width of MMCSD. More...
 
#define MMCSD_CMD_SETFREQUENCY   (MMCSD_CMD_RESERVED + 1U)
 Set bus frequency of MMCSD. More...
 
#define MMCSD_CMD_GETBUSWIDTH   (MMCSD_CMD_RESERVED + 2U)
 Get bus width of MMCSD. More...
 
#define MMCSD_CMD_GETFREQUENCY   (MMCSD_CMD_RESERVED + 3U)
 Get bus frequency of MMCSD. More...
 
#define MMCSD_CMD_GETMEDIAPARAMS   (MMCSD_CMD_RESERVED + 4U)
 Get media (SD/eMMC/MMC) parameters. More...
 
#define MMCSD_INVALID_MUXNUM   (-1)
 Invalid Mux num. More...
 
#define MMCSD_INVALID_MUX_EVENTNUM   (-1)
 Invalid Mux In/Out event num. More...
 
#define MMCSD_BUS_WIDTH_1BIT   (1U)
 Card bus width configuration for 1-bit mode. More...
 
#define MMCSD_BUS_WIDTH_4BIT   (4U)
 Card bus width configuration for 4-bit mode. More...
 
#define MMCSD_BUS_WIDTH_8BIT   (8U)
 Card bus width configuration for 8-bit mode. More...
 
#define MMCSD_TRANSPEED_25MBPS   (0x32U)
 Card bus frequency configuration for 25 Mbps. More...
 
#define MMCSD_TRANSPEED_50MBPS   (0x5AU)
 Card bus frequency configuration for 50 Mbps. More...
 
#define MMCSD_TRANSPEED_DEFAULT   (0x32U)
 Card bus frequency configuration for 25 Mbps. More...
 
#define MMCSD_TRANSPEED_HS   (0x5AU)
 Card bus frequency configuration for 50 Mbps. More...
 
#define MMCSD_TRANSPEED_SDR12   (0x32U)
 Card bus frequency configuration for 25 Mbps. More...
 
#define MMCSD_TRANSPEED_SDR25   (0x5AU)
 Card bus frequency configuration for 50 Mbps. More...
 
#define MMCSD_TRANSPEED_SDR50   (0xBU)
 Card bus frequency configuration for 100 Mbps. More...
 
#define MMCSD_TRANSPEED_SDR104   (0x2BU)
 Card bus frequency configuration for 200 Mbps. More...
 
#define MMCSD_TRANSPEED_DDR50   (0x3BU)
 Card bus frequency configuration for 100 Mbps. More...
 
#define MMCSD_TRANSPEED_HS200   (0x2BU)
 Card bus frequency configuration for 200 Mbps. More...
 
#define MMCSD_LOOPBACK_ANY   (0x0U)
 MMC any loop back. More...
 
#define MMCSD_LOOPBACK_INTERNAL   (0x1U)
 MMC internal loop back. More...
 
#define MMCSD_LOOPBACK_PAD   (0x2U)
 MMC pad loop back. More...
 
#define MMCSD_VOLTAGE_ANY   (0x0U)
 MMC any operating voltage. More...
 

Typedefs

typedef void * MMCSD_Handle
 
typedef int32_t(* MMCSD_iodelayFxn) (uint32_t instanceNum, MMCSD_ioDelayParams *iodelayParams)
 Return status of MMCSD. More...
 
typedef int32_t(* MMCSD_switchVoltage) (uint32_t controllerNum, MMCSD_BusVoltage voltage)
 A function pointer to set the voltage of the MMC I/O Cells and PBAIS to the desired voltage. More...
 
typedef uint32_t(* MMCSD_inputClockControl) (uint32_t instNum, uint32_t *clkFreq, MMCSD_inputClkCtrlMode_e)
 A function pointer to read/configure the input clock to the MMC controller. More...
 

Enumerations

enum  MMCSD_resetLineMask { MMCSD_RESET_LINE_MASK_DATA = CSL_MMC_SYSCTL_SRD_MASK, MMCSD_RESET_LINE_MASK_CMD = CSL_MMC_SYSCTL_SRC_MASK, MMCSD_RESET_LINE_MASK_ALL = CSL_MMC_SYSCTL_SRA_MASK }
 MMCSD instance attributes - used during init time. More...
 
enum  MMCSD_clkAct { MMCSD_CLK_ACT_ICLK_FCLK_OFF = CSL_MMC_SYSCONFIG_CLOCKACTIVITY_NONE, MMCSD_CLK_ACT_FCLK_OFF = CSL_MMC_SYSCONFIG_CLOCKACTIVITY_FUNC, MMCSD_CLK_ACT_ICLK_OFF = CSL_MMC_SYSCONFIG_CLOCKACTIVITY_OCP, MMCSD_CLK_ACT_ICLK_FLCK_ON = CSL_MMC_SYSCONFIG_CLOCKACTIVITY_BOTH }
 Enumerates the clock activity configurations during wake up . More...
 
enum  MMCSD_standbyMode { MMCSD_STANDBY_MODE_FORCE = CSL_MMC_SYSCONFIG_STANDBYMODE_FORCE, MMCSD_STANDBY_MODE_NONE = CSL_MMC_SYSCONFIG_STANDBYMODE_NOIDLE, MMCSD_STANDBY_MODE_SMART = CSL_MMC_SYSCONFIG_STANDBYMODE_SMART, MMCSD_STANDBY_MODE_SMART_WAKEUP }
 Enumerates the standby modes. More...
 
enum  MMCSD_pwrCtrl { MMCSD_PWR_CTRL_ON = CSL_MMC_HCTL_SDBP_PWRON, MMCSD_PWR_CTRL_OFF = CSL_MMC_HCTL_SDBP_PWROFF }
 Enumerates macros to configure power on/off. More...
 
enum  MMCSD_suppVolt { MMCSD_SUPP_VOLT_1P8 = CSL_MMC_CAPA_VS18_MASK, MMCSD_SUPP_VOLT_3P0 = CSL_MMC_CAPA_VS30_MASK, MMCSD_SUPP_VOLT_3P3 = CSL_MMC_CAPA_VS33_MASK }
 Enumerates the list of supported bus voltages. More...
 
enum  MMCSD_cmdType { MMCSD_CMD_TYPE_OTHER = CSL_MMC_CMD_CMD_TYPE_NORMAL, MMCSD_CMD_TYPE_BUS_SUSPEND = CSL_MMC_CMD_CMD_TYPE_SUSPEND, MMCSD_CMD_TYPE_FUNC_SEL = CSL_MMC_CMD_CMD_TYPE_RESUME, MMCSD_CMD_TYPE_IO_ABORT = CSL_MMC_CMD_CMD_TYPE_ABORT }
 Enumerates the list of command types. More...
 
enum  MMCSD_rspType { MMCSD_RSP_TYPE_NONE = CSL_MMC_CMD_RSP_TYPE_NORSP, MMCSD_RSP_TYPE_LEN_136 = CSL_MMC_CMD_RSP_TYPE_LGHT36, MMCSD_RSP_TYPE_LEN_48 = CSL_MMC_CMD_RSP_TYPE_LGHT48, MMCSD_RSP_TYPE_LEN_48_BUSY = CSL_MMC_CMD_RSP_TYPE_LGHT48B }
 Enumerates the list of response types. More...
 
enum  MMCSD_xFerType { MMCSD_XFER_TYPE_TX = CSL_MMC_CMD_DDIR_WRITE, MMCSD_XFER_TYPE_RX = CSL_MMC_CMD_DDIR_READ }
 Enumerates the list of response types. More...
 
enum  MMCSD_intrMask {
  MMCSD_INTR_MASK_BADACCESS = CSL_MMC_IE_BADA_ENABLE_MASK, MMCSD_INTR_MASK_CARDERROR = CSL_MMC_IE_CERR_ENABLE_MASK, MMCSD_INTR_MASK_ADMAERROR = CSL_MMC_IE_ADMAE_ENABLE_MASK, MMCSD_INTR_MASK_ACMD12ERR = CSL_MMC_IE_ACE_ENABLE_MASK,
  MMCSD_INTR_MASK_DATABITERR = CSL_MMC_IE_DEB_ENABLE_MASK, MMCSD_INTR_MASK_DATACRCERR = CSL_MMC_IE_DCRC_ENABLE_MASK, MMCSD_INTR_MASK_DATATIMEOUT = CSL_MMC_IE_DTO_ENABLE_MASK, MMCSD_INTR_MASK_CMDINDXERR = CSL_MMC_IE_CIE_ENABLE_MASK,
  MMCSD_INTR_MASK_CMDBITERR = CSL_MMC_IE_CEB_ENABLE_MASK, MMCSD_INTR_MASK_CMDCRCERR = CSL_MMC_IE_CCRC_ENABLE_MASK, MMCSD_INTR_MASK_CMDTIMEOUT = CSL_MMC_IE_CTO_ENABLE_MASK, MMCSD_INTR_MASK_ERR = CSL_MMC_IE_NULL_MASK,
  MMCSD_INTR_MASK_CARDREM = CSL_MMC_IE_CREM_ENABLE_MASK, MMCSD_INTR_MASK_CARDINS = CSL_MMC_IE_CINS_ENABLE_MASK, MMCSD_INTR_MASK_BUFRDRDY = CSL_MMC_IE_BRR_ENABLE_MASK, MMCSD_INTR_MASK_BUFWRRDY = CSL_MMC_IE_BWR_ENABLE_MASK,
  MMCSD_INTR_MASK_TRNFCOMP = CSL_MMC_IE_TC_ENABLE_MASK, MMCSD_INTR_MASK_CMDCOMP = CSL_MMC_IE_CC_ENABLE_MASK
}
 Enumerates the controller's interrupt masks. More...
 
enum  MMCSD_idleMode { MMCSD_IDLE_MODE_FORCE = CSL_MMC_SYSCONFIG_SIDLEMODE_FORCE, MMCSD_IDLE_MODE_NONE = CSL_MMC_SYSCONFIG_SIDLEMODE_NOIDLE, MMCSD_IDLE_MODE_SMART = CSL_MMC_SYSCONFIG_SIDLEMODE_SMART }
 Enumerates the idle modes. More...
 
enum  MMCSD_busVolt { MMCSD_BUS_VOLT_1P8 = CSL_MMC_HCTL_SDVS__1V8, MMCSD_BUS_VOLT_3P0 = CSL_MMC_HCTL_SDVS__3V0, MMCSD_BUS_VOLT_3P3 = CSL_MMC_HCTL_SDVS__3V3 }
 Enumerates mmc sd controller's bus voltages. More...
 
enum  MMCSD_BusVoltage { MMCSD_BUS_VOLTAGE_1_8V = 0x1U, MMCSD_BUS_VOLTAGE_3_0V = 0x2U, MMCSD_BUS_VOLTAGE_3_3V = 0x4U }
 
enum  MMCSD_inputClkCtrlMode_e { MMCSD_INPUT_CLOCK_CTRL_GET, MMCSD_INPUT_CLOCK_CTRL_SET }
 ENUMs to read/configure the input clock to the MMC controller. More...
 

Functions

void MMCSD_init (void)
 This function initializes the MMCSD module. More...
 
void MMCSD_deinit (void)
 This function de-initializes the MMCSD module. More...
 
void MMCSD_Params_init (MMCSD_Params *mmcsdParams)
 Initialize data structure with defaults. More...
 
MMCSD_Handle MMCSD_open (uint32_t index, const MMCSD_Params *openParams)
 This function opens a given MMCSD peripheral. More...
 
void MMCSD_close (MMCSD_Handle handle)
 Function to close a MMCSD peripheral specified by the MMCSD handle. More...
 
MMCSD_Handle MMCSD_getHandle (uint32_t index)
 This function returns the handle of an open MMCSD Instance from the instance index. More...
 
int32_t MMCSD_read (MMCSD_Handle handle, uint8_t *buf, uint32_t startBlk, uint32_t numBlks)
 Function to perform block reads from the MMC/SD media. More...
 
int32_t MMCSD_write (MMCSD_Handle handle, uint8_t *buf, uint32_t startBlk, uint32_t numBlks)
 Function to perform block writes to the MMC/SD media. More...
 
uint32_t MMCSD_getBlockSize (MMCSD_Handle handle)
 This function returns the block size of the MMC/SD media connected to the MMCSD controller. More...
 
uint32_t MMCSD_getBlockCount (MMCSD_Handle handle)
 This function returns the block count of User Data Area of the MMC/SD media connected to the MMCSD controller. More...
 

Variables

MMCSD_Config gMmcsdConfig []
 Externally defined driver configuration array. More...
 
uint32_t gMmcsdConfigNum
 Externally defined driver configuration array size. More...