AM263x MCU+ SDK  08.06.00
mcspi_dma_edma.h
Go to the documentation of this file.
1 /*
2  * Copyright (C) 2022-2023 Texas Instruments Incorporated
3  *
4  * Redistribution and use in source and binary forms, with or without
5  * modification, are permitted provided that the following conditions
6  * are met:
7  *
8  * Redistributions of source code must retain the above copyright
9  * notice, this list of conditions and the following disclaimer.
10  *
11  * Redistributions in binary form must reproduce the above copyright
12  * notice, this list of conditions and the following disclaimer in the
13  * documentation and/or other materials provided with the
14  * distribution.
15  *
16  * Neither the name of Texas Instruments Incorporated nor the names of
17  * its contributors may be used to endorse or promote products derived
18  * from this software without specific prior written permission.
19  *
20  * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS
21  * "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT
22  * LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR
23  * A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT
24  * OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL,
25  * SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT
26  * LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE,
27  * DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY
28  * THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT
29  * (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE
30  * OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
31  */
32 
33 #ifndef MCSPI_DMA_EDMA_H_
34 #define MCSPI_DMA_EDMA_H_
35 
36 #include <stdint.h>
37 #include <drivers/edma.h>
38 
39 #ifdef __cplusplus
40 extern "C"
41 {
42 #endif
43 
44 typedef struct McspiDma_EdmaArgs_s
45 {
46  void *drvHandle;
49 
50 typedef struct MCSPI_DmaChConfig_s
51 {
52  uint32_t edmaTccRx;
54  uint32_t edmaTccTx;
56  uint32_t edmaRxChId;
58  uint32_t edmaTxChId;
60  uint32_t edmaRxParam;
62  uint32_t edmaTxParam;
64  uint32_t edmaDummyParam;
66  uint32_t edmaRegionId;
68  uint32_t edmaBaseAddr;
74  uint32_t isOpen;
77 
78 #ifdef __cplusplus
79 }
80 #endif
81 
82 #endif /* MCSPI_DMA_EDMA_H_ */
MCSPI_DmaChConfig
Definition: mcspi_dma_edma.h:51
MCSPI_DmaChConfig::edmaDummyParam
uint32_t edmaDummyParam
Definition: mcspi_dma_edma.h:64
MCSPI_DmaChConfig::edmaBaseAddr
uint32_t edmaBaseAddr
Definition: mcspi_dma_edma.h:68
MCSPI_DmaChConfig::edmaIntrObjRx
Edma_IntrObject edmaIntrObjRx
Definition: mcspi_dma_edma.h:70
Edma_IntrObject
EDMA interrupt configuration object. The object is passed to the EDMA_registerIntr() function....
Definition: edma/v0/edma.h:479
MCSPI_DmaChConfig::edmaTxChId
uint32_t edmaTxChId
Definition: mcspi_dma_edma.h:58
MCSPI_DmaChConfig::edmaRegionId
uint32_t edmaRegionId
Definition: mcspi_dma_edma.h:66
edma.h
McspiDma_EdmaArgs
Definition: mcspi_dma_edma.h:45
MCSPI_DmaChConfig::edmaTccTx
uint32_t edmaTccTx
Definition: mcspi_dma_edma.h:54
MCSPI_DmaChConfig::edmaIntrObjTx
Edma_IntrObject edmaIntrObjTx
Definition: mcspi_dma_edma.h:72
MCSPI_DmaChConfig::edmaRxParam
uint32_t edmaRxParam
Definition: mcspi_dma_edma.h:60
MCSPI_DmaChConfig::edmaRxChId
uint32_t edmaRxChId
Definition: mcspi_dma_edma.h:56
MCSPI_DmaChConfig::edmaTxParam
uint32_t edmaTxParam
Definition: mcspi_dma_edma.h:62
MCSPI_DmaChConfig::isOpen
uint32_t isOpen
Definition: mcspi_dma_edma.h:74
MCSPI_DmaChConfig::edmaTccRx
uint32_t edmaTccRx
Definition: mcspi_dma_edma.h:52
McspiDma_EdmaArgs::drvHandle
void * drvHandle
Definition: mcspi_dma_edma.h:46