MCSPI Driver API/interface file.
Go to the source code of this file.
Data Structures | |
| struct | MCSPI_Transaction |
| Data structure used with MCSPI_transfer() More... | |
| struct | MCSPI_OpenParams |
| MCSPI Parameters. More... | |
| struct | MCSPI_ChConfig |
| MCSPI configuration parameters for the channel. More... | |
| struct | MCSPI_Attrs |
| MCSPI instance attributes - used during init time. More... | |
| struct | MCSPI_ChObject |
| MCSPI channel object. More... | |
| struct | MCSPI_Object |
| MCSPI driver object. More... | |
| struct | MCSPI_Config |
| MCSPI global configuration array. More... | |
Macros | |
| #define | MCSPI_MAX_NUM_CHANNELS (4U) |
| Max number of channels/Chip Select (CS) supported. More... | |
| #define | MCSPI_FIFO_LENGTH (64U) |
| Total length of FIFO for both TX/RX. More... | |
| #define | MCSPI_RX_FIFO_ENABLE |
| McSPI peripheral Rx FIFO is enabled. More... | |
| #define | MCSPI_RX_FIFO_DISABLE |
| McSPI peripheral Rx FIFO is disabled. More... | |
| #define | MCSPI_TX_FIFO_ENABLE |
| McSPI peripheral Tx FIFO is enabled. More... | |
| #define | MCSPI_TX_FIFO_DISABLE |
| McSPI peripheral Tx FIFO is disabled. More... | |
| #define | MCSPI_REG_OFFSET (0x14U) |
| McSPI Register Offset for MCSPI_CHxCONF, MCSPI_CHxSTAT, MCSPI_CHxCTRL, MCSPI_TXx and MCSPI_RXx register set. More... | |
| #define | MCSPI_CHCONF(x) |
| Base address of McSPI_CHCONF(x) More... | |
| #define | MCSPI_CHSTAT(x) |
| Base address of McSPI_CHSTAT(x) More... | |
| #define | MCSPI_CHCTRL(x) |
| Base address of McSPI_CHCTRL(x) More... | |
| #define | MCSPI_CHTX(x) |
| Base address of McSPI_CHTX(x) More... | |
| #define | MCSPI_CHRX(x) |
| Base address of McSPI_CHRX(x) More... | |
| #define | MCSPI_CLKD_MASK (0x0FU) |
| #define | MCSPI_IRQSTATUS_CLEAR_ALL |
| Bit mask to clear all status bits. More... | |
Channel Id | |
| #define | MCSPI_CHANNEL_0 (0U) |
| #define | MCSPI_CHANNEL_1 (1U) |
| #define | MCSPI_CHANNEL_2 (2U) |
| #define | MCSPI_CHANNEL_3 (3U) |
Operating Mode | |
| #define | MCSPI_OPER_MODE_POLLED (0U) |
| #define | MCSPI_OPER_MODE_INTERRUPT (1U) |
| #define | MCSPI_OPER_MODE_DMA (2U) |
Transfer Status Code | |
| #define | MCSPI_TRANSFER_COMPLETED (0U) |
| #define | MCSPI_TRANSFER_STARTED (1U) |
| #define | MCSPI_TRANSFER_CANCELLED (2U) |
| #define | MCSPI_TRANSFER_FAILED (3U) |
| #define | MCSPI_TRANSFER_CSN_DEASSERT (4U) |
| #define | MCSPI_TRANSFER_TIMEOUT (5U) |
Transfer Mode | |
This determines whether the driver operates synchronously or asynchronously In MCSPI_TRANSFER_MODE_BLOCKING mode MCSPI_transfer() blocks code execution until the transaction has completed In MCSPI_TRANSFER_MODE_CALLBACK MCSPI_transfer() does not block code execution and instead calls a MCSPI_CallbackFxn callback function when the transaction has completed | |
| #define | MCSPI_TRANSFER_MODE_BLOCKING (0U) |
| MCSPI_transfer() blocks execution. This mode can only be used when called within a Task context More... | |
| #define | MCSPI_TRANSFER_MODE_CALLBACK (1U) |
| MCSPI_transfer() does not block code execution and will call a MCSPI_CallbackFxn. This mode can be used in a Task, Swi, or Hwi context More... | |
Modes of Operation | |
Definitions for various MCSPI modes of operation The MCSPI driver operates in both controller and SPI peripheral modes. Logically, the implementation is identical, however the difference between these two modes is driven by hardware. The default mode is MCSPI_MS_MODE_CONTROLLER, but can be set to peripheral mode by setting MCSPI_OpenParams.msMode to MCSPI_MS_MODE_PERIPHERAL in the parameters passed to MCSPI_open(). | |
| #define | MCSPI_MS_MODE_CONTROLLER (CSL_MCSPI_MODULCTRL_MS_MASTER) |
| The module generates the clock and CS. More... | |
| #define | MCSPI_MS_MODE_PERIPHERAL (CSL_MCSPI_MODULCTRL_MS_SLAVE) |
| The module receives the clock and CS. More... | |
Frame Format | |
| #define | MCSPI_FF_POL0_PHA0 (0U) |
| #define | MCSPI_FF_POL0_PHA1 (1U) |
| #define | MCSPI_FF_POL1_PHA0 (2U) |
| #define | MCSPI_FF_POL1_PHA1 (3U) |
Chip-select Polarity | |
| #define | MCSPI_CS_POL_HIGH (CSL_MCSPI_CH0CONF_EPOL_ACTIVEHIGH) |
| SPIEN (CS) is held high during the ACTIVE state. More... | |
| #define | MCSPI_CS_POL_LOW (CSL_MCSPI_CH0CONF_EPOL_ACTIVELOW) |
| SPIEN (CS) is held low during the ACTIVE state. More... | |
Transmit-Receive Modes | |
| #define | MCSPI_TR_MODE_TX_RX (CSL_MCSPI_CH0CONF_TRM_TRANSRECEI) |
| #define | MCSPI_TR_MODE_RX_ONLY (CSL_MCSPI_CH0CONF_TRM_RECEIVONLY) |
| #define | MCSPI_TR_MODE_TX_ONLY (CSL_MCSPI_CH0CONF_TRM_TRANSONLY) |
Input Select | |
| #define | MCSPI_IS_D0 (CSL_MCSPI_CH0CONF_IS_LINE0) |
| Data line 0 (SPIDAT[0]) selected for reception. More... | |
| #define | MCSPI_IS_D1 (CSL_MCSPI_CH0CONF_IS_LINE1) |
| Data line 1 (SPIDAT[1]) selected for reception. More... | |
Transmission Enable for Data Line | |
| #define | MCSPI_DPE_ENABLE (CSL_MCSPI_CH0CONF_DPE0_ENABLED) |
| Data line selected for transmission. More... | |
| #define | MCSPI_DPE_DISABLE (CSL_MCSPI_CH0CONF_DPE0_DISABLED) |
| No transmission on Data Line. More... | |
Peripheral Chip-select Signal Select | |
| #define | MCSPI_SLV_CS_SELECT_0 (CSL_MCSPI_CH0CONF_SPIENSLV_SPIEN0) |
| #define | MCSPI_SLV_CS_SELECT_1 (CSL_MCSPI_CH0CONF_SPIENSLV_SPIEN1) |
| #define | MCSPI_SLV_CS_SELECT_2 (CSL_MCSPI_CH0CONF_SPIENSLV_SPIEN2) |
| #define | MCSPI_SLV_CS_SELECT_3 (CSL_MCSPI_CH0CONF_SPIENSLV_SPIEN3) |
Start-bit Polarity | |
| #define | MCSPI_SB_POL_HIGH (CSL_MCSPI_CH0CONF_SBPOL_HIGHLEVEL) |
| SStart-bit polarity is held to 1 during MCSPI transfer. More... | |
| #define | MCSPI_SB_POL_LOW (CSL_MCSPI_CH0CONF_SBPOL_LOWLEVEL) |
| Start-bit polarity is held to 0 during MCSPI transfer. More... | |
Chip-select Idle Time | |
| #define | MCSPI_TCS0_0_CLK (CSL_MCSPI_CH0CONF_TCS0_ZEROCYCLEDLY) |
| 0.5 clock cycles delay More... | |
| #define | MCSPI_TCS0_1_CLK (CSL_MCSPI_CH0CONF_TCS0_ONECYCLEDLY) |
| 1.5 clock cycles delay More... | |
| #define | MCSPI_TCS0_2_CLK (CSL_MCSPI_CH0CONF_TCS0_TWOCYCLEDLY) |
| 2.5 clock cycles delay More... | |
| #define | MCSPI_TCS0_3_CLK (CSL_MCSPI_CH0CONF_TCS0_THREECYCLEDLY) |
| 3.5 clock cycles delay More... | |
Channel Mode | |
| #define | MCSPI_CH_MODE_SINGLE (CSL_MCSPI_MODULCTRL_SINGLE_SINGLE) |
| Only one channel will be used in controller mode. This should be used when CS is used in forced enable mode. More... | |
| #define | MCSPI_CH_MODE_MULTI (CSL_MCSPI_MODULCTRL_SINGLE_MULTI) |
| More than one channel will be used in controller mode. More... | |
Pin Mode | |
| #define | MCSPI_PINMODE_3PIN (CSL_MCSPI_MODULCTRL_PIN34_3PINMODE) |
| SPIEN (CS) is not used. In this mode all related options to chip-select have no meaning. More... | |
| #define | MCSPI_PINMODE_4PIN (CSL_MCSPI_MODULCTRL_PIN34_4PINMODE) |
Init Delay | |
| #define | MCSPI_INITDLY_0 (CSL_MCSPI_MODULCTRL_INITDLY_NODELAY) |
| No delay. More... | |
| #define | MCSPI_INITDLY_4 (CSL_MCSPI_MODULCTRL_INITDLY_4CLKDLY) |
| 4 SPI bus clock delays More... | |
| #define | MCSPI_INITDLY_8 (CSL_MCSPI_MODULCTRL_INITDLY_8CLKDLY) |
| 8 SPI bus clock delays More... | |
| #define | MCSPI_INITDLY_16 (CSL_MCSPI_MODULCTRL_INITDLY_16CLKDLY) |
| 16 SPI bus clock delays More... | |
| #define | MCSPI_INITDLY_32 (CSL_MCSPI_MODULCTRL_INITDLY_32CLKDLY) |
| 32 SPI bus clock delays More... | |
Typedefs | |
| typedef void * | MCSPI_Handle |
| A handle that is returned from a MCSPI_open() call. More... | |
| typedef void(* | MCSPI_CallbackFxn) (MCSPI_Handle handle, MCSPI_Transaction *transaction) |
| The definition of a callback function used by the SPI driver when used in MCSPI_TRANSFER_MODE_CALLBACK. More... | |
Functions | |
| void | MCSPI_init (void) |
| This function initializes the MCSPI module. More... | |
| void | MCSPI_deinit (void) |
| This function de-initializes the MCSPI module. More... | |
| MCSPI_Handle | MCSPI_open (uint32_t index, const MCSPI_OpenParams *openPrms) |
| This function opens a given MCSPI peripheral. More... | |
| void | MCSPI_close (MCSPI_Handle handle) |
| Function to close a MCSPI peripheral specified by the MCSPI handle. More... | |
| int32_t | MCSPI_chConfig (MCSPI_Handle handle, const MCSPI_ChConfig *chCfg) |
| Function to configure a MCSPI channel. More... | |
| int32_t | MCSPI_dmaChConfig (MCSPI_Handle handle, const MCSPI_ChConfig *chCfg, const MCSPI_DmaChConfig *dmaChCfg) |
| Function to configure a DMA of a channel. More... | |
| int32_t | MCSPI_transfer (MCSPI_Handle handle, MCSPI_Transaction *transaction) |
| Function to perform MCSPI transactions. More... | |
| int32_t | MCSPI_transferCancel (MCSPI_Handle handle) |
| Function to cancel MCSPI transactions on channel of a SPI peripheral specified by the MCSPI handle. More... | |
| static void | MCSPI_OpenParams_init (MCSPI_OpenParams *openPrms) |
| Function to initialize the MCSPI_OpenParams struct to its defaults. More... | |
| static void | MCSPI_ChConfig_init (MCSPI_ChConfig *chConfig) |
| Function to initialize the MCSPI_ChConfig struct to its defaults. More... | |
| static void | MCSPI_Transaction_init (MCSPI_Transaction *trans) |
| Function to initialize the MCSPI_Transaction struct to its defaults. More... | |
| uint32_t | MCSPI_getBaseAddr (MCSPI_Handle handle) |
| Function to get base address of MCSPI instance of a particular handle. More... | |
| int32_t | MCSPI_reConfigFifo (MCSPI_Handle handle, uint32_t chNum, uint32_t numWordsRxTx) |
| Function to re-configure Effective FIFO Words. More... | |
| static uint32_t | MCSPI_getBufWidthShift (uint32_t dataSize) |
| This API will return the buffer width in bytes based on dataSize. More... | |
| static uint32_t | MCSPI_readChStatusReg (uint32_t baseAddr, uint32_t chNum) |
| This API will return the status of the McSPI channel currently in use. More... | |
| static uint32_t | MCSPI_readChCtrlReg (uint32_t baseAddr, uint32_t chNum) |
| This API returns Channel control register value. More... | |
| static void | MCSPI_writeChCtrlReg (uint32_t baseAddr, uint32_t chNum, uint32_t regVal) |
| This API sets Channel control register value. More... | |
| static uint32_t | MCSPI_readChConf (uint32_t baseAddr, uint32_t chNum) |
| This API returns Channel Config register value. More... | |
| static void | MCSPI_writeChConfReg (uint32_t baseAddr, uint32_t chNum, uint32_t regVal) |
| This API sets Channel Config register value. More... | |
| static void | MCSPI_writeTxDataReg (uint32_t baseAddr, uint32_t txData, uint32_t chNum) |
| This API will put the data on to the McSPI Channel transmit register. More... | |
| static void | MCSPI_enableTxFIFO (uint32_t baseAddr, uint32_t chNum, uint32_t enableFlag) |
| This API will enable/disable the Tx FIFOs of McSPI peripheral. More... | |
| static void | MCSPI_enableRxFIFO (uint32_t baseAddr, uint32_t chNum, uint32_t enableFlag) |
| This API will enable/disable the Rx FIFOs of McSPI peripheral. More... | |
| static uint32_t | MCSPI_readRxDataReg (uint32_t baseAddr, uint32_t chNum) |
| This API will return the data present in the MCSPI_RX register. More... | |
| static void | MCSPI_setDataWidth (uint32_t baseAddr, uint32_t chNum, uint32_t dataWidth) |
| This API will set the data width in the channel config register. More... | |
Variables | |
| MCSPI_Config | gMcspiConfig [] |
| Externally defined driver configuration array. More... | |
| uint32_t | gMcspiConfigNum |
| Externally defined driver configuration array size. More... | |