|
AM263x MCU+ SDK
08.06.00
|
|
Go to the documentation of this file.
54 #ifndef ICSSG_STATS_H_
55 #define ICSSG_STATS_H_
85 typedef struct IcssgStats_MacPort_s
275 typedef struct IcssgStats_Pa_s
uint32_t preemptFragCntTxSlice0
Definition: icssg_stats.h:482
uint32_t txPort1TsDroppedPkt
Definition: icssg_stats.h:397
uint32_t rxClass1
Definition: icssg_stats.h:124
uint32_t hostQ7Overflow
Definition: icssg_stats.h:367
uint32_t rxClass3
Definition: icssg_stats.h:130
uint32_t rxErrorSlice0
Definition: icssg_stats.h:379
uint32_t txGoodFrame
Definition: icssg_stats.h:208
uint32_t rxErrorSlice1
Definition: icssg_stats.h:382
uint32_t port1Q5Overflow
Definition: icssg_stats.h:313
uint32_t port1Q0Overflow
Definition: icssg_stats.h:298
uint32_t txMinSizeErrFrame
Definition: icssg_stats.h:232
uint32_t rxClass13
Definition: icssg_stats.h:160
uint32_t hostTxPktCnt
Definition: icssg_stats.h:287
uint32_t txMcastFrame
Definition: icssg_stats.h:214
uint32_t infAftDropTaggedSlice1
Definition: icssg_stats.h:440
uint32_t rxOverrunFrame
Definition: icssg_stats.h:118
uint32_t infPortDisabledSlice0
Definition: icssg_stats.h:404
uint32_t rxEofRtuDsInvalidSlice1
Definition: icssg_stats.h:388
uint32_t infAftDropNoTagSlice1
Definition: icssg_stats.h:456
uint32_t rx64BSizedFrame
Definition: icssg_stats.h:184
uint32_t preemptAsmOkSlice1
Definition: icssg_stats.h:491
uint32_t txOddNibbleFrame
Definition: icssg_stats.h:217
uint32_t txTotalByte
Definition: icssg_stats.h:265
uint32_t txBucket3SizeConfig
Definition: icssg_stats.h:241
uint32_t rxGoodFrames
Definition: icssg_stats.h:88
uint32_t infAftDropNoTagSlice0
Definition: icssg_stats.h:452
uint32_t rxBucket3SizeConfig
Definition: icssg_stats.h:178
uint64_t hostTxByteCnt
Definition: icssg_stats.h:281
uint32_t preemptFragCntRxSlice1
Definition: icssg_stats.h:497
uint32_t txBucket2SizeConfig
Definition: icssg_stats.h:238
uint32_t port2Q7Overflow
Definition: icssg_stats.h:343
uint32_t txUnderFlowErr
Definition: icssg_stats.h:220
uint32_t hostQ3Overflow
Definition: icssg_stats.h:355
uint32_t rxClass5
Definition: icssg_stats.h:136
uint32_t rxClass14
Definition: icssg_stats.h:163
uint32_t infSaBlSlice1
Definition: icssg_stats.h:424
uint32_t rxMinSizeFrame
Definition: icssg_stats.h:112
uint32_t port1Q4Overflow
Definition: icssg_stats.h:310
uint32_t rxClass11
Definition: icssg_stats.h:154
uint32_t infSaBlSlice0
Definition: icssg_stats.h:420
uint32_t rxTotalByte
Definition: icssg_stats.h:202
uint32_t rxOddNibbleFrame
Definition: icssg_stats.h:103
uint32_t rxBucket5SizedFrame
Definition: icssg_stats.h:199
uint32_t tx64BSizedFrame
Definition: icssg_stats.h:247
uint32_t rxEofRtuDsInvalidSlice0
Definition: icssg_stats.h:385
uint32_t fdbNoSpaceToLearn
Definition: icssg_stats.h:467
uint32_t rxBucket2SizeConfig
Definition: icssg_stats.h:175
uint32_t preemptFragCntRxSlice0
Definition: icssg_stats.h:494
uint32_t preemptAsmErrSlice1
Definition: icssg_stats.h:479
uint32_t preemptAsmErrSlice0
Definition: icssg_stats.h:476
uint32_t txBucket4SizeConfig
Definition: icssg_stats.h:244
uint32_t txPort2TsDroppedPkt
Definition: icssg_stats.h:400
uint32_t infAftDropPrioTaggedSlice1
Definition: icssg_stats.h:448
uint32_t txBucket3SizedFrame
Definition: icssg_stats.h:256
uint32_t txBcastFrame
Definition: icssg_stats.h:211
uint32_t txPort1DroppedPkt
Definition: icssg_stats.h:391
uint32_t port2Q2Overflow
Definition: icssg_stats.h:328
uint32_t rxClass7
Definition: icssg_stats.h:142
uint32_t infPortBlockedSlice0
Definition: icssg_stats.h:428
uint32_t txBucket1SizedFrame
Definition: icssg_stats.h:250
uint32_t port1Q3Overflow
Definition: icssg_stats.h:307
uint32_t rxClass8
Definition: icssg_stats.h:145
uint32_t infPortBlockedSlice1
Definition: icssg_stats.h:432
uint32_t txBucket2SizedFrame
Definition: icssg_stats.h:253
uint32_t preemptAsmOkSlice0
Definition: icssg_stats.h:488
uint32_t rxClass4
Definition: icssg_stats.h:133
uint32_t infPortDisabledSlice1
Definition: icssg_stats.h:408
uint32_t rxClass6
Definition: icssg_stats.h:139
uint32_t rxMinSizeErrFrame
Definition: icssg_stats.h:115
uint32_t preemptBadFragSlice0
Definition: icssg_stats.h:470
uint32_t hostQ5Overflow
Definition: icssg_stats.h:361
uint32_t rxMIIErrors
Definition: icssg_stats.h:100
uint32_t rtu0PktDroppedSlice1
Definition: icssg_stats.h:295
uint32_t port1Q1Overflow
Definition: icssg_stats.h:301
uint32_t preemptFragCntTxSlice1
Definition: icssg_stats.h:485
uint32_t rxBucket4SizedFrame
Definition: icssg_stats.h:196
ICSSG statistics counters.
Definition: icssg_stats.h:86
uint32_t droppedPktSlice0
Definition: icssg_stats.h:373
uint32_t txPort2DroppedPkt
Definition: icssg_stats.h:394
uint32_t port2Q5Overflow
Definition: icssg_stats.h:337
uint32_t port2Q4Overflow
Definition: icssg_stats.h:334
uint32_t hostQ6Overflow
Definition: icssg_stats.h:364
uint32_t infAftDropNotMemberSlice0
Definition: icssg_stats.h:460
ICSSG Packet Accelerator (PA) statistics counters.
Definition: icssg_stats.h:276
uint32_t port2Q1Overflow
Definition: icssg_stats.h:325
uint64_t hostRxByteCnt
Definition: icssg_stats.h:278
uint32_t infAftDropTaggedSlice0
Definition: icssg_stats.h:436
uint32_t infAftDropNotMemberSlice1
Definition: icssg_stats.h:464
uint32_t rxBucket1SizedFrame
Definition: icssg_stats.h:187
uint32_t infSavSlice1
Definition: icssg_stats.h:416
uint32_t rxEofShortFrameErrSlice1
Definition: icssg_stats.h:505
uint32_t rxBucket4SizeConfig
Definition: icssg_stats.h:181
uint32_t port2Q0Overflow
Definition: icssg_stats.h:322
uint32_t rxEofShortFrameErrSlice0
Definition: icssg_stats.h:501
uint32_t hostQ0Overflow
Definition: icssg_stats.h:346
This file contains the type definitions and helper macros for the Enet Statistics module interface.
uint32_t rxSMDFragErr
Definition: icssg_stats.h:169
uint32_t hostQ1Overflow
Definition: icssg_stats.h:349
uint32_t rxMaxSizeFrame
Definition: icssg_stats.h:106
uint32_t hostQ4Overflow
Definition: icssg_stats.h:358
uint32_t rtu0PktDroppedSlice0
Definition: icssg_stats.h:291
uint32_t rxBucket3SizedFrame
Definition: icssg_stats.h:193
uint32_t txBucket5SizedFrame
Definition: icssg_stats.h:262
uint32_t txMaxSizeFrame
Definition: icssg_stats.h:223
uint32_t rxClass9
Definition: icssg_stats.h:148
uint32_t preemptBadFragSlice1
Definition: icssg_stats.h:473
uint32_t rxClass2
Definition: icssg_stats.h:127
uint32_t rxTxTotalByte
Definition: icssg_stats.h:205
uint32_t rxBCastFrames
Definition: icssg_stats.h:91
uint32_t rxMCastFrames
Definition: icssg_stats.h:94
uint32_t port1Q2Overflow
Definition: icssg_stats.h:304
uint32_t rxClass12
Definition: icssg_stats.h:157
uint32_t hostEgressQPreOverflow
Definition: icssg_stats.h:370
uint32_t rxCRCErrors
Definition: icssg_stats.h:97
uint32_t txBucket4SizedFrame
Definition: icssg_stats.h:259
uint32_t rxMaxSizeErrFrame
Definition: icssg_stats.h:109
uint32_t infSavSlice0
Definition: icssg_stats.h:412
uint32_t txMaxSizeErrFrame
Definition: icssg_stats.h:226
uint32_t port2Q3Overflow
Definition: icssg_stats.h:331
uint32_t infAftDropPrioTaggedSlice0
Definition: icssg_stats.h:444
uint32_t rxBucket1SizeConfig
Definition: icssg_stats.h:172
uint32_t rxClass0
Definition: icssg_stats.h:121
uint32_t port1Q6Overflow
Definition: icssg_stats.h:316
uint32_t droppedPktSlice1
Definition: icssg_stats.h:376
uint32_t rxClass10
Definition: icssg_stats.h:151
uint32_t hostRxPktCnt
Definition: icssg_stats.h:284
uint32_t txMinSizeFrame
Definition: icssg_stats.h:229
uint32_t txBucket1SizeConfig
Definition: icssg_stats.h:235
uint32_t port1Q7Overflow
Definition: icssg_stats.h:319
uint32_t port2Q6Overflow
Definition: icssg_stats.h:340
uint32_t hostQ2Overflow
Definition: icssg_stats.h:352
uint32_t rxBucket2SizedFrame
Definition: icssg_stats.h:190
uint32_t rxClass15
Definition: icssg_stats.h:166