AM263x MCU+ SDK  08.06.00
hsmclient.h
Go to the documentation of this file.
1 /*
2  * Copyright (C) 2022-23 Texas Instruments Incorporated
3  *
4  * Redistribution and use in source and binary forms, with or without
5  * modification, are permitted provided that the following conditions
6  * are met:
7  *
8  * Redistributions of source code must retain the above copyright
9  * notice, this list of conditions and the following disclaimer.
10  *
11  * Redistributions in binary form must reproduce the above copyright
12  * notice, this list of conditions and the following disclaimer in the
13  * documentation and/or other materials provided with the
14  * distribution.
15  *
16  * Neither the name of Texas Instruments Incorporated nor the names of
17  * its contributors may be used to endorse or promote products derived
18  * from this software without specific prior written permission.
19  *
20  * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS
21  * "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT
22  * LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR
23  * A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT
24  * OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL,
25  * SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT
26  * LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE,
27  * DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY
28  * THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT
29  * (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE
30  * OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
31  */
32 
33 #ifndef HSM_CLIENT_H_
34 #define HSM_CLIENT_H_
35 
36 #ifdef __cplusplus
37 extern "C" {
38 #endif
39 
40 /* Header file for HSM client driver */
41 #include <stdint.h>
42 #include <drivers/sipc_notify.h>
45 #include <kernel/dpl/SemaphoreP.h>
46 
62 typedef union HsmVer_t_
63 {
64  uint64_t HsmrtVer ;
65  struct
66  {
67  uint8_t PatchVer ;
68  uint8_t MinorVer ;
69  uint8_t MajorVer;
70  uint8_t ApiVer ;
71  uint8_t SocType ;
72  uint8_t BinType ;
73  uint8_t HsmType ;
74  uint8_t DevType ;
77 #if defined(_TMS320C6X)
78 }__attribute__((packed)) HsmVer_t_;
79 #else
80 }__attribute__((packed)) HsmVer_t;
81 #endif
82 
83 
89 typedef struct HsmClient_t_
90 {
93  HsmMsg_t ReqMsg ;
94  HsmMsg_t RespMsg ;
95  uint8_t RespFlag ;
96  uint8_t ClientId ;
98 } HsmClient_t ;
99 
105 typedef struct EfuseRead_t_
106 {
107  uint32_t rowData ;
108  uint8_t rowIdx ;
109  uint8_t rsvd[3];
110 } EfuseRead_t;
111 
117 typedef struct EfuseRowWrite_t_
118 {
119  uint32_t rowData ;
120  uint32_t rowBitMask ;
121  uint8_t rowIdx ;
122  uint8_t rsvd[3];
124 
130 typedef struct EfuseRowCount_t_
131 {
132  uint32_t rowCount ;
133  uint8_t rowSize ;
134  uint8_t rsvd[3];
136 
143 typedef struct EfuseRowProt_t_
144 {
145  uint8_t rowidx ;
146  uint8_t readProt ;
147  uint8_t writeProt ;
148  uint8_t rsvd[1];
149 } EfuseRowProt_t ;
150 
161 int32_t HsmClient_init(SIPC_Params* params);
162 
168 void HsmClient_deInit(void);
169 
185 int32_t HsmClient_getVersion(HsmClient_t *HsmClient ,
186  HsmVer_t* verId,uint32_t timeToWaitInTick);
187 
203 int32_t HsmClient_getUID(HsmClient_t* HsmClient,
204  uint8_t* uid, uint32_t timeout);
205 
222 int32_t HsmClient_openDbgFirewall(HsmClient_t* HsmClient,
223  uint8_t* cert,
224  uint32_t cert_size,
225  uint32_t timeout);
226 
239 int32_t HsmClient_readOTPRow(HsmClient_t* HsmClient,
240  EfuseRead_t* readRow);
241 
254 int32_t HsmClient_writeOTPRow(HsmClient_t* HsmClient,
255  EfuseRowWrite_t* writeRow);
256 
269 int32_t HsmClient_lockOTPRow(HsmClient_t* HsmClient,
270  EfuseRowProt_t* rowProt);
271 
284 int32_t HsmClient_getOTPRowCount(HsmClient_t* HsmClient,
285  EfuseRowCount_t* rowCount);
286 
299 int32_t HsmClient_getOTPRowProtection(HsmClient_t* HsmClient,
300  EfuseRowProt_t* rowProt);
301 
313 int32_t HsmClient_register(HsmClient_t* HsmClient, uint8_t clientId);
314 
323 void HsmClient_unregister(HsmClient_t* HsmClient,uint8_t clientId);
337 int32_t HsmClient_waitForBootNotify(HsmClient_t* HsmClient,uint32_t timeToWaitInTicks);
338 
347 int32_t Hsmclient_loadHSMRtFirmware(const uint8_t *pHSMRt_firmware);
348 
351 #ifdef __cplusplus
352 }
353 #endif
354 
355 #endif /* HSM_CLIENT_H_ */
SIPC_Params
Parameters used by SIPC_init.
Definition: sipc_notify.h:84
EfuseRead_t::rowData
uint32_t rowData
Definition: hsmclient.h:107
HsmVer_t_
type for reading HSMRt version.
Definition: hsmclient.h:63
HsmVer_t_::PatchVer
uint8_t PatchVer
Definition: hsmclient.h:67
EfuseRowProt_t
This is a EfuseRowProt type which holds the information of eFuse row index and protection status corr...
Definition: hsmclient.h:144
EfuseRowCount_t::rowCount
uint32_t rowCount
Definition: hsmclient.h:132
HsmClient_t::RespFlag
uint8_t RespFlag
Definition: hsmclient.h:95
EfuseRowWrite_t::rowBitMask
uint32_t rowBitMask
Definition: hsmclient.h:120
EfuseRowProt_t::rowidx
uint8_t rowidx
Definition: hsmclient.h:145
EfuseRowWrite_t
This is a EfuseRowWrite type which holds the information regarding programming eFuse row.
Definition: hsmclient.h:118
Hsmclient_loadHSMRtFirmware
int32_t Hsmclient_loadHSMRtFirmware(const uint8_t *pHSMRt_firmware)
Loads the HSMRt firmware. This is typically called by SBL.
Definition: hsmclient_loadhsmrt.c:254
__attribute__
union HsmVer_t_ __attribute__((packed)) HsmVer_t
type for reading HSMRt version.
EfuseRead_t::rowIdx
uint8_t rowIdx
Definition: hsmclient.h:108
HsmVer_t_::HsmType
uint8_t HsmType
Definition: hsmclient.h:73
HsmVer_t_::MajorVer
uint8_t MajorVer
Definition: hsmclient.h:69
HsmClient_t
This is a HSMClient type which holds the information needed by hsm client to communicate with HSM .
Definition: hsmclient.h:90
HsmVer_t_::SocType
uint8_t SocType
Definition: hsmclient.h:71
HsmVer_t_::ApiVer
uint8_t ApiVer
Definition: hsmclient.h:70
SemaphoreP.h
HsmVer_t_::HsmrtVer
uint64_t HsmrtVer
Definition: hsmclient.h:64
sipc_notify.h
HsmVer_t_::DevType
uint8_t DevType
Definition: hsmclient.h:74
HsmClient_t::RespMsg
HsmMsg_t RespMsg
Definition: hsmclient.h:94
HsmClient_openDbgFirewall
int32_t HsmClient_openDbgFirewall(HsmClient_t *HsmClient, uint8_t *cert, uint32_t cert_size, uint32_t timeout)
The service issued to HSM Server verifies the certificate and by default the hsm flag is set to HSM_F...
Definition: hsmclient.c:342
HsmClient_register
int32_t HsmClient_register(HsmClient_t *HsmClient, uint8_t clientId)
register a client to a particular ClientId
Definition: hsmclient.c:162
EfuseRowCount_t
This is a EfuseRowCount type which holds the information regarding eFuse row count and size of each r...
Definition: hsmclient.h:131
HsmClient_getOTPRowCount
int32_t HsmClient_getOTPRowCount(HsmClient_t *HsmClient, EfuseRowCount_t *rowCount)
The service issued to HSM Server retrieves the count of extended OTP rows.
Definition: hsmclient.c:592
EfuseRowProt_t::readProt
uint8_t readProt
Definition: hsmclient.h:146
HsmClient_init
int32_t HsmClient_init(SIPC_Params *params)
Initialize the HSM client for current core.
Definition: hsmclient.c:191
HsmClient_getOTPRowProtection
int32_t HsmClient_getOTPRowProtection(HsmClient_t *HsmClient, EfuseRowProt_t *rowProt)
The service issued to HSM Server retrieves the extended otp efuse row protection status.
Definition: hsmclient.c:653
HsmVer_t_::BinType
uint8_t BinType
Definition: hsmclient.h:72
HsmVer_t_::VerStruct
struct HsmVer_t_::@0 VerStruct
HsmClient_unregister
void HsmClient_unregister(HsmClient_t *HsmClient, uint8_t clientId)
unregister a client to a particular ClientId
Definition: hsmclient.c:212
hsmclient_msg.h
HsmClient_writeOTPRow
int32_t HsmClient_writeOTPRow(HsmClient_t *HsmClient, EfuseRowWrite_t *writeRow)
The service issued to HSM Server writes the data to extended OTP efuse row based on row index provide...
Definition: hsmclient.c:470
HsmClient_readOTPRow
int32_t HsmClient_readOTPRow(HsmClient_t *HsmClient, EfuseRead_t *readRow)
The service issued to HSM Server retrieves the data of GP OTP row based on row index provided as para...
Definition: hsmclient.c:408
HsmClient_waitForBootNotify
int32_t HsmClient_waitForBootNotify(HsmClient_t *HsmClient, uint32_t timeToWaitInTicks)
Current core will wait for bootnotify message from HSM core.
Definition: hsmclient.c:714
EfuseRowWrite_t::rowData
uint32_t rowData
Definition: hsmclient.h:119
HsmClient_t::Semaphore
SemaphoreP_Object Semaphore
Definition: hsmclient.h:91
HsmVer_t_::MinorVer
uint8_t MinorVer
Definition: hsmclient.h:68
EfuseRowProt_t::writeProt
uint8_t writeProt
Definition: hsmclient.h:147
EfuseRead_t
This is a EfuseRead type which holds the information of eFuse row index and row data corresponding to...
Definition: hsmclient.h:106
HsmClient_getUID
int32_t HsmClient_getUID(HsmClient_t *HsmClient, uint8_t *uid, uint32_t timeout)
The service issued to HSM Server populates the Device UID by default the hsm flag is set to HSM_FLAG_...
Definition: hsmclient.c:280
EfuseRowWrite_t::rowIdx
uint8_t rowIdx
Definition: hsmclient.h:121
HsmClient_t::ClientId
uint8_t ClientId
Definition: hsmclient.h:96
SemaphoreP_Object
Opaque semaphore object used with the semaphore APIs.
Definition: SemaphoreP.h:59
EfuseRowCount_t::rowSize
uint8_t rowSize
Definition: hsmclient.h:133
HsmClient_getVersion
int32_t HsmClient_getVersion(HsmClient_t *HsmClient, HsmVer_t *verId, uint32_t timeToWaitInTick)
populates the current HSMRT version Id by default the hsm flag is set to HSM_FLAG_AOP for this servic...
Definition: hsmclient.c:218
HsmClient_lockOTPRow
int32_t HsmClient_lockOTPRow(HsmClient_t *HsmClient, EfuseRowProt_t *rowProt)
The service issued to HSM Server sets the protection status bit of the specified row to 1.
Definition: hsmclient.c:531
hsmclient_utils.h
HsmClient_t::ReqMsg
HsmMsg_t ReqMsg
Definition: hsmclient.h:93
HsmClient_deInit
void HsmClient_deInit(void)
De initialize the HSM client for current core.