AM263x MCU+ SDK  08.06.00
APIs for Tamagawa Encoder Over UART

Introduction

Here is the list of APIs used for Tamagawa encoder communication protocol

Data Structures

struct  tamagawa_tx
 Tamagawa Interface Transmit data. More...
 
struct  tamagawa_rx
 Tamagawa Interface Received data. More...
 
struct  tamagawa_uart_interface
 Tamagawa Interface. More...
 

Functions

int32_t tamagawa_command_process (volatile struct tamagawa_uart_interface *tamagawa_interface, UART_Handle *gUartHandle, int32_t cmd)
 Process The Tamagawa Command. More...
 
int32_t tamagawa_crc_verify (volatile struct tamagawa_uart_interface *tamagawa_interface)
 Compare Received CRC and Calculated CRC. More...
 
void tamagawa_init (volatile struct tamagawa_uart_interface *tamagawa_interface, uint32_t instance, uint32_t base_address, uint32_t pin_number, uint32_t pin_direction)
 Configure GOPIO pin for RTSn(sw flow control) More...
 

Enumerations

enum  data_id {
  DATA_ID_0, DATA_ID_1, DATA_ID_2, DATA_ID_3,
  DATA_ID_6, DATA_ID_7, DATA_ID_8, DATA_ID_C,
  DATA_ID_D, DATA_ID_NUM
}
 Data ID codes. More...
 

Macros

#define MAX_EEPROM_ADDRESS   (127)
 Used to set the maximum address that can be used for EEPROM Read/Write. More...
 
#define MAX_EEPROM_WRITE_DATA   (255)
 Used to set the maximum value that can be written in EEPROM. More...
 

Macro Definition Documentation

◆ MAX_EEPROM_ADDRESS

#define MAX_EEPROM_ADDRESS   (127)

Used to set the maximum address that can be used for EEPROM Read/Write.

◆ MAX_EEPROM_WRITE_DATA

#define MAX_EEPROM_WRITE_DATA   (255)

Used to set the maximum value that can be written in EEPROM.

Enumeration Type Documentation

◆ data_id

enum data_id

Data ID codes.

Enumerator
DATA_ID_0 

Data readout data in one revolution

DATA_ID_1 

Data readout multi-turn data

DATA_ID_2 

Data readout encoder ID

DATA_ID_3 

Data readout data in one revolution, encoder ID, multi-turn, encoder error

DATA_ID_6 

EEPROM write

DATA_ID_7 

Reset

DATA_ID_8 

Reset

DATA_ID_C 

Reset

DATA_ID_D 

EEPROM read

DATA_ID_NUM 

Number of Data ID codes

Function Documentation

◆ tamagawa_command_process()

int32_t tamagawa_command_process ( volatile struct tamagawa_uart_interface tamagawa_interface,
UART_Handle gUartHandle,
int32_t  cmd 
)

Process The Tamagawa Command.

Parameters
[in]tamagawa_interfaceTamagawa Interface
[in]gUartHandleuart handle
[in]cmdtamagawa command number
Return values
0success
-EINVALfailure

◆ tamagawa_crc_verify()

int32_t tamagawa_crc_verify ( volatile struct tamagawa_uart_interface tamagawa_interface)

Compare Received CRC and Calculated CRC.

Parameters
[in]tamagawa_interfaceTamagawa Interface
Return values
1CRC Success
0CRC failure

◆ tamagawa_init()

void tamagawa_init ( volatile struct tamagawa_uart_interface tamagawa_interface,
uint32_t  instance,
uint32_t  base_address,
uint32_t  pin_number,
uint32_t  pin_direction 
)

Configure GOPIO pin for RTSn(sw flow control)

Parameters
[in]tamagawa_interfaceTamagawa Interface
[in]instanceUART communication instance
[in]base_addressGPIO PIN address
[in]pin_numberGPIO PIN Number
[in]pin_directionGPIO pin direction (output/input)