AM263x MCU+ SDK  08.06.00

Introduction

===========================================================================

@{

Enumerations

enum  SDL_STC_TestResult {
  SDL_STC_COMPLETED_SUCCESS, SDL_STC_COMPLETED_FAILURE, SDL_STC_NOT_COMPLETED, SDL_STC_NOT_RUN,
  INVALID_RESULT
}
 
enum  SDL_STC_TestType { SDL_STC_TEST, SDL_STC_NEG_TEST, INVALID_TEST }
 

DCC Operation Mode

typedef uint32_t SDL_DCC_mode
 Enum to select the DCC Operation Mode. More...
 
#define SDL_DCC_MODE_SINGLE_SHOT   (DCC_DCCGCTRL_SINGLESHOT_MODE)
 
#define SDL_DCC_MODE_CONTINUOUS   (DCC_DCCGCTRL_SINGLESHOT_DISABLE)
 

DCC Clock source of COUNT0

typedef uint32_t SDL_DCC_clkSrc0
 Enum to select the COUNT0 clock source. More...
 
#define SDL_DCC_CLK0_SRC_CLOCK0_0   (DCC_DCCCLKSRC0_CLKSRC0_0)
 
#define SDL_DCC_CLK0_SRC_CLOCK0_1   (DCC_DCCCLKSRC0_CLKSRC0_1)
 
#define SDL_DCC_CLK0_SRC_CLOCK0_2   (DCC_DCCCLKSRC0_CLKSRC0_2)
 

DCC Clock source of COUNT1

typedef uint32_t SDL_DCC_clkSrc1
 Enum to select the COUNT1 clock source. More...
 
#define SDL_DCC_CLK1_SRC_CLOCKSRC0   (DCC_DCCCLKSRC1_CLKSRC_0)
 
#define SDL_DCC_CLK1_SRC_CLOCKSRC1   (DCC_DCCCLKSRC1_CLKSRC_1)
 
#define SDL_DCC_CLK1_SRC_CLOCKSRC2   (DCC_DCCCLKSRC1_CLKSRC_2)
 
#define SDL_DCC_CLK1_SRC_CLOCKSRC3   (DCC_DCCCLKSRC1_CLKSRC_3)
 
#define SDL_DCC_CLK1_SRC_CLOCKSRC4   (DCC_DCCCLKSRC1_CLKSRC_4)
 
#define SDL_DCC_CLK1_SRC_CLOCKSRC5   (DCC_DCCCLKSRC1_CLKSRC_5)
 
#define SDL_DCC_CLK1_SRC_CLOCKSRC6   (DCC_DCCCLKSRC1_CLKSRC_6)
 
#define SDL_DCC_CLK1_SRC_CLOCKSRC7   (DCC_DCCCLKSRC1_CLKSRC_7)
 
#define SDL_DCC_CLK1_SRC_FICLK   (SDL_DCC2_DCCCLKSRC1_CLKSRC_OTHER)
 

DCC Interrupt type

typedef uint32_t SDL_DCC_intrType
 Enum for DCC interrupts. More...
 
#define SDL_DCC_INTERRUPT_ERR   (0x0U)
 
#define SDL_DCC_INTERRUPT_DONE   (0x1U)
 

Macro Definition Documentation

◆ SDL_DCC_MODE_SINGLE_SHOT

#define SDL_DCC_MODE_SINGLE_SHOT   (DCC_DCCGCTRL_SINGLESHOT_MODE)

Stop counting when counter0 and valid0 both reach zero

◆ SDL_DCC_MODE_CONTINUOUS

#define SDL_DCC_MODE_CONTINUOUS   (DCC_DCCGCTRL_SINGLESHOT_DISABLE)

< Stop counting when counter1 reaches zero Continuously repeat (until error)

◆ SDL_DCC_CLK0_SRC_CLOCK0_0

#define SDL_DCC_CLK0_SRC_CLOCK0_0   (DCC_DCCCLKSRC0_CLKSRC0_0)

SYS_CLK1 is selected as source for COUNT0

◆ SDL_DCC_CLK0_SRC_CLOCK0_1

#define SDL_DCC_CLK0_SRC_CLOCK0_1   (DCC_DCCCLKSRC0_CLKSRC0_1)

SYS_CLK2 is selected as source for COUNT0

◆ SDL_DCC_CLK0_SRC_CLOCK0_2

#define SDL_DCC_CLK0_SRC_CLOCK0_2   (DCC_DCCCLKSRC0_CLKSRC0_2)

XREF_CLK is selected as source for COUNT0

◆ SDL_DCC_CLK1_SRC_CLOCKSRC0

#define SDL_DCC_CLK1_SRC_CLOCKSRC0   (DCC_DCCCLKSRC1_CLKSRC_0)

TEST_CLK0 is selected as source for COUNT1

◆ SDL_DCC_CLK1_SRC_CLOCKSRC1

#define SDL_DCC_CLK1_SRC_CLOCKSRC1   (DCC_DCCCLKSRC1_CLKSRC_1)

TEST_CLK1 is selected as source for COUNT1

◆ SDL_DCC_CLK1_SRC_CLOCKSRC2

#define SDL_DCC_CLK1_SRC_CLOCKSRC2   (DCC_DCCCLKSRC1_CLKSRC_2)

TEST_CLK2 is selected as source for COUNT1

◆ SDL_DCC_CLK1_SRC_CLOCKSRC3

#define SDL_DCC_CLK1_SRC_CLOCKSRC3   (DCC_DCCCLKSRC1_CLKSRC_3)

TEST_CLK3 is selected as source for COUNT1

◆ SDL_DCC_CLK1_SRC_CLOCKSRC4

#define SDL_DCC_CLK1_SRC_CLOCKSRC4   (DCC_DCCCLKSRC1_CLKSRC_4)

TEST_CLK4 is selected as source for COUNT1

◆ SDL_DCC_CLK1_SRC_CLOCKSRC5

#define SDL_DCC_CLK1_SRC_CLOCKSRC5   (DCC_DCCCLKSRC1_CLKSRC_5)

TEST_CLK5 is selected as source for COUNT1

◆ SDL_DCC_CLK1_SRC_CLOCKSRC6

#define SDL_DCC_CLK1_SRC_CLOCKSRC6   (DCC_DCCCLKSRC1_CLKSRC_6)

TEST_CLK6 is selected as source for COUNT1

◆ SDL_DCC_CLK1_SRC_CLOCKSRC7

#define SDL_DCC_CLK1_SRC_CLOCKSRC7   (DCC_DCCCLKSRC1_CLKSRC_7)

TEST_CLK7 is selected as source for COUNT1

◆ SDL_DCC_CLK1_SRC_FICLK

#define SDL_DCC_CLK1_SRC_FICLK   (SDL_DCC2_DCCCLKSRC1_CLKSRC_OTHER)

OTHER_CLK is selected as source for COUNT1

◆ SDL_DCC_INTERRUPT_ERR

#define SDL_DCC_INTERRUPT_ERR   (0x0U)

The error signal

◆ SDL_DCC_INTERRUPT_DONE

#define SDL_DCC_INTERRUPT_DONE   (0x1U)

Done interrupt signal

Typedef Documentation

◆ SDL_DCC_mode

typedef uint32_t SDL_DCC_mode

Enum to select the DCC Operation Mode.

    DCC can either operate in single shot or continuous mode.

◆ SDL_DCC_clkSrc0

typedef uint32_t SDL_DCC_clkSrc0

Enum to select the COUNT0 clock source.

◆ SDL_DCC_clkSrc1

typedef uint32_t SDL_DCC_clkSrc1

Enum to select the COUNT1 clock source.

◆ SDL_DCC_intrType

typedef uint32_t SDL_DCC_intrType

Enum for DCC interrupts.

Enumeration Type Documentation

◆ SDL_STC_TestResult

Enumerator
SDL_STC_COMPLETED_SUCCESS 

The STC completed and the test passed

SDL_STC_COMPLETED_FAILURE 

The STC completed and the test failed

SDL_STC_NOT_COMPLETED 

The STC was active but could not be completed.

SDL_STC_NOT_RUN 

The STC was not performed on this device

INVALID_RESULT 

The STC was not performed on this device

◆ SDL_STC_TestType

Enumerator
SDL_STC_TEST 

The STC test should be completed and the test passed for this testType

SDL_STC_NEG_TEST 

The STC test should be completed and the test failed for this testType

INVALID_TEST