AM263x MCU+ SDK  08.06.00

Introduction

This module contains APIs to program and use the SPINLOCK module.

Files

file  spinlock/v0/spinlock.h
 SPINLOCK Driver API/interface file.
 

Functions

uint32_t Spinlock_getNumLocks (uint32_t baseAddr)
 This API provides returns the number of locks supported. More...
 
int32_t Spinlock_lock (uint32_t baseAddr, uint32_t lockNumber)
 This API performs the Read operation for Lock status of the SPINLOCK_LOCK_REG, in order to acquire a Spinlock. More...
 
void Spinlock_unlock (uint32_t baseAddr, uint32_t lockNumber)
 This API performs the write operation for Lock status of the SPINLOCK_LOCK_REG, in order to Free the lock If lockNumber is invalid (out of range), no operation is performed Lock state : Write 0x0: Set the lock to Not Taken(Free) Write 0x1: No update to the lock value. More...
 

Macros

#define SPINLOCK_LOCK_STATUS_FREE   (0U)
 Flag to indicate spinlock is free. More...
 
#define SPINLOCK_LOCK_STATUS_INUSE   (1U)
 Flag to indicate spinlock is in use. More...
 

Macro Definition Documentation

◆ SPINLOCK_LOCK_STATUS_FREE

#define SPINLOCK_LOCK_STATUS_FREE   (0U)

Flag to indicate spinlock is free.

◆ SPINLOCK_LOCK_STATUS_INUSE

#define SPINLOCK_LOCK_STATUS_INUSE   (1U)

Flag to indicate spinlock is in use.

Function Documentation

◆ Spinlock_getNumLocks()

uint32_t Spinlock_getNumLocks ( uint32_t  baseAddr)

This API provides returns the number of locks supported.

Parameters
baseAddrMemory address of SPINLOCK module
Returns
Number of locks in an instance

◆ Spinlock_lock()

int32_t Spinlock_lock ( uint32_t  baseAddr,
uint32_t  lockNumber 
)

This API performs the Read operation for Lock status of the SPINLOCK_LOCK_REG, in order to acquire a Spinlock.

Parameters
baseAddrMemory address of SPINLOCK module
lockNumberLock number in Spinlock module that should be acquired
Returns
Status of the Lock Register Lock state : SPINLOCK_LOCK_STATUS_FREE: Lock was previously NOT Taken (Free). The requester is granted the lock SPINLOCK_LOCK_STATUS_INUSE: Lock was previously Taken (Not Free). The requester is not granted the lock and must retry SystemP_FAILURE: lockNumber is invalid (out of range)

◆ Spinlock_unlock()

void Spinlock_unlock ( uint32_t  baseAddr,
uint32_t  lockNumber 
)

This API performs the write operation for Lock status of the SPINLOCK_LOCK_REG, in order to Free the lock If lockNumber is invalid (out of range), no operation is performed Lock state : Write 0x0: Set the lock to Not Taken(Free) Write 0x1: No update to the lock value.

Parameters
baseAddrMemory address of SPINLOCK module
lockNumberLock number in Spinlock module that should be released