This file contains the type definitions and helper macros for the Enet Module interface.
Go to the source code of this file.
Data Structures | |
| struct | EnetMod_Obj |
| Ethernet Module object. More... | |
Macros | |
| #define | ENET_MOD(mod) ((EnetMod_Handle)mod) |
| Convert module specific handle to EnetMod generic handle. More... | |
Typedefs | |
| typedef struct EnetMod_Obj_s * | EnetMod_Handle |
| Ethernet Module handle. More... | |
| typedef int32_t(*const | EnetMod_Open) (EnetMod_Handle hMod, Enet_Type enetType, uint32_t instId, const void *cfg, uint32_t cfgSize) |
| Open and initialize the Enet Module. More... | |
| typedef int32_t(*const | EnetMod_Rejoin) (EnetMod_Handle hMod, Enet_Type enetType, uint32_t instId) |
| Rejoin the Enet Module. More... | |
| typedef int32_t(*const | EnetMod_Ioctl) (EnetMod_Handle hMod, uint32_t cmd, Enet_IoctlPrms *prms) |
| Issue an operation on the Enet Module. More... | |
| typedef void(*const | EnetMod_Close) (EnetMod_Handle hMod) |
| Close the Enet Module. More... | |
Functions | |
| int32_t | EnetMod_open (EnetMod_Handle hMod, Enet_Type enetType, uint32_t instId, const void *cfg, uint32_t cfgSize) |
| Wrapper to open and initialize an Enet Module. More... | |
| int32_t | EnetMod_rejoin (EnetMod_Handle hMod, Enet_Type enetType, uint32_t instId) |
| Wrapper to rejoin an Enet Module. More... | |
| int32_t | EnetMod_ioctl (EnetMod_Handle hMod, uint32_t cmd, Enet_IoctlPrms *prms) |
| Wrapper function to issue an operation on an Enet Module. More... | |
| int32_t | EnetMod_ioctlFromIsr (EnetMod_Handle hMod, uint32_t cmd, Enet_IoctlPrms *prms) |
| Wrapper function to issue an operation on an Enet Module from ISR context. More... | |
| void | EnetMod_close (EnetMod_Handle hMod) |
| Wrapper function to close an Enet Module. More... | |
| static bool | EnetMod_isOpen (EnetMod_Handle hMod) |
| Check if Enet Module is open or not. More... | |
| #define ENET_MOD | ( | mod | ) | ((EnetMod_Handle)mod) |
Convert module specific handle to EnetMod generic handle.
| typedef struct EnetMod_Obj_s* EnetMod_Handle |
Ethernet Module handle.
Ethernet Module handle used to call any EnetMod related APIs.
| typedef int32_t(*const EnetMod_Open) (EnetMod_Handle hMod, Enet_Type enetType, uint32_t instId, const void *cfg, uint32_t cfgSize) |
Open and initialize the Enet Module.
Opens and initializes the Enet Module with the configuration parameters provided by the caller.
| hMod | Enet Module handle |
| enetType | Enet Peripheral type |
| instId | Enet Peripheral instance id |
| cfg | Configuration parameters |
| cfgSize | Size of the configuration parameters |
| typedef int32_t(* const EnetMod_Rejoin) (EnetMod_Handle hMod, Enet_Type enetType, uint32_t instId) |
Rejoin the Enet Module.
Reopens the Enet Module, but doesn't perform any hardware initialization. This function is expected to be called to attach to a running module.
| hMod | Enet Module opaque handle |
| enetType | Enet Peripheral type |
| instId | Enet Peripheral instance id |
| typedef int32_t(* const EnetMod_Ioctl) (EnetMod_Handle hMod, uint32_t cmd, Enet_IoctlPrms *prms) |
Issue an operation on the Enet Module.
Issues a control operation on the Enet Module.
| hMod | Enet Module opaque handle |
| cmd | IOCTL command Id |
| prms | IOCTL parameters |
| typedef void(* const EnetMod_Close) (EnetMod_Handle hMod) |
Close the Enet Module.
Closes the Enet Module.
| hMod | Enet Module opaque handle |
| int32_t EnetMod_open | ( | EnetMod_Handle | hMod, |
| Enet_Type | enetType, | ||
| uint32_t | instId, | ||
| const void * | cfg, | ||
| uint32_t | cfgSize | ||
| ) |
Wrapper to open and initialize an Enet Module.
| hMod | Enet Module handle |
| enetType | Enet Peripheral type |
| instId | Enet Peripheral instance id |
| cfg | Configuration parameters |
| cfgSize | Size of the configuration parameters |
| int32_t EnetMod_rejoin | ( | EnetMod_Handle | hMod, |
| Enet_Type | enetType, | ||
| uint32_t | instId | ||
| ) |
Wrapper to rejoin an Enet Module.
| hMod | Enet Module handle |
| enetType | Enet Peripheral type |
| instId | Enet Peripheral instance id |
| int32_t EnetMod_ioctl | ( | EnetMod_Handle | hMod, |
| uint32_t | cmd, | ||
| Enet_IoctlPrms * | prms | ||
| ) |
Wrapper function to issue an operation on an Enet Module.
| hMod | Enet Module handle |
| cmd | IOCTL command Id |
| prms | IOCTL parameters |
| int32_t EnetMod_ioctlFromIsr | ( | EnetMod_Handle | hMod, |
| uint32_t | cmd, | ||
| Enet_IoctlPrms * | prms | ||
| ) |
Wrapper function to issue an operation on an Enet Module from ISR context.
| hMod | Enet Module handle |
| cmd | IOCTL command Id |
| prms | IOCTL parameters |
| void EnetMod_close | ( | EnetMod_Handle | hMod | ) |
Wrapper function to close an Enet Module.
| hMod | Enet Module handle |
|
inlinestatic |
Check if Enet Module is open or not.
| hMod | Enet Module handle |