This file contains the type definitions and helper macros for the Enet CPDMA data path (DMA) interface.
Go to the source code of this file.
Data Structures | |
| struct | EnetCpdma_PktTsInfo |
| CPPI buffer timestamp info. More... | |
| struct | EnetCpdma_SGListEntry |
| Transmit Packet scatter gather list entry. More... | |
| struct | EnetCpdma_SGList |
| Transmit packet scatter list info. More... | |
| struct | EnetCpdma_PktInfo |
| Packet data structure. More... | |
| struct | EnetCpdma_OpenTxChPrms |
| Param struct for the TX channel open function. More... | |
| struct | EnetCpdma_OpenRxChPrms |
| Param struct for the RX channel open function. More... | |
| struct | EnetCpdma_RxChInitPrms |
| Global Param struct for the Rx channel open. More... | |
| struct | EnetCpdma_Cfg |
| Config structure for Enet CPDMA. More... | |
| struct | EnetDma_initCfg |
| Config structure for Enet CPDMA Data Path initialization. More... | |
Macros | |
| #define | ENET_CPDMA_CPSW_MAX_SG_LIST (4U) |
| #define | ENET_CPDMA_CSUM_START_BYTE_SHIFT (16U) |
| #define | ENET_CPDMA_CSUM_START_BYTE_MASK (((uint32_t) 0xFFU) << ENET_CPDMA_CSUM_START_BYTE_SHIFT) |
| #define | ENET_CPDMA_CSUM_RESULT_BYTE_SHIFT (24U) |
| #define | ENET_CPDMA_CSUM_RESULT_BYTE_MASK (((uint32_t) 0xFFU) << ENET_CPDMA_CSUM_RESULT_BYTE_SHIFT) |
| #define | ENET_CPDMA_CSUM_BYTE_COUNT_SHIFT (0U) |
| #define | ENET_CPDMA_CSUM_BYTE_COUNT_MASK (((uint32_t) 0x3FFU) << ENET_CPDMA_CSUM_BYTE_COUNT_SHIFT) |
| #define | ENET_CPDMA_GET_CSUM_RESULT_BYTE(chkSumInfo) ENET_FEXT(chkSumInfo, ENET_CPDMA_CSUM_RESULT_BYTE) |
| #define | ENET_CPDMA_GET_CSUM_START_BYTE(chkSumInfo) ENET_FEXT(chkSumInfo, ENET_CPDMA_CSUM_START_BYTE) |
| #define | ENET_CPDMA_GET_CSUM_BYTE_COUNT(chkSumInfo) ENET_FEXT(chkSumInfo, ENET_CPDMA_CSUM_BYTE_COUNT) |
Enet CPDMA instance configuration | |
Configuration macros for Enet CPDMA module. | |
| #define | ENET_CPDMA_CPSW_MAX_TX_CH (8U) |
| Maximum number of CPSW TX DMA channels. More... | |
| #define | ENET_CPDMA_CPSW_MAX_RX_CH (8U) |
| Maximum number of CPSW RX DMA channels. More... | |
Typedefs | |
| typedef EnetCpdma_SGListEntry | EnetDma_SGListEntry |
| typedef EnetCpdma_OpenRxChPrms | EnetDma_OpenRxChPrms |
| Param struct for the RX channel open function. We include this typedef as top level DMA APIs use EnetDma_OpenRxChPrms struct. More... | |
Enet DMA driver opaque handles | |
Enet DMA configuration structure. Opaque handle typedefs for Enet DMA driver objects. | |
| typedef struct EnetCpdma_Cfg_s | EnetDma_Cfg |
| Opaque handle that holds config Info for Enet DMA channel. More... | |
| typedef void(* | EnetDma_PktNotifyCb) (void *cbArg) |
| Function pointer type for packet notify call back. More... | |
Functions | |
| EnetDma_Handle | EnetCpdma_open (Enet_Type enetType, uint32_t instId, const void *dmaCfg, uint32_t appCoreId) |
| Set default data path parameters. More... | |
| int32_t | EnetCpdma_close (EnetDma_Handle hEnetDma) |
| Close Enet DMA (data path). More... | |
| int32_t | EnetCpdma_rxThreshIsr (EnetDma_Handle hEnetDma) |
| ENET CPDMA Rx Threshold interrupt service routine. More... | |
| int32_t | EnetCpdma_rxIsr (EnetDma_Handle hEnetDma) |
| ENET CPDMA Rx interrupt service routine. More... | |
| int32_t | EnetCpdma_txIsr (EnetDma_Handle hEnetDma) |
| ENET CPDMA Tx interrupt service routine. More... | |
| int32_t | EnetCpdma_miscIsrGetStatus (EnetDma_Handle hEnetDma, uint32_t *pStatusMask) |
| ENET CPDMA Miscellaneous interrupt service routine. More... | |
| int32_t | EnetCpdma_ackMiscIsr (EnetDma_Handle hEnetDma) |
| void | EnetCpdma_initParams (Enet_Type enetType, EnetDma_Cfg *pDmaConfig) |
| Initialize CPDMA config params. More... | |