|
AM263x MCU+ SDK
08.06.00
|
|
Go to the documentation of this file.
68 #define DP83869_LED_NUM (4U)
77 typedef enum Dp83869_Gpio0Mode_e
110 typedef enum Dp83869_Gpio1Mode_e
143 typedef enum Dp83869_LedMode_e
191 typedef struct Dp83869_Cfg_s
uint8_t txFifoDepth
Definition: dp83869.h:206
@ DP83869_GPIO0_RXERR
Definition: dp83869.h:80
@ DP83869_GPIO0_1588RXSFD
Definition: dp83869.h:86
void Dp83869_initCfg(Dp83869_Cfg *cfg)
Initialize DP83869 PHY specific config params.
@ DP83869_LED_LINKED
Definition: dp83869.h:146
@ DP83869_LED_TXACT
Definition: dp83869.h:152
uint32_t impedanceInMilliOhms
Definition: dp83869.h:213
@ DP83869_GPIO1_ENERGYDET
Definition: dp83869.h:125
@ DP83869_GPIO1_COL
Definition: dp83869.h:113
Dp83869_LedMode
LED modes (sources).
Definition: dp83869.h:144
uint32_t txDelayInPs
Definition: dp83869.h:200
@ DP83869_LED_LINKED_100BTX
Definition: dp83869.h:164
@ DP83869_LED_RXACT
Definition: dp83869.h:155
Dp83869_Gpio0Mode
GPIO_0 mux modes.
Definition: dp83869.h:78
@ DP83869_LED_RXTXERR
Definition: dp83869.h:182
uint32_t rxDelayInPs
Definition: dp83869.h:203
@ DP83869_GPIO1_CONSTANT0
Definition: dp83869.h:134
@ DP83869_GPIO1_CONSTANT1
Definition: dp83869.h:137
@ DP83869_LED_RXERR
Definition: dp83869.h:185
@ DP83869_LED_LINKED_1000BT
Definition: dp83869.h:161
DP83869 PHY configuration parameters.
Definition: dp83869.h:192
@ DP83869_LED_RXTXACT
Definition: dp83869.h:149
uint32_t idleCntThresh
Definition: dp83869.h:209
@ DP83869_GPIO0_CONSTANT1
Definition: dp83869.h:104
@ DP83869_GPIO0_PRBSERR
Definition: dp83869.h:98
bool txClkShiftEn
Definition: dp83869.h:194
Dp83869_Gpio1Mode
GPIO_1 mux modes.
Definition: dp83869.h:111
@ DP83869_GPIO0_1588TXSFD
Definition: dp83869.h:83
@ DP83869_GPIO0_WOL
Definition: dp83869.h:89
#define DP83869_LED_NUM
Number of LEDs available in the PHY.
Definition: dp83869.h:68
@ DP83869_LED_LINKED_1001000BT
Definition: dp83869.h:173
@ DP83869_GPIO0_ENERGYDET
Definition: dp83869.h:92
@ DP83869_LED_LINKED_10BT
Definition: dp83869.h:167
@ DP83869_GPIO1_PRBSERR
Definition: dp83869.h:131
@ DP83869_GPIO1_1588TXSFD
Definition: dp83869.h:116
@ DP83869_GPIO1_WOL
Definition: dp83869.h:122
@ DP83869_LED_COLLDET
Definition: dp83869.h:158
@ DP83869_GPIO1_1588RXSFD
Definition: dp83869.h:119
bool rxClkShiftEn
Definition: dp83869.h:197
@ DP83869_GPIO0_LED3
Definition: dp83869.h:95
@ DP83869_LED_LINKED_10100BT
Definition: dp83869.h:170
Dp83869_Gpio0Mode gpio0Mode
Definition: dp83869.h:216
@ DP83869_GPIO1_LED3
Definition: dp83869.h:128
@ DP83869_LED_FULLDUPLEX
Definition: dp83869.h:176
Dp83869_Gpio1Mode gpio1Mode
Definition: dp83869.h:219
@ DP83869_LED_LINKED_BLINKACT
Definition: dp83869.h:179
@ DP83869_GPIO0_CONSTANT0
Definition: dp83869.h:101