AM263x MCU+ SDK  08.06.00
Security

Introduction

Getting started

The HSM or Hardware security Module is a subsystem that acts as the secure host by offering security services to the rest of the system. TI offers HS-FS (High Security - Field Securable) as the primary device for the customers. The MCU+ SDK supports HS-FS device type for AM263x. It supports loading the HSM firmware (TIFS-MCU) via SBL (Secondary Boot Loader), which enables access to the hardware resources for cryptographic operations for R5FSS.

Bootloader_socLoadHsmRtFw

The SBL for AM263x supports for loading firmware on the HSM. The firmware is provided in an encrypted form at source/drivers/hsmclient/soc/hsmRtImg.h. The function Bootloader_socLoadHsmRtFw sends a message to ROM and ROM loads the HSM firmware. After the HSM firmware is loaded and has done its init time operations, it sends a message to the SBL called HSM_MSG_BOOT_NOTIFY.

int main()
{
...
Drivers_open();
Bootloader_profileAddProfilePoint("Drivers_open");
DebugP_log("\r\n");
Bootloader_socLoadHsmRtFw(gHsmRtFw, HSMRT_IMG_SIZE_IN_BYTES);
Bootloader_profileAddProfilePoint("LoadHsmRtFw");
DebugP_log("Starting QSPI Bootloader ... \r\n");
...
}

Resources available

By default, the access to the crypto resources are firewalled on HS-FS devices. The HSM firmware so loaded, bypasses the firewalls and makes the following crypto modules available for the R5FSS to use.

  • AES (public context)
  • SHA (public context)
  • PKA
  • TRNG

This provides ability for the R5F core to be able to do the following computations:

  • AES encryption/decryption
  • SHA/HMAC hash calculation
  • RSA encryption/decryption, signing/verification
  • ECDSA encryption/decryption, signing/verification

SBL should always wait for HSM_MSG_BOOT_NOTIFY before using the crypto accelerator because HSM firmware initializes these firewalls. Failing to do so, the SBL or application may run into abort exception while accessing the MMR regions for the crypto accelerator.

Services

The TIFS-MCU firmware that gets loaded on HSM provides the following services.

  • Get Version
    • This service when invoked provides the version of the TIFS-MCU firmware loaded on HSM. Please refer to HSM Services Example.
  • Get UID
    • This service when invoked provides the unique identifier (UID) of the device. Please refer to HSM Services Example.

Modules

This page links to sub modules that enable authentication, data integrity and its confidentiality with the on-chip hardware accelarators.

The cryptographic accelarator on this device is supported via these modules in the SDK:

  • Cryptography Modules
    • DTHE (Data Transform and Hashing Engine)
      • Description of DTHE architecture and APIs available to use AES and SHA engine.
Note
EDMA support for AES and SHA will be added in future releases. Currently, the drivers only operate in CPU mode of data copy.