AM263x MCU+ SDK  08.06.00
Release Notes 08.02.01

Attention
Also refer to individual module pages for more details on each feature, unsupported features, important usage guidelines.
Note
The examples will show usage of SW modules and APIs on a specific CPU instance and OS combination.
Unless explicitly noted otherwise, the SW modules would work in both FreeRTOS and no-RTOS environment.
Unless explicitly noted otherwise, the SW modules would work on any of the R5F's present on the SOC.

New in this Release

Feature Module
AM263x LaunchPad support board/EVM support
MCSPI DMA mode of operation drivers
ADC burst mode oversampling example drivers
Ramp wave and random voltage examples for DAC peripheral drivers
Driver APIs and sysconfig support for EPWM XCMP feature drivers
FSI TX delay line API, SOC Address translation APIs drivers
CPSW Enhaced Scheduled Traffic (EST) support drivers
CpuId and Queue implementation DPL

Device and Validation Information

SOC Supported CPUs EVM Host PC
AM263x R5F AM263x ControlCard (referred to as am263x-cc in code).
Limited validation done with this release (08.02.01) on AM263x ControlCard. Please use 08.02.00 SDK for ControlCard
Windows 10 64b or Ubuntu 18.04 64b
AM263x R5F AM263x LaunchPad (referred to as am263x-lp in code) Windows 10 64b or Ubuntu 18.04 64b

Dependent Tools and Compiler Information

Tools Supported CPUs Version
Code Composer Studio R5F 12.1.0
SysConfig R5F 1.14.0, build 2667
TI ARM CLANG R5F 2.1.2.LTS
FreeRTOS Kernel R5F 10.4.3
LwIP R5F STABLE-2_1_2_RELEASE

Key Features

OS Kernel

OS Supported CPUs SysConfig Support Key features tested Key features not tested / NOT supported
FreeRTOS Kernel R5F NA Task, Task notification, interrupts, semaphores, mutexs, timers Task load measurement using FreeRTOS run time statistics APIs. Limited support for ROV features.
FreeRTOS POSIX R5F NA pthread, mqueue, semaphore, clock -
NO RTOS R5F NA See Driver Porting Layer (DPL) below -

Driver Porting Layer (DPL)

Module Supported CPUs SysConfig Support OS support Key features tested Key features not tested / NOT supported
Cache R5F YES FreeRTOS, NORTOS Cache write back, invalidate, enable/disable -
Clock R5F YES FreeRTOS, NORTOS Tick timer at user specified resolution, timeouts and delays -
CpuId R5F NA FreeRTOS, NORTOS Verify Core ID and Cluster ID that application is currently running on -
CycleCounter R5F NA FreeRTOS, NORTOS Measure CPU cycles using CPU specific internal counters -
Debug R5F YES FreeRTOS, NORTOS Logging and assert to any combo of: UART, CCS, shared memory -
Heap R5F NA FreeRTOS, NORTOS Create arbitrary heaps in user defined memory segments -
Hwi R5F YES FreeRTOS, NORTOS Interrupt register, enable/disable/restore, Interrupt prioritization -
MPU R5F YES FreeRTOS, NORTOS Setup MPU and control access to address space -
Semaphore R5F NA FreeRTOS, NORTOS Binary, Counting Semaphore, recursive mutexs with timeout -
Task R5F NA FreeRTOS Create, delete tasks -
Timer R5F YES FreeRTOS, NORTOS Configure arbitrary timers -

Secondary Bootloader (SBL)

Module Supported CPUs SysConfig Support OS support Key features tested Key features not tested / NOT supported
Bootloader R5FSS0-0 YES NORTOS Boot modes: QSPI, UART. All R5F's. RPRC, multi-core image format Force Dual Core Mode, Disable Dual Core Switch and R5SS1 only not tested

SOC Device Drivers

Peripheral Supported CPUs SysConfig Support DMA Supported Key features tested Key features not tested / NOT supported
ADC R5F YES Yes. Example: adc_soc_continuous_dma Single software triggered conversion, Multiple ADC trigger using PWM, Result read using DMA, EPWM trip through PPB limit, burst mode oversampling -
Bootloader R5F YES Yes. DMA enabled for SBL QSPI Boot modes: QSPI, UART. All R5F's -
CMPSS R5F YES NA Asynchronous PWM trip -
CPSW R5F YES No MAC loopback, PHY loopback, LWIP: Getting IP, Ping, Iperf, Layer 2 MAC, Layer 2 PTP Timestamping and CPSW Switch support -
DAC R5F YES Yes. Example: dac_sine_dma Constant voltage, Square wave generation, Sine wave generation with and without DMA, Ramp wave generation, Random Voltage generation -
ECAP R5F YES No ECAP APWM mode, PWM capture -
EDMA R5F YES NA DMA transfer using interrupt and polling mode, QDMA Transfer, Channel Chaining, PaRAM Linking -
EPWM R5F YES Yes. Example: epwm_dma PWM outputs A and B in up-down count mode, Trip zone, Update PWM using EDMA, Valley switching, High resolution time period adjustment XCMP feature not tested
EQEP R5F YES NA Speed and Position measurement. Frequency Measurement not tested
FSI R5F YES No RX, TX, polling, interrupt mode, single lane loopback. -
GPIO R5F YES NA Output, Input and Interrupt functionality -
I2C R5F YES No Controller mode, basic read/write -
IPC Notify R5F YES NA Mailbox functionality, IPC between RTOS/NORTOS CPUs M4F core
IPC Rpmsg R5F YES NA RPMessage protocol based IPC M4F core
MCAN R5F YES No RX, TX, interrupt and polling mode Bus Off
MCSPI R5F YES Yes. Example: mcspi_loopback_dma Controller/Peripheral mode, basic read/write, polling, interrupt and DMA mode -
MDIO R5F YES NA Register read/write, link status and link interrupt enable API -
MPU Firewall R5F YES NA Only compiled (Works only on HS-SE device) -
PINMUX R5F YES NA Tested with multiple peripheral pinmuxes -
PRUICSS R5F YES NA Tested with Ethercat FW HAL -
QSPI R5F YES Yes. Example: qspi_flash_dma_transfer Read direct, Write indirect, Read/Write commands, DMA for read -
SDFM R5F YES No Filter data read from CPU, Filter data read with PWM sync -
SOC R5F YES NA Lock/unlock MMRs, clock enable, set Hz, Xbar configuration -
SPINLOCK R5F NA NA Lock, unlock HW spinlocks -
UART R5F YES No Basic read/write at baud rate 115200, polling, interrupt mode HW flow control not tested, DMA mode not supported
WATCHDOG R5F YES NA Reset mode Interrupt mode

Board Device Drivers

Peripheral Supported CPUs SysConfig Support Key features tested Key features not tested
EEPROM R5F YES Only compiled -
ETHPHY R5F YES Tested with ethercat_peripheral_beckhoff_ssc_demo example -
FLASH R5F YES QSPI Flash -
LED R5F YES GPIO -

CMSIS

Module Supported CPUs SysConfig Support OS Support Key features tested Key features not tested
- - - - - -

Industrial Communications Toolkit

Module Supported CPUs SysConfig Support OS Support Key features tested Key features not tested
EtherCAT Peripheral FWHAL R5F NO FreeRTOS Tested with ethercat_peripheral_beckhoff_ssc_demo example Reset isolation

Motor Control

Module Supported CPUs SysConfig Support OS Support Key features tested Key features not tested
- - - - - -

Networking

Module Supported CPUs SysConfig Support OS Support Key features tested Key features not tested
LwIP R5F YES FreeRTOS TCP/UDP IP networking stack, DHCP, ping, TCP iperf, TCP/UDP IP Other LwIP features, performance and memory optimizations pending, more robustness tests pending
Ethernet driver (ENET) R5F YES FreeRTOS Ethernet as port using CPSW and ICSS,Layer 2 MAC, Layer 2 PTP Timestamping, CPSW Switch, CPSW EST -
ICSS-EMAC R5F YES FreeRTOS Only compiled Not tested

Demos

Module Supported CPUs SysConfig Support OS Support Key features tested Key features not tested
- - - - - -

Fixed Issues

ID Head Line Module Applicable Releases Applicable Devices Resolution/Comments
MCUSDK-2254 SBL QSPI bootmode is not working with DMA enabled SBL 08_02_01 AM263x EDMA Parameters were configured incorrectly. Enabled DMA by default in SBL SYSCFG.
MCUSDK-3398 Address translation for R5FSS1 is missing SBL 08_02_00 AM263x Fixed
MCUSDK-3408 sbl_uart_uniflash extra bytes written to the flash when flashing images SBL 08_02_00 AM263x Added a parameter actual file size in the uniflash header. This parameter will be used to determine how many bytes to flash
MCUSDK-3618 AM263x: ePWM_setPhaseShift() API function doesn't correctly configure TBPHS EPWM 08_02_00 AM263x EPWM_setPhaseShift() uses 16-bit read/write, but TBPHS is a 32-bit register. Hence EPWM_setPhaseShift() doesn't take effect. Problem is resolved in 32-bit read/write is used instead of 16-bit read/write.
MCUSDK-3773 Enet LWIP example fails with SBL on AM263X-LP SBL, LWIP 08_02_01 AM263x Increased the memory region for updated Descriptor memory
MCUSDK-3774 Multi Core application with SBL QSPI DMA enabled is failing on AM263X-LP EDMA, IPC_Notify, SBL 08_02_01 AM263x For R5SS0-1 core, 0x8000 is the address where reset vectors needs to be copied. But in SBL QSPI with DMA enabled, actual physical address need to be passed while copying reset vectors via EDMA. During SBL execution R5SS0-0 core runs in Lockstep mode so Virtual to Physical Address calculation need to use LockStep TCM Size i.e. 64KB but only 32KB(R5SS0-0) is used.Updated this API.
MCUSDK-3804 SDFM: API doc/comments: Valid value macros have unexpected CSL_ prefix SDFM 08_02_00 AM263x Fixed. Removed unwanted CSL_ prefix used in the documentation/comments for SDFM macros
MCUSDK-3823 Wrong boot mode documentation for LP Docs 08_02_01 AM263x Boot mode switch setting not consistent in LP and CC. Fixed BOOT MODE documentation in Getting Started -> EVM Setup page.
MCUSDK-3864 DAC: Incorrect reference voltage selection macros DAC 08_02_01 AM263x Fixed. enum DAC_ReferenceVoltage is now corrected with "DAC_REF_VREF and DAC_REF_VDDA" from "DAC_REF_VDAC and DAC_REF_ADC_VREFHI"
MCUSDK-3930 DAC Sysconfig: Incorrect argument passed to DAC_setPWMSyncSignal results in ASSERT DAC 08_02_01 AM263x Fixed. Sysconfig scripts fixed to pass correct argument (1-32 for EPWM0-EPWM31) as per the DAC_setPWMSyncSignal requirement
MCUSDK-3712 [FSI]Maximum value of external inputs for triggering frame transmission is limited to 32 SOC 08_00_00 onwards AM263x Fixed

Known Issues

ID Head Line Module Reported in release Workaround
MCUSDK-1016 Semaphore does not function as expected when "post" call is present in multiple ISRs at different priorities DPL, FreeRTOS 08_00_03 Disable interrupt nesting
MCUSDK-2252 GPIO Pin Direction GPIO. GPIO Pin Direction not getting automatically configured. 08_00_02 Use GPIO_setDirMode to set pin direction for GPIO pin.
MCUSDK-2464 ADC sysconfig code generation issue ADC 08_00_03 -
MCUSDK-2557 eqep_frequency_measurement example is failing SBL 08_02_00 -
MCUSDK-2703 Interrupt XBAR instance for FSI is static FSI 08_00_03 -
MCUSDK-3436 QSPI flashing fails with uniflash Flash 08_02_00 -
MCUSDK-3869 AM263x - LwIP ICMP tests fails Enet, LWIP 08_02_00 -
MCUSDK-3886 MDIO - Phy link issue for MAC PORT 1 on am263x-lp Enet, LWIP 08_02_01 -
SITARAAPPS-2040 Dual Core configuration issue with CSP 1.1.3 (Sitara MCU Device Support) on AM263x CSP Gel Scripts 08_02_01 Edit gel file as mentioned in Prerequisites while running multi core applications.

Limitations

ID Head Line Module Reported in release Workaround
- - - - -

Upgrade and Compatibility Information

Not Applicable

SOC Device Drivers

Module Affected API Change Additional Remarks
Bootloader SOC_rcmSetR5Clock, SOC_rcmGetR5Clock & SOC_rcmsetR5SysClock Added additional parameter cpuId to set R5F clock based on R5F Cluster 0 and 1. -
DAC DAC_setReferenceVoltage The enum DAC_ReferenceVoltage is now corrected with "DAC_REF_VREF and DAC_REF_VDDA" from "DAC_REF_VDAC and DAC_REF_ADC_VREFHI" -