Introduction
This example demonstrates the use of HSM services.
Two services are available.
- UID is a unique identifier for each device. It can be extracted using get_uid service.
- HSM get_version_service serves the client with TIFS-MCU version information.
Supported Combinations
| Parameter | Value |
| CPU + OS | r5fss0_0 nortos |
| Toolchain | ti-arm-clang |
| Boards | am263x-cc |
| Example folder | /examples/hsm_client/hsm_services/ |
Steps to Run the Example
Via SBL_qspi bootloader
Build sbl_qspi
cd ~/ti/mcu_plus_sdk
make -s -C examples/drivers/boot/sbl_qspi/am263x-cc/r5fss0-0_nortos/ti-arm-clang/ all DEVICE=am263x
Build sbl_uart_uniflash
cd ~/ti/mcu_plus_sdk
make -s -C examples/drivers/boot/sbl_uart_uniflash/am263x-cc/r5fss0-0_nortos/ti-arm-clang/ all DEVICE=am263x
Edit default_sbl_qspi.cfg to include the correct images
#-----------------------------------------------------------------------------#
# #
# DEFAULT CONFIGURATION FILE TO BE USED WITH THE FLASHWRITER SCRIPT #
# #
#-----------------------------------------------------------------------------#
#
# By default this config file,
# - points to pre-built flash writer, bootloader for this EVM
# - The application image points to relative path of the ipc echo application image for this EVM
# - Make sure this application is built before running this script
# - You can customized this config file to point to your own bootloader and/or application images
# - You can use --operation=flashverify if you just want to verify the flash contents and not flash the file.
#
# First point to sbl_uart_uniflash binary, which function's as a server to flash one or more files
--flash-writer=sbl_prebuilt/am263x-cc/sbl_uart_uniflash.release.tiimage
# Now send one or more files to flash or flashverify as needed. The order of sending files does not matter
# When sending bootloader make sure to flash at offset 0x0. ROM expects bootloader at offset 0x0
--file=sbl_prebuilt/am263x-cc/sbl_qspi.release.tiimage --operation=flash --flash-offset=0x0
# When sending application image, make sure to flash at offset 0x80000 (default) or to whatever offset your bootloader is configured for
--file=../../examples/drivers/hsmclient/hsm_services/am263x-cc/r5fss0-0_nortos/ti-arm-clang/hsm_services.release.appimage --operation=flash --flash-offset=0x80000
Sample output
On successful boot, following message will be seen on terminal.
Services Sample Output
Set board for UART boot
See EVM setup
Load image
Power cycle and load image via xmodem (teraterm/minicom, baud rate 115200bps)
Sample Output
On successful boot, following message will be seen on terminal. Please note that the R5F application has not been side-loaded yet.
Sample Output