AM263x MCU+ SDK  08.06.00
QSPI Flash Transfer

Introduction

This example demonstrates the data transfer from flash connected to QSPI interface

Supported Combinations

Parameter Value
CPU + OS r5fss0-0 freertos
r5fss0-0 nortos
Toolchain ti-arm-clang
Boards am263x-cc, am263x-lp,
Example folder examples/drivers/qspi/qspi_flash_transfer

Steps to Run the Example

Sample Output

Shown below is a sample output when the application is run,

[QSPI Flash Transfer Test] Starting ...
[QSPI Flash Transfer Test] Flash Manufacturer ID : 0x1
[QSPI Flash Transfer Test] Flash Device ID : 0x2018
[QSPI Flash Transfer Test] Executing Flash Erase on first block...
[QSPI Flash Transfer Test] Done !!!
[QSPI Flash Transfer Test] Performing Write-Read Test...
[QSPI Flash Transfer Test] Write-Read Test Passed!
All tests have passed!!