AM263x MCU+ SDK  08.06.00
ADC SOC software

Introduction

This example uses the ADC to perform an ADC SOC conversion triggered by software.

The example does the below

  • Configures SOC0 to be triggered by software.
  • Configures ADC interrupt 1 to be generated at end of conversion of SOC0.
  • Forces the SOC0 through software and waits for completion by polling ADC interrupt 1 status.

External Connections

  • ADC0_AIN0 pin should be connected to signals to be converted.

AM263X-CC

When using AM263x-CC with TMDSHSECDOCK (HSEC180 controlCARD Baseboard Docking Station)

  • Feed analog input (non-zero voltage) to HSEC Pin 12

AM263X-LP

When using AM263x-LP

  • Feed analog input (non-zero voltage) to boosterpack header J1/J3 Pin 23.

Supported Combinations

Parameter Value
CPU + OS r5fss0-0 nortos
Toolchain ti-arm-clang
Board am263x-cc, am263x-lp
Example folder examples/drivers/adc/adc_soc_software/

Steps to Run the Example

  • When using CCS projects to build, import the CCS project for the required combination and build it using the CCS project menu (see Using SDK with CCS Projects).
  • When using makefiles to build, note the required combination and build using make command (see Using SDK with Makefiles)
  • Establish connections as mentioned in External Connections section
  • Launch a CCS debug session and run the executable, see CCS Launch, Load and Run
  • View the ADC conversion results in UART console logs

See Also

ADC

Sample Output

Shown below is a sample output when the application is run,

ADC Software Triggered Conversion Test Started ...
ADC Software Triggered Conversion Test Passed!!
All tests have passed!!