Example Description :
This example shows oversamping on a given ADC channel, periodically triggered by EPWM. ADC1 Channel 2 is sampled by SOC (2-5) and are triggered by EPWMSOCA along with SOC 0 (sampling channel 0) and SOC 1 (sampling Channel 1).
SOC Configurations :
- SOC(0-5) are triggered by EPWMSOCA. Sample window is set at 16.
- SOC 0 samples on channel 0
- SOC 1 samples on channel 1
- SOC (2-5) sample on channel 2
INT Configurations
- ADC1INT1 is set for EOC/SOC5
ISR Configurations
- INTXbar0 is set for ADC1INT1.
- App_adcISR services this interrupt.
- reads the results for the SOC(0-5),
- freezes EPWM counter if required conversions are complete.
External Connections
- AM263X-CC
- Feed Analog Voltages on ADC 1 Channel 0 - HSEC PIN 18
- Feed Analog Voltages on ADC 1 Channel 1 - HSEC PIN 20
- Feed Analog Voltages on ADC 1 Channel 2 - HSEC PIN 21
- AM263X-LP
- Feed Analog Voltages on ADC 1 Channel 0 - J1/3 PIN 24
- Feed Analog Voltages on ADC 1 Channel 1 - J1/3 PIN 29
- Feed Analog Voltages on ADC 1 Channel 2 - J5/7 PIN 67
Watch Variables
- gAdc1Channel0Result - array of digital represented voltages on ADC1 channel 0
- gAdc1Channel1Result - array of digital represented voltages on ADC1 channel 1
- gAdc1Channel2Result - array of digital represented voltages on ADC1 channel 2
Supported Combinations
| Parameter | Value |
| CPU + OS | r5fss0-0 nortos |
| Toolchain | ti-arm-clang |
| Board | am263x-cc, am263x-lp |
| Example folder | examples/drivers/adc/adc_soc_oversampling/ |
Steps to Run the Example
- When using CCS projects to build, import the CCS project for the required combination and build it using the CCS project menu (see Using SDK with CCS Projects).
- When using makefiles to build, note the required combination and build using make command (see Using SDK with Makefiles)
- Establish connections as mentioned in External Connections section
- Launch a CCS debug session and run the executable, see CCS Launch, Load and Run
- Using watch variables, view the ADC conversion results.
- View the ADC conversion results in UART console logs
See Also
ADC
Sample Output
Shown below is a sample output when the application is run,
ADC SOC Oversampling Test Started ...
ADC 1 Channel 0 Channel 1 Channel 2
776 785 778
777 787 780
779 784 782
781 787 782
782 787 782
783 787 784
781 787 785
783 789 786
783 787 786
783 785 784
779 784 782
ADC SOC Oversampling Test Passed
All tests have passed!!