diff --git a/source/kernel/freertos/dpl/a53/ClockP_freertos_a53.c b/source/kernel/freertos/dpl/a53/ClockP_freertos_a53.c
index 20dd094f78..22c2e27de6 100644
--- a/source/kernel/freertos/dpl/a53/ClockP_freertos_a53.c
+++ b/source/kernel/freertos/dpl/a53/ClockP_freertos_a53.c
@@ -1,5 +1,5 @@
 /*
- *  Copyright (C) 2018-2021 Texas Instruments Incorporated
+ *  Copyright (C) 2018-2023 Texas Instruments Incorporated
  *
  *  Redistribution and use in source and binary forms, with or without
  *  modification, are permitted provided that the following conditions
@@ -87,6 +87,7 @@ void ClockP_init(void)
     timerHwiParams.intNum = gClockConfig.timerHwiIntNum;
     timerHwiParams.callback = ClockP_timerTickIsr;
     timerHwiParams.isPulse = 0;
+    timerHwiParams.priority = gClockConfig.intrPriority;
     HwiP_construct(&gClockCtrl.timerHwiObj, &timerHwiParams);
 
     /* start the tick timer */
diff --git a/source/kernel/freertos/dpl/common/SemaphoreP_freertos.c b/source/kernel/freertos/dpl/common/SemaphoreP_freertos.c
index 4664b93044..480e0ef477 100755
--- a/source/kernel/freertos/dpl/common/SemaphoreP_freertos.c
+++ b/source/kernel/freertos/dpl/common/SemaphoreP_freertos.c
@@ -44,27 +44,36 @@ typedef struct SemaphoreP_Struct_ {
 
 int32_t SemaphoreP_constructBinary(SemaphoreP_Object *obj, uint32_t initCount)
 {
-    SemaphoreP_Struct *pSemaphore = (SemaphoreP_Struct *)obj;
-    int32_t status;
+    SemaphoreP_Struct *pSemaphore = NULL;
+    int32_t status = SystemP_FAILURE;
 
     DebugP_assert(sizeof(SemaphoreP_Struct) <= sizeof(SemaphoreP_Object) );
 
-    pSemaphore->isRecursiveMutex = 0;
-    pSemaphore->semHndl = xSemaphoreCreateBinaryStatic(&pSemaphore->semObj);
-    if( pSemaphore->semHndl == NULL )
+    if(obj != NULL)
     {
-        status = SystemP_FAILURE;
+        pSemaphore = (SemaphoreP_Struct *)obj;
+        status = SystemP_SUCCESS;
     }
-    else
-    {
-        vQueueAddToRegistry(pSemaphore->semHndl, "Binary Sem (DPL)");
 
-        if(initCount == 1U)
+    if (SystemP_SUCCESS == status)
+    {
+        pSemaphore->isRecursiveMutex = 0;
+        pSemaphore->semHndl = xSemaphoreCreateBinaryStatic(&pSemaphore->semObj);
+        if( pSemaphore->semHndl == NULL )
         {
-            /* post a semaphore to increment initial count to 1 */
-            (void)xSemaphoreGive(pSemaphore->semHndl);
+            status = SystemP_FAILURE;
+        }
+        else
+        {
+            vQueueAddToRegistry(pSemaphore->semHndl, "Binary Sem (DPL)");
+
+            if(initCount == 1U)
+            {
+                /* post a semaphore to increment initial count to 1 */
+                (void)xSemaphoreGive(pSemaphore->semHndl);
+            }
+            status = SystemP_SUCCESS;
         }
-        status = SystemP_SUCCESS;
     }
 
     return status;
diff --git a/source/kernel/freertos/dpl/m4/ClockP_freertos_m4.c b/source/kernel/freertos/dpl/m4/ClockP_freertos_m4.c
index f127b8b39f..7cb209b9a6 100755
--- a/source/kernel/freertos/dpl/m4/ClockP_freertos_m4.c
+++ b/source/kernel/freertos/dpl/m4/ClockP_freertos_m4.c
@@ -1,5 +1,5 @@
 /*
- *  Copyright (C) 2018-2021 Texas Instruments Incorporated
+ *  Copyright (C) 2018-2023 Texas Instruments Incorporated
  *
  *  Redistribution and use in source and binary forms, with or without
  *  modification, are permitted provided that the following conditions
@@ -87,6 +87,7 @@ void ClockP_init(void)
     timerHwiParams.intNum = gClockConfig.timerHwiIntNum;
     timerHwiParams.callback = ClockP_timerTickIsr;
     timerHwiParams.isPulse = 0;
+    timerHwiParams.priority = gClockConfig.intrPriority;
     HwiP_construct(&gClockCtrl.timerHwiObj, &timerHwiParams);
 
     /* start the tick timer */
diff --git a/source/kernel/freertos/dpl/r5/ClockP_freertos_r5.c b/source/kernel/freertos/dpl/r5/ClockP_freertos_r5.c
index df5f7933b2..2fef9a383f 100755
--- a/source/kernel/freertos/dpl/r5/ClockP_freertos_r5.c
+++ b/source/kernel/freertos/dpl/r5/ClockP_freertos_r5.c
@@ -87,6 +87,7 @@ void ClockP_init(void)
     timerHwiParams.intNum = gClockConfig.timerHwiIntNum;
     timerHwiParams.callback = ClockP_timerTickIsr;
     timerHwiParams.isPulse = 0;
+    timerHwiParams.priority = gClockConfig.intrPriority;
     (void)HwiP_construct(&gClockCtrl.timerHwiObj, &timerHwiParams);
 
     /* start the tick timer */
diff --git a/source/kernel/freertos/dpl/r5/HwiP_armv7r_handlers_freertos.c b/source/kernel/freertos/dpl/r5/HwiP_armv7r_handlers_freertos.c
index ab5c13b978..94a8a9d043 100644
--- a/source/kernel/freertos/dpl/r5/HwiP_armv7r_handlers_freertos.c
+++ b/source/kernel/freertos/dpl/r5/HwiP_armv7r_handlers_freertos.c
@@ -33,6 +33,8 @@
 #include <kernel/dpl/HwiP.h>
 #include <kernel/nortos/dpl/r5/HwiP_armv7r_vim.h>
 #include <drivers/hw_include/csl_types.h>
+#include <drivers/hw_include/soc_config.h>
+#include <drivers/pmu.h>
 
 static volatile uint32_t gdummy;
 
@@ -44,7 +46,49 @@ void __attribute__((section(".text.hwi"))) HwiP_irq_handler_c(void);
 void __attribute__((interrupt("UNDEF"), section(".text.hwi"))) HwiP_reserved_handler(void);
 void __attribute__((interrupt("UNDEF"), section(".text.hwi"))) HwiP_undefined_handler(void);
 void __attribute__((interrupt("ABORT"), section(".text.hwi"))) HwiP_prefetch_abort_handler(void);
+#ifdef __cplusplus
+extern "C" {
+#endif
 void __attribute__((interrupt("ABORT"), section(".text.hwi"))) HwiP_data_abort_handler(void);
+#ifdef __cplusplus
+}
+#endif
+
+#ifdef INTR_PROF
+void __attribute__((section(".text.hwi"))) HwiP_irq_profile_c(uint32_t intNum)
+{
+    uint32_t idx = 0, exists = 1;
+
+    for(idx = 0; idx <= gHwiCtrlProf.traceInterruptedISRIndex; idx++)
+    {
+        if(gHwiCtrlProf.traceInterruptedISR[idx] == intNum)
+        {
+            gHwiCtrlProf.traceInterruptedISR[idx] = 0;
+            gHwiCtrlProf.traceInterruptedISRIndex --;
+            if(gHwiCtrlProf.traceInterruptedISRIndex == 0)
+            {
+                gHwiCtrlProf.readCounterStop = CSL_armR5PmuReadCntr(CSL_ARM_R5_PMU_CYCLE_COUNTER_NUM);
+                if(gHwiCtrlProf.readCounterStop > gHwiCtrlProf.readCounterStart)
+                {
+                    gHwiCtrlProf.pmuCountVal += gHwiCtrlProf.readCounterStop - gHwiCtrlProf.readCounterStart - gHwiCtrlProf.pmuCalibration;
+                }
+                else
+                {
+                    gHwiCtrlProf.pmuCountVal += (0xFFFFFFFFU - gHwiCtrlProf.readCounterStart) + gHwiCtrlProf.readCounterStop - gHwiCtrlProf.pmuCalibration;
+                }
+            }
+            exists = 0;
+            break;
+        }
+    }
+    if(exists)
+    {
+        gHwiCtrlProf.traceInterruptedISR[(gHwiCtrlProf.traceInterruptedISRIndex)] = intNum;
+        gHwiCtrlProf.traceInterruptedISRIndex ++;
+        gHwiCtrlProf.readCounterStart = CSL_armR5PmuReadCntr(CSL_ARM_R5_PMU_CYCLE_COUNTER_NUM);
+    }
+}
+#endif
 
 /* IRQ handler starts execution in HwiP_irq_handler, defined in portASM.S
  * After some initial assembly logic it then branches to this function.
@@ -66,6 +110,13 @@ void __attribute__((section(".text.hwi"))) HwiP_irq_handler_c(void)
     status = HwiP_getIRQ(&intNum);
     if(status==SystemP_SUCCESS)
     {
+        #ifdef INTR_PROF
+        if(gHwiCtrlProf.profileIntr == 1)
+        {
+            HwiP_irq_profile_c(intNum);
+        }
+        #endif
+
         uint32_t isPulse = HwiP_isPulse(intNum);
         HwiP_FxnCallback isr;
         void *args;
@@ -96,6 +147,13 @@ void __attribute__((section(".text.hwi"))) HwiP_irq_handler_c(void)
             HwiP_clearInt(intNum);
         }
         HwiP_ackIRQ(intNum);
+
+        #ifdef INTR_PROF
+        if(gHwiCtrlProf.profileIntr == 1)
+        {
+            HwiP_irq_profile_c(intNum);
+        }
+        #endif
     }
     else
     {
diff --git a/source/kernel/freertos/dpl/r5/HwiP_armv7r_handlers_freertos_asm.S b/source/kernel/freertos/dpl/r5/HwiP_armv7r_handlers_freertos_asm.S
index a9bd14ddde..a4d92f7233 100644
--- a/source/kernel/freertos/dpl/r5/HwiP_armv7r_handlers_freertos_asm.S
+++ b/source/kernel/freertos/dpl/r5/HwiP_armv7r_handlers_freertos_asm.S
@@ -48,25 +48,36 @@ HwiP_data_abort_handler:
          * instruction set) points to the second instruction beyond the address where
          * the exception was generated.
          */
-        SUB		lr, lr, #6
+
+        /*   Push used registers. */
+        PUSH	{r0-r4, r12}
+
+        /* SPSR has the snapshot of CPSR before data abort. Compare thumb state bit in SPSR */
+        MRS r0, SPSR
+        AND r1, r0, #0x20
+        CMP R1, #0
+
+        /* branches to label ARM_STATE if the thumb state bit is not set */
+        BEQ ARM_STATE
+        SUB lr, lr, #2
+        ARM_STATE:
+        SUB lr, lr, #4
+        END:
 
         /*   Push the return address and SPSR. */
         PUSH	{lr}
         MRS	lr, SPSR
         PUSH	{lr}
 
-        /*   Push used registers. */
-        PUSH	{r0-r4, r12}
-
         /*   Call the interrupt handler. */
         LDR	r1, HwiP_data_abort_handler_const
         BLX	r1
 
         /*  Restore used registers, LR and SPSR before  returning. */
-        POP	{r0-r4, r12}
         POP	{LR}
         MSR	SPSR_cxsf, LR
         POP	{LR}
+        POP	{r0-r4, r12}
         MOVS	PC, LR
 
 HwiP_data_abort_handler_const: .word HwiP_data_abort_handler_c