diff --git a/source/kernel/dpl/ClockP.h b/source/kernel/dpl/ClockP.h
index 04cf2c9ce5..a7ca3c73b7 100755
--- a/source/kernel/dpl/ClockP.h
+++ b/source/kernel/dpl/ClockP.h
@@ -79,6 +79,7 @@ typedef struct ClockP_Config_
     uint32_t timerInputClkHz; /**< Timer clock in units of Hz */
     uint32_t timerInputPreScaler; /**< Timer divider to apply to the input clock */
     uint32_t usecPerTick; /**< period of one timer tick in units of usecs */
+    uint8_t  intrPriority; /**< Tick Interrupt priority */
 
 } ClockP_Config;
 
@@ -228,6 +229,11 @@ uint64_t ClockP_ticksToUsec(uint32_t ticks);
 
 /**
  * \brief Get current time in units of usecs
+ * 
+ * \note This API shouldn't be called from an ISR with priority higher than 
+ *       that of Tick Interrupt. This is because Tick interrupt won't be able  
+ *       to preempt the current ISR and \ref ClockP_getTimeUsec may return 
+ *       incorrect value.
  */
 uint64_t ClockP_getTimeUsec(void);
 
diff --git a/source/kernel/dpl/CpuIdP.h b/source/kernel/dpl/CpuIdP.h
index 4ef2bc7ca7..2d9e1cba9f 100644
--- a/source/kernel/dpl/CpuIdP.h
+++ b/source/kernel/dpl/CpuIdP.h
@@ -75,6 +75,12 @@ typedef struct
  */
 void CSL_armR5GetCpuID(CSL_ArmR5CPUInfo *cpuInfo);
 
+/**
+ *  \brief Set current R5 Core to Standby mode
+ *
+ */
+void CSL_armR5SetWFIMode(void);
+
 /** @} */
 
 #ifdef __cplusplus
diff --git a/source/kernel/dpl/MmuP_armv8.h b/source/kernel/dpl/MmuP_armv8.h
index b242e15804..eebba28736 100644
--- a/source/kernel/dpl/MmuP_armv8.h
+++ b/source/kernel/dpl/MmuP_armv8.h
@@ -128,7 +128,7 @@ void MmuP_MapAttrs_init(MmuP_MapAttrs *attrs);
 /**
  * \brief Enable MMU sub-system
  */
-void MmuP_enable();
+void MmuP_enable(void);
 
 /**
  * \brief Disable MMU sub-system
@@ -140,7 +140,7 @@ void MmuP_disable(void);
  *
  * \return 0: MMU sub-system is disabled, 1: MMU sub-system is enabled
  */
-uint32_t MmuP_isEnabled();
+uint32_t MmuP_isEnabled(void);
 
 /* Memory map */
 
@@ -160,7 +160,7 @@ int32_t MmuP_map(uintptr_t vaddr, uintptr_t paddr, uint32_t size, MmuP_MapAttrs
  * \brief Initialize MMU sub-system, called by SysConfig, not to be called by end users
  *
  */
-void MmuP_init();
+void MmuP_init(void);
 
 /** @} */