diff --git a/source/drivers/udma/include/udma_types.h b/source/drivers/udma/include/udma_types.h
index 2e4de6338e..68c0341112 100755
--- a/source/drivers/udma/include/udma_types.h
+++ b/source/drivers/udma/include/udma_types.h
@@ -1,5 +1,5 @@
 /*
- *  Copyright (C) 2018-2021 Texas Instruments Incorporated
+ *  Copyright (C) 2018-2023 Texas Instruments Incorporated
  *
  *  Redistribution and use in source and binary forms, with or without
  *  modification, are permitted provided that the following conditions
@@ -76,7 +76,7 @@ typedef void *                          Udma_FlowHandle;
 #define UDMA_CACHELINE_ALIGNMENT        (128U)
 
 /** \brief Macro to align the size in bytes to UDMA cache line alignment */
-#define UDMA_ALIGN_SIZE(x)              (((x) + UDMA_CACHELINE_ALIGNMENT) & ~(UDMA_CACHELINE_ALIGNMENT - 1U))
+#define UDMA_ALIGN_SIZE(x)              (((x) + UDMA_CACHELINE_ALIGNMENT - 1U) & ~(UDMA_CACHELINE_ALIGNMENT - 1U))
 
 /** \brief Default UDMA channel disable timeout */
 #define UDMA_DEFAULT_CH_DISABLE_TIMEOUT (100U)
diff --git a/source/drivers/udma/include/udma_utils.h b/source/drivers/udma/include/udma_utils.h
index 81aa2f9a05..0be9d4f30f 100755
--- a/source/drivers/udma/include/udma_utils.h
+++ b/source/drivers/udma/include/udma_utils.h
@@ -190,6 +190,25 @@ static inline uint32_t UdmaUtils_getTrpdTr15Response(const uint8_t *trpdMem,
 static inline CSL_UdmapTR15 *UdmaUtils_getTrpdTr15Pointer(uint8_t *trpdMem,
                                                           uint32_t trIndex);
 
+/**
+ *  \brief Map L2G event for BCDMA trigger
+ *
+ *  \param drvHandle    [IN] UDMA driver handle - static memory needs to
+ *                           allocated by caller. This is used by the driver to
+ *                           maintain the driver states.
+ *                           This cannot be NULL.
+ *  \param chHandle     [IN] UDMA channel handle.
+ *                           This parameter can't be NULL.
+ *  \param localeventID [IN] Local event ID for the corresponding IP.
+ *
+ *  \param eventMode    [IN] Edge triggering signal or pulsed signal.
+ *
+ *
+ *  \return SYSTEMP_SUCESS OR SYSTEMP_FAILURE.
+ */
+int32_t UdmaUtils_mapLocaltoGlobalEvent(Udma_DrvHandle drvHandle, Udma_ChHandle chHandle,
+                                        uint32_t localeventID, uint32_t eventMode);
+
 /* ========================================================================== */
 /*                       Static Function Definitions                          */
 /* ========================================================================== */
diff --git a/source/drivers/udma/udma_utils.c b/source/drivers/udma/udma_utils.c
index 5b31c3d924..5c988d3bcc 100755
--- a/source/drivers/udma/udma_utils.c
+++ b/source/drivers/udma/udma_utils.c
@@ -263,3 +263,25 @@ void *Udma_defaultPhyToVirtFxn(uint64_t phyAddr,
 
     return ((void *) temp);
 }
+
+int32_t UdmaUtils_mapLocaltoGlobalEvent(Udma_DrvHandle drvHandle, Udma_ChHandle chHandle, uint32_t localeventID, uint32_t eventMode)
+{
+    int32_t status = SystemP_SUCCESS;
+
+    if(drvHandle != NULL && chHandle != NULL)
+    {
+        /*Map l2g event for DMA*/
+        Udma_ChObjectInt    *chHandleInt = (Udma_ChObjectInt*)chHandle;
+        Udma_DrvObjectInt   *drvHandleInt = (Udma_DrvObjectInt*)drvHandle;
+        CSL_intaggrMapEventToLocalEvent(&drvHandleInt->iaRegs,
+                                        CSL_DMSS_GEM_BCDMA_TRIGGER_OFFSET + chHandleInt->txChNum * 2 ,
+                                        localeventID ,eventMode);
+
+    }
+    else
+    {
+        status = SystemP_FAILURE;
+    }
+
+    return status;
+}