diff --git a/source/drivers/ecap/v0/ecap.c b/source/drivers/ecap/v0/ecap.c
index 9b328c3682..06803956e8 100644
--- a/source/drivers/ecap/v0/ecap.c
+++ b/source/drivers/ecap/v0/ecap.c
@@ -1,5 +1,5 @@
 /*
- * Copyright (C) 2021 Texas Instruments Incorporated
+ * Copyright (C) 2021-2023 Texas Instruments Incorporated
  *
  * Redistribution and use in source and binary forms, with or without
  * modification, are permitted provided that the following conditions
@@ -160,7 +160,7 @@ void ECAP_captureEvtCntrRstConfig(uint32_t baseAddr, uint32_t counterRst1,
     HW_WR_REG16(temp_addr, value);
 }
 
-void ECAP_continousModeConfig(uint32_t baseAddr)
+void ECAP_continuousModeConfig(uint32_t baseAddr)
 {
     uint32_t temp_addr = baseAddr + ECAP_ECCTL2;
     uint16_t value = HW_RD_REG16(temp_addr);
diff --git a/source/drivers/ecap/v0/ecap.h b/source/drivers/ecap/v0/ecap.h
index 744b7379cd..74a80a6dc1 100644
--- a/source/drivers/ecap/v0/ecap.h
+++ b/source/drivers/ecap/v0/ecap.h
@@ -1,5 +1,5 @@
 /*
- * Copyright (C) 2021 Texas Instruments Incorporated
+ * Copyright (C) 2021-2023 Texas Instruments Incorporated
  *
  * Redistribution and use in source and binary forms, with or without
  * modification, are permitted provided that the following conditions
@@ -336,7 +336,7 @@ void ECAP_captureEvtCntrRstConfig(uint32_t baseAddr, uint32_t counterRst1,
  *
  * \param   baseAddr   It is the Memory address of the ECAP instance used.
  */
-void ECAP_continousModeConfig(uint32_t baseAddr);
+void ECAP_continuousModeConfig(uint32_t baseAddr);
 
 /**
  * \brief   This function configures ECAP to One-shot mode and also
diff --git a/source/drivers/ecap/v1/ecap.h b/source/drivers/ecap/v1/ecap.h
index 4367669771..0d8df3bf1f 100644
--- a/source/drivers/ecap/v1/ecap.h
+++ b/source/drivers/ecap/v1/ecap.h
@@ -848,6 +848,15 @@ typedef enum
 #define ECAP_MONITORING_UNIT_2       1U
 
 //*****************************************************************************
+//
+//! Values that can be passed to ECAP_selectShadowLoadMode() as the
+//! \e loadMode parameter.
+//
+//*****************************************************************************
+//! Load on next sync event
+#define ECAP_ACTIVE_LOAD_SYNC_EVT            0U
+//! Load on EPWM GLDLCSTRB event
+#define ECAP_ACTIVE_LOAD_GLDLCSTRB_EVT       1U
 
 //*****************************************************************************
 //
@@ -1351,7 +1360,7 @@ static inline uint16_t ECAP_getInterruptSource(uint32_t base)
     //
     // Return contents of ECFLG register
     //
-    return(HW_RD_REG16(base + CSL_ECAP_ECFLG) & 0xFEU);
+    return(HW_RD_REG16(base + CSL_ECAP_ECFLG) & 0x1EFEU);
 }
 
 //*****************************************************************************
diff --git a/source/drivers/ecap/v2/ecap.c b/source/drivers/ecap/v2/ecap.c
index acef6f3936..a2c9ab3a33 100644
--- a/source/drivers/ecap/v2/ecap.c
+++ b/source/drivers/ecap/v2/ecap.c
@@ -1,5 +1,5 @@
 /*
- * Copyright (C) 2021 Texas Instruments Incorporated
+ * Copyright (C) 2021-2023 Texas Instruments Incorporated
  *
  * Redistribution and use in source and binary forms, with or without
  * modification, are permitted provided that the following conditions
@@ -160,7 +160,7 @@ void ECAP_captureEvtCntrRstConfig(uint32_t baseAddr, uint32_t counterRst1,
     HW_WR_REG32(temp_addr, value);
 }
 
-void ECAP_continousModeConfig(uint32_t baseAddr)
+void ECAP_continuousModeConfig(uint32_t baseAddr)
 {
     uint32_t temp_addr = baseAddr + CSL_ECAP_ECCTL1_ECCTL2;
     uint32_t value = HW_RD_REG32(temp_addr);
diff --git a/source/drivers/ecap/v2/ecap.h b/source/drivers/ecap/v2/ecap.h
index 322223f9cf..021e5ccb7b 100644
--- a/source/drivers/ecap/v2/ecap.h
+++ b/source/drivers/ecap/v2/ecap.h
@@ -1,5 +1,5 @@
 /*
- * Copyright (C) 2021 Texas Instruments Incorporated
+ * Copyright (C) 2021-2023 Texas Instruments Incorporated
  *
  * Redistribution and use in source and binary forms, with or without
  * modification, are permitted provided that the following conditions
@@ -339,7 +339,7 @@ void ECAP_captureEvtCntrRstConfig(uint32_t baseAddr, uint32_t counterRst1,
  *
  * \param   baseAddr   It is the Memory address of the ECAP instance used.
  */
-void ECAP_continousModeConfig(uint32_t baseAddr);
+void ECAP_continuousModeConfig(uint32_t baseAddr);
 
 /**
  * \brief   This function configures ECAP to One-shot mode and also
@@ -511,8 +511,8 @@ void ECAP_intrStatusClear(uint32_t baseAddr, uint32_t flag);
  * \param   baseAddr  It is the Memory address of the ECAP instance used.
  * \param   srcSelect Capture input select
  *                    0x0 capture input is ECAPxINPUT[0]
- *                    0x1 capture input is ECAPxINPUT[1] 
- *                    0x7F  capture input is ECAPxINPUT[127] 
+ *                    0x1 capture input is ECAPxINPUT[1]
+ *                    0x7F  capture input is ECAPxINPUT[127]
  */
 void ECAP_captureInputSourceSelect(uint32_t baseAddr, uint8_t srcSelect);