diff --git a/source/drivers/bootloader/bootloader.c b/source/drivers/bootloader/bootloader.c
index e7ef17e24e..3aa46db106 100644
--- a/source/drivers/bootloader/bootloader.c
+++ b/source/drivers/bootloader/bootloader.c
@@ -159,7 +159,7 @@ int32_t Bootloader_runCpu(Bootloader_Handle handle, Bootloader_CpuInfo *cpuInfo)
     return status;
 }
 
-int32_t Bootloader_loadSelfCpu(Bootloader_Handle handle, Bootloader_CpuInfo *cpuInfo)
+int32_t Bootloader_loadSelfCpu(Bootloader_Handle handle, Bootloader_CpuInfo *cpuInfo, uint32_t skipLoad)
 {
     int32_t status = SystemP_SUCCESS;
     uint32_t cpuId = cpuInfo->cpuId;
@@ -190,7 +190,7 @@ int32_t Bootloader_loadSelfCpu(Bootloader_Handle handle, Bootloader_CpuInfo *cpu
     {
         status = Bootloader_socMemInitCpu(cpuId);
     }
-    if(SystemP_SUCCESS == status)
+    if((SystemP_SUCCESS == status) && (skipLoad == FALSE))
     {
         if( cpuInfo->rprcOffset != BOOTLOADER_INVALID_ID)
         {
@@ -259,7 +259,7 @@ int32_t Bootloader_bootSelfCpu(Bootloader_Handle handle, Bootloader_BootImageInf
 
     while( selfCpuList[i] != BOOTLOADER_INVALID_ID)
     {
-        status = Bootloader_loadSelfCpu(handle, &bootImageInfo->cpuInfo[ selfCpuList[i] ] );
+        status = Bootloader_loadSelfCpu(handle, &bootImageInfo->cpuInfo[ selfCpuList[i] ], FALSE);
         if(status!=SystemP_SUCCESS)
         {
             break;
@@ -402,9 +402,8 @@ uint32_t Bootloader_getMsgLen(uint8_t *x509_cert_ptr, uint32_t x509_cert_size)
     uint8_t *boot_seq_ptr;
     uint32_t msg_len = 0, boot_seq_len;
     uint8_t *msg_len_ptr = (uint8_t *)&msg_len;
-    /* oid encoding of image_integrity extension - 1.3.6.1.4.1.294.1.22 */
-    uint8_t boot_seq_oid[] = {0x06, 0x09, 0x2B, 0x06, 0x01, 0x04, 0x01, 0x82, 0x26, 0x01, 0x22};
-
+    uint8_t boot_seq_oid[11];
+    Bootloader_socGetBootSeqOid(boot_seq_oid);
     boot_seq_ptr = Bootloader_findSeq(x509_cert_ptr, x509_cert_size, boot_seq_oid, sizeof(boot_seq_oid));
 
     /* length of seq is stored in the byte after the 0x30 seq_id */
@@ -522,7 +521,7 @@ int32_t Bootloader_verifyMulticoreImage(Bootloader_Handle handle)
         else if(config->bootMedia == BOOTLOADER_MEDIA_FLASH)
         {
             Bootloader_FlashArgs *flashArgs = (Bootloader_FlashArgs *)(config->args);
-            certLoadAddr = flashArgs->appImageOffset + 0x60000000;
+            certLoadAddr = flashArgs->appImageOffset + SOC_getFlashDataBaseAddr();
         }
 #ifdef DRV_VERSION_MMCSD_V0
         else if(config->bootMedia == BOOTLOADER_MEDIA_EMMC)
@@ -571,9 +570,9 @@ int32_t Bootloader_verifyMulticoreImage(Bootloader_Handle handle)
         {
             if(config->disableAppImageAuth == TRUE)
             {
-                /* NOTE: This is an option to skip image authentication in a signed 
-                image to aid initial development on HS devices. If the user has 
-                opted to disable image authentication, do not authenticate/decrypt. 
+                /* NOTE: This is an option to skip image authentication in a signed
+                image to aid initial development on HS devices. If the user has
+                opted to disable image authentication, do not authenticate/decrypt.
                 Skip the certificate length and start loading as in GP */
                 authStatus = SystemP_SUCCESS;
             }
@@ -581,9 +580,13 @@ int32_t Bootloader_verifyMulticoreImage(Bootloader_Handle handle)
             {
                 authStatus = Bootloader_socAuthImage(certLoadAddr);
             }
+
+            /* Invalidate the cache before reading in case HSM decrypted image */
+            CacheP_inv((void *)certLoadAddr, cacheAlignedLen, CacheP_TYPE_ALL);
+
             if(config->bootMedia == BOOTLOADER_MEDIA_BUFIO)
             {
-                /* Authentication will fail in Buf Io because we don't have full data yet, 
+                /* Authentication will fail in Buf Io because we don't have full data yet,
                 so make it pass here for testing. Default behaviour is to assert. */
 
                 /* authStatus = SystemP_SUCCESS; */
@@ -826,7 +829,7 @@ int32_t Bootloader_parseAndLoadLinuxAppImage(Bootloader_Handle handle, Bootloade
         }
         else
         {
-            status = SystemP_SUCCESS;
+            status = SystemP_FAILURE;
         }
     }
 
diff --git a/source/drivers/bootloader/soc/am263x/bootloader_hsmRt_load.c b/source/drivers/bootloader/soc/am263x/bootloader_hsmRt_load.c
index c115c3a6ff..5a26fae84f 100644
--- a/source/drivers/bootloader/soc/am263x/bootloader_hsmRt_load.c
+++ b/source/drivers/bootloader/soc/am263x/bootloader_hsmRt_load.c
@@ -60,7 +60,7 @@
 /* ========================================================================== */
 
 
-CSL_top_ctrlRegs * ptrTopCtrlRegs = (CSL_top_ctrlRegs *)CSL_TOP_CTRL_U_BASE;
+extern CSL_top_ctrlRegs * ptrTopCtrlRegs;
 
 /* ========================================================================== */
 /*                             Function Definitions                           */
diff --git a/source/drivers/bootloader/soc/am263x/bootloader_soc.c b/source/drivers/bootloader/soc/am263x/bootloader_soc.c
index cd7ffeed2f..6c49cc74f4 100644
--- a/source/drivers/bootloader/soc/am263x/bootloader_soc.c
+++ b/source/drivers/bootloader/soc/am263x/bootloader_soc.c
@@ -1,5 +1,5 @@
 /*
- *  Copyright (C) 2021 Texas Instruments Incorporated
+ *  Copyright (C) 2021-2023 Texas Instruments Incorporated
  *
  *  Redistribution and use in source and binary forms, with or without
  *  modification, are permitted provided that the following conditions
@@ -37,6 +37,9 @@
 #include <kernel/dpl/CacheP.h>
 #include <kernel/dpl/HwiP.h>
 
+#define BOOTLOADER_SOC_APP_CERT_SIZE (0x1000)
+#define BOOTLOADER_R5SS_FREQ_200MHz (1U)
+
 Bootloader_resMemSections gResMemSection =
 {
     .numSections    = 1,
@@ -147,6 +150,8 @@ Bootloader_CoreAddrTranslateInfo gAddrTranslateInfo[] =
     },
 };
 
+CSL_top_ctrlRegs * ptrTopCtrlRegs = (CSL_top_ctrlRegs *)CSL_TOP_CTRL_U_BASE;
+
 volatile uint32_t gR5ss0MemInitDone = FALSE, gR5ss1MemInitDone = FALSE, gR5ss1PORDone = FALSE;
 volatile uint32_t gR5ss0Core1ImagePresent = FALSE, gR5ss1Core1ImagePresent = FALSE;
 
@@ -430,9 +435,10 @@ uint32_t Bootloader_socTranslateSectionAddr(uint32_t cslCoreId, uint32_t addr)
 void Bootloader_socConfigurePll(void)
 {
     SOC_RcmPllHsDivOutConfig hsDivCfg;
+    uint32_t r5ClkSrc_restore;
 
     /* Pre Requisite Sequence to relock core pll needs to be done */
-    SOC_rcmCoreApllRelockPreRequisite();
+    r5ClkSrc_restore = SOC_rcmCoreApllRelockPreRequisite();
 
     hsDivCfg.hsdivOutEnMask = (RCM_PLL_HSDIV_OUTPUT_ENABLE_0 |
                               RCM_PLL_HSDIV_OUTPUT_ENABLE_1 |
@@ -447,6 +453,9 @@ void Bootloader_socConfigurePll(void)
     hsDivCfg.hsDivOutFreqHz[0] = SOC_RCM_FREQ_MHZ2HZ(160U);
     hsDivCfg.hsDivOutFreqHz[1] = SOC_RCM_FREQ_MHZ2HZ(192U);
     SOC_rcmPerApllConfig(RCM_PLL_FOUT_FREQID_CLK_1920MHZ, &hsDivCfg);
+
+    /* Restore R5F source clock*/
+    SOC_rcmSetR5ClockSource(r5ClkSrc_restore);
 }
 
 void Bootloader_socInitL2MailBoxMemory(void)
@@ -462,10 +471,52 @@ Bootloader_resMemSections* Bootloader_socGetSBLMem(void)
 
 int32_t Bootloader_socAuthImage(uint32_t certLoadAddr)
 {
-    return SystemP_SUCCESS;
+    int32_t status = SystemP_FAILURE;
+    HsmClient_t client ;
+    status = HsmClient_register(&client, BOOTLOADER_CLIENT_ID);
+
+    /* Request TIFS-MCU to authenticate (and decrypt if mentioned in the x509 cert) the image */
+    status = HsmClient_procAuthBoot(&client, (uint8_t *)certLoadAddr, BOOTLOADER_SOC_APP_CERT_SIZE, SystemP_WAIT_FOREVER);
+
+    return status;
 }
 
 uint32_t Bootloader_socIsAuthRequired(void)
 {
-    return FALSE;
+    uint32_t isAuthRequired = TRUE;
+
+    if(ptrTopCtrlRegs->EFUSE_DEVICE_TYPE == BOOTLOADER_DEVTYPE_HSSE)
+    {
+        isAuthRequired = TRUE;
+    }
+    else
+    {
+        isAuthRequired = FALSE;
+    }
+
+    return isAuthRequired;
+}
+
+void Bootloader_socGetBootSeqOid(uint8_t* boot_seq_oid){
+    uint8_t boot_seq[] = {0x06, 0x09, 0x2B, 0x06, 0x01, 0x04, 0x01, 0x82, 0x26, 0x01, 0x01};
+    memcpy(boot_seq_oid, boot_seq, sizeof(boot_seq));
 }
+
+void Bootloader_socSetAutoClock()
+{
+    if (((ptrTopCtrlRegs->EFUSE1_ROW_12) & CSL_TOP_CTRL_EFUSE1_ROW_12_R5SS_FREQ_MASK) == BOOTLOADER_R5SS_FREQ_200MHz)
+    {
+
+        uint32_t cpuFreq = 200 * 1000000, sysClkFreq = 200 * 1000000;
+        uint32_t testCpuFreq;
+
+        SOC_rcmsetR5SysClock(cpuFreq, sysClkFreq, CSL_CORE_ID_R5FSS0_0);
+        testCpuFreq = SOC_rcmGetR5Clock(CSL_CORE_ID_R5FSS0_0);
+
+        DebugP_assert(testCpuFreq == 200 * 1000000);
+    }
+    else
+    {
+        Bootloader_socCpuSetClock(CSL_CORE_ID_R5FSS0_0, (uint32_t)(400*1000000));
+    }
+}
\ No newline at end of file
diff --git a/source/drivers/bootloader/soc/am263x/bootloader_soc.h b/source/drivers/bootloader/soc/am263x/bootloader_soc.h
index e6c93d0324..fb039264fe 100644
--- a/source/drivers/bootloader/soc/am263x/bootloader_soc.h
+++ b/source/drivers/bootloader/soc/am263x/bootloader_soc.h
@@ -1,5 +1,5 @@
 /*
- *  Copyright (C) 2021 Texas Instruments Incorporated
+ *  Copyright (C) 2021-2023 Texas Instruments Incorporated
  *
  *  Redistribution and use in source and binary forms, with or without
  *  modification, are permitted provided that the following conditions
@@ -40,6 +40,7 @@ extern "C"
 
 
 #include <drivers/hw_include/cslr_soc.h>
+#include <drivers/hsmclient.h>
 /* ========================================================================== */
 /*                           Macros & Typedefs                                */
 /* ========================================================================== */
@@ -55,6 +56,8 @@ extern "C"
 #define BOOTLOADER_DEVTYPE_HSFS         (0xAAU)
 /** \brief device type GP   */
 #define BOOTLOADER_DEVTYPE_GP           (0x03U)
+/** \brief hsmclient ID for bootloader */
+#define BOOTLOADER_CLIENT_ID            (0x02)
 /** @} */
 /**
  * \brief Data structure containing information about a core specific to the SOC
@@ -271,11 +274,23 @@ int32_t Bootloader_socAuthImage(uint32_t certLoadAddr);
  */
 uint32_t Bootloader_socIsAuthRequired(void);
 
+/**
+ * \brief API to get boot sequence oid
+ *
+ * \param boot_seq_oid [in] pointer to integer array for populating boot sequence oid
+ *
+ */
+void Bootloader_socGetBootSeqOid(uint8_t* boot_seq_oid);
+
 /**
  * \brief API to load hsm runtime firmware
  */
 void Bootloader_socLoadHsmRtFw(const uint8_t *HsmRtFw, uint32_t hsmRTSize);
 
+/**
+ * \brief API to set CPU clock to 200 MHz or 400 MHz on the basis of eFUSE bits configuration
+ */
+void Bootloader_socSetAutoClock();
 #ifdef __cplusplus
 }
 #endif
diff --git a/source/drivers/bootloader/soc/am273x/bootloader_hsmRt_load.c b/source/drivers/bootloader/soc/am273x/bootloader_hsmRt_load.c
index bb07109778..31ec1c538f 100644
--- a/source/drivers/bootloader/soc/am273x/bootloader_hsmRt_load.c
+++ b/source/drivers/bootloader/soc/am273x/bootloader_hsmRt_load.c
@@ -60,7 +60,7 @@
 /* ========================================================================== */
 
 
-CSL_top_ctrlRegs * ptrTopCtrlRegs = (CSL_top_ctrlRegs *)CSL_TOP_CTRL_U_BASE;
+extern CSL_top_ctrlRegs * ptrTopCtrlRegs;
 
 /* ========================================================================== */
 /*                             Function Definitions                           */
diff --git a/source/drivers/bootloader/soc/am273x/bootloader_soc.c b/source/drivers/bootloader/soc/am273x/bootloader_soc.c
index b4c5367372..062a1f00a2 100644
--- a/source/drivers/bootloader/soc/am273x/bootloader_soc.c
+++ b/source/drivers/bootloader/soc/am273x/bootloader_soc.c
@@ -1,5 +1,5 @@
 /*
- *  Copyright (C) 2021 Texas Instruments Incorporated
+ *  Copyright (C) 2021-2023 Texas Instruments Incorporated
  *
  *  Redistribution and use in source and binary forms, with or without
  *  modification, are permitted provided that the following conditions
@@ -40,6 +40,8 @@
 #define BOOTLOADER_SOC_RSV_MEM_START (0x10200000)
 #define BOOTLOADER_SOC_RSV_MEM_END   (0x10220000)
 
+#define BOOTLOADER_SOC_APP_CERT_SIZE (0x1000)
+
 Bootloader_resMemSections gResMemSection =
 {
     .numSections    = 2,
@@ -151,6 +153,8 @@ int32_t Bootloader_socCpuSetClock(uint32_t cpuId, uint32_t cpuHz)
     return status;
 }
 
+CSL_top_ctrlRegs * ptrTopCtrlRegs = (CSL_top_ctrlRegs *)CSL_TOP_CTRL_U_BASE;
+
 int32_t Bootloader_socCpuPowerOnReset(uint32_t cpuId,void *socCoreOpMode)
 {
     int32_t status = SystemP_SUCCESS;
@@ -217,14 +221,14 @@ int32_t Bootloader_socMemInitCpu(uint32_t cpuId)
             }
             break;
         case CSL_CORE_ID_C66SS0:
-            if (gR5ss0MemInitDone == FALSE)
+            if (gDssMemInitDone == FALSE)
             {
                 SOC_rcmStartMemInitDSSL2(SOC_RCM_MEMINIT_DSSL2_MEMBANK_ALL);
                 SOC_rcmStartMemInitDSSL3(SOC_RCM_MEMINIT_DSSL3_MEMBANK_ALL);
                 SOC_rcmWaitMemInitDSSL2(SOC_RCM_MEMINIT_DSSL2_MEMBANK_ALL);
                 SOC_rcmWaitMemInitDSSL3(SOC_RCM_MEMINIT_DSSL3_MEMBANK_ALL);
                 SOC_rcmMemInitDssMailboxMemory();
-                gR5ss0MemInitDone = TRUE;
+                gDssMemInitDone = TRUE;
             }
             break;
         default:
@@ -313,10 +317,33 @@ Bootloader_resMemSections* Bootloader_socGetSBLMem(void)
 
 int32_t Bootloader_socAuthImage(uint32_t certLoadAddr)
 {
-    return SystemP_SUCCESS;
+    int32_t status = SystemP_FAILURE;
+    HsmClient_t client ;
+    status = HsmClient_register(&client, BOOTLOADER_CLIENT_ID);
+
+    /* Request TIFS-MCU to authenticate (and decrypt if mentioned in the x509 cert) the image */
+    status = HsmClient_procAuthBoot(&client, (uint8_t *)certLoadAddr, BOOTLOADER_SOC_APP_CERT_SIZE, SystemP_WAIT_FOREVER);
+
+    return status;
 }
 
 uint32_t Bootloader_socIsAuthRequired(void)
 {
-    return FALSE;
+    uint32_t isAuthRequired = TRUE;
+
+    if(ptrTopCtrlRegs->EFUSE_DEVICE_TYPE == BOOTLOADER_DEVTYPE_HSSE)
+    {
+        isAuthRequired = TRUE;
+    }
+    else
+    {
+        isAuthRequired = FALSE;
+    }
+
+    return isAuthRequired;
+}
+
+void Bootloader_socGetBootSeqOid(uint8_t* boot_seq_oid){
+    uint8_t boot_seq[] = {0x06, 0x09, 0x2B, 0x06, 0x01, 0x04, 0x01, 0x82, 0x26, 0x01, 0x01};
+    memcpy(boot_seq_oid, boot_seq, sizeof(boot_seq));
 }
diff --git a/source/drivers/bootloader/soc/am273x/bootloader_soc.h b/source/drivers/bootloader/soc/am273x/bootloader_soc.h
index af5c1baeaa..4cf44feb3d 100644
--- a/source/drivers/bootloader/soc/am273x/bootloader_soc.h
+++ b/source/drivers/bootloader/soc/am273x/bootloader_soc.h
@@ -1,5 +1,5 @@
 /*
- *  Copyright (C) 2021 Texas Instruments Incorporated
+ *  Copyright (C) 2021-2023 Texas Instruments Incorporated
  *
  *  Redistribution and use in source and binary forms, with or without
  *  modification, are permitted provided that the following conditions
@@ -40,6 +40,7 @@ extern "C"
 
 
 #include <drivers/hw_include/cslr_soc.h>
+#include <drivers/hsmclient.h>
 /* ========================================================================== */
 /*                           Macros & Typedefs                                */
 /* ========================================================================== */
@@ -55,6 +56,8 @@ extern "C"
 #define BOOTLOADER_DEVTYPE_HSFS         (0xAAU)
 /** \brief device type GP   */
 #define BOOTLOADER_DEVTYPE_GP           (0x03U)
+/** \brief hsmclient ID for bootloader */
+#define BOOTLOADER_CLIENT_ID            (0x02)
 /** @} */
 /**
  * \brief Data structure containing information about a core specific to the AM273x SOC
@@ -264,6 +267,14 @@ uint32_t Bootloader_socIsAuthRequired(void);
  */
 void Bootloader_socLoadHsmRtFw(const uint8_t *HsmRtFw, uint32_t hsmRTSize);
 
+/**
+ * \brief API to get boot sequence oid
+ *
+ * \param boot_seq_oid [in] pointer to integer array for populating boot sequence oid
+ *
+ */
+void Bootloader_socGetBootSeqOid(uint8_t* boot_seq_oid);
+
 #ifdef __cplusplus
 }
 #endif
diff --git a/source/drivers/bootloader/soc/am64x_am243x/bootloader_soc.c b/source/drivers/bootloader/soc/am64x_am243x/bootloader_soc.c
index a6f38f03ba..5c032b48c0 100644
--- a/source/drivers/bootloader/soc/am64x_am243x/bootloader_soc.c
+++ b/source/drivers/bootloader/soc/am64x_am243x/bootloader_soc.c
@@ -1,5 +1,5 @@
 /*
- *  Copyright (C) 2021-2022 Texas Instruments Incorporated
+ *  Copyright (C) 2021-2023 Texas Instruments Incorporated
  *
  *  Redistribution and use in source and binary forms, with or without
  *  modification, are permitted provided that the following conditions
@@ -927,7 +927,7 @@ int32_t Bootloader_socCpuResetReleaseSelf(void)
         bDualSelfR5F = TRUE;
     }
 
-    
+
     if(bDualSelfR5F == TRUE)
     {
         sciclientCpuProcIdCore1 = Bootloader_socGetSciclientCpuProcId(CSL_CORE_ID_R5FSS0_1);
@@ -1319,3 +1319,8 @@ void Bootloader_socNotifyFirewallOpen(void)
 
     CSL_REG32_WR(psramPtr, SOC_FWL_OPEN_MAGIC_NUM);
 }
+
+void Bootloader_socGetBootSeqOid(uint8_t* boot_seq_oid){
+    uint8_t boot_seq[] = {0x06, 0x09, 0x2B, 0x06, 0x01, 0x04, 0x01, 0x82, 0x26, 0x01, 0x22};
+    memcpy(boot_seq_oid, boot_seq, sizeof(boot_seq));
+}
\ No newline at end of file
diff --git a/source/drivers/bootloader/soc/am64x_am243x/bootloader_soc.h b/source/drivers/bootloader/soc/am64x_am243x/bootloader_soc.h
index ccf39e3ae2..68c2f7576e 100644
--- a/source/drivers/bootloader/soc/am64x_am243x/bootloader_soc.h
+++ b/source/drivers/bootloader/soc/am64x_am243x/bootloader_soc.h
@@ -1,5 +1,5 @@
 /*
- *  Copyright (C) 2021-2022 Texas Instruments Incorporated
+ *  Copyright (C) 2021-2023 Texas Instruments Incorporated
  *
  *  Redistribution and use in source and binary forms, with or without
  *  modification, are permitted provided that the following conditions
@@ -282,8 +282,8 @@ uint32_t Bootloader_socIsR5FSSDual(uint32_t ssNum);
  * \brief API to check the GPN variant of the SOC - whether it's a quad core,
  * dual core or a single core variant
  *
- * \return \ref BOOTLOADER_DEVICE_VARIANT_SINGLE_CORE, 
- *         \ref BOOTLOADER_DEVICE_VARIANT_DUAL_CORE or 
+ * \return \ref BOOTLOADER_DEVICE_VARIANT_SINGLE_CORE,
+ *         \ref BOOTLOADER_DEVICE_VARIANT_DUAL_CORE or
  *         \ref BOOTLOADER_DEVICE_VARIANT_QUAD_CORE or
  *          0xFFFFFFFF if invalid bit field read
  */
@@ -319,6 +319,14 @@ uint32_t Bootloader_socIsMCUResetIsoEnabled(void);
  */
 void Bootloader_socNotifyFirewallOpen(void);
 
+/**
+ * \brief API to get boot sequence oid
+ *
+ * \param boot_seq_oid [in] pointer to integer array for populating boot sequence oid
+ *
+ */
+void Bootloader_socGetBootSeqOid(uint8_t* boot_seq_oid);
+
 #ifdef __cplusplus
 }
 #endif
diff --git a/source/drivers/bootloader/soc/awr294x/bootloader_hsmRt_load.c b/source/drivers/bootloader/soc/awr294x/bootloader_hsmRt_load.c
new file mode 100644
index 0000000000..df3c1bf5a2
--- /dev/null
+++ b/source/drivers/bootloader/soc/awr294x/bootloader_hsmRt_load.c
@@ -0,0 +1,97 @@
+/*
+ *  Copyright (C) 2022-2023 Texas Instruments Incorporated
+ *
+ *  Redistribution and use in source and binary forms, with or without
+ *  modification, are permitted provided that the following conditions
+ *  are met:
+ *
+ *    Redistributions of source code must retain the above copyright
+ *    notice, this list of conditions and the following disclaimer.
+ *
+ *    Redistributions in binary form must reproduce the above copyright
+ *    notice, this list of conditions and the following disclaimer in the
+ *    documentation and/or other materials provided with the
+ *    distribution.
+ *
+ *    Neither the name of Texas Instruments Incorporated nor the names of
+ *    its contributors may be used to endorse or promote products derived
+ *    from this software without specific prior written permission.
+ *
+ *  THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS
+ *  "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT
+ *  LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR
+ *  A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT
+ *  OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL,
+ *  SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT
+ *  LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE,
+ *  DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY
+ *  THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT
+ *  (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE
+ *  OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
+ *
+ */
+
+/**
+ *  \file bootloader_hsmRt_load.c
+ *
+ *  \brief Implementation of hsm runtime boot test for CCS initialization
+ *
+ */
+
+/* ========================================================================== */
+/*                             Include Files                                  */
+/* ========================================================================== */
+
+#include <stdint.h>
+#include <string.h>
+#include <stdio.h>
+#include <drivers/bootloader/soc/bootloader_soc.h>
+#include <kernel/dpl/SystemP.h>
+#include <kernel/nortos/dpl/r5/HwiP_armv7r_vim.h>
+#include <drivers/hsmclient.h>
+#include <kernel/dpl/DebugP.h>
+#include <drivers/hw_include/cslr_soc.h>
+/* ========================================================================== */
+/*                           Macros & Typedefs                                */
+/* ========================================================================== */
+
+/* ========================================================================== */
+/*                            Global Variables                                */
+/* ========================================================================== */
+
+
+extern CSL_top_ctrlRegs * ptrTopCtrlRegs;
+
+/* ========================================================================== */
+/*                             Function Definitions                           */
+/* ========================================================================== */
+
+void Bootloader_socLoadHsmRtFw(const uint8_t *HsmRtFw, uint32_t hsmRTSize)
+{
+    int32_t retVal = SystemP_SUCCESS;
+
+    /* Load hsmRt firmware only when device is HSSE */
+    if(ptrTopCtrlRegs->EFUSE_DEVICE_TYPE == BOOTLOADER_DEVTYPE_HSSE)
+    {
+        DebugP_logInfo("DevType : HSSE  \r\n");
+        retVal = Hsmclient_loadHSMRtFirmware((uint8_t*)HsmRtFw);
+        DebugP_logInfo("HSMRT Size in Bytes : %ld \r\n", (uint32_t)hsmRTSize);
+        if(retVal == SystemP_SUCCESS)
+        {
+            DebugP_logInfo("hsm runtime firmware load complete ... \r\n");
+        }
+        else
+        {
+            DebugP_logInfo("hsm runtime firmware load failure ... \r\n");
+        }
+    }
+    else if(ptrTopCtrlRegs->EFUSE_DEVICE_TYPE == BOOTLOADER_DEVTYPE_HSFS)
+    {
+        DebugP_logInfo("Device Type : HSFS  \r\n");
+    }
+    else
+    {
+        /* None */
+    }
+    DebugP_assertNoLog(retVal==SystemP_SUCCESS);
+}
diff --git a/source/drivers/bootloader/soc/awr294x/bootloader_soc.c b/source/drivers/bootloader/soc/awr294x/bootloader_soc.c
index 3a36684941..0a7e96d1f6 100644
--- a/source/drivers/bootloader/soc/awr294x/bootloader_soc.c
+++ b/source/drivers/bootloader/soc/awr294x/bootloader_soc.c
@@ -1,5 +1,5 @@
 /*
- *  Copyright (C) 2021-23 Texas Instruments Incorporated
+ *  Copyright (C) 2021-2023 Texas Instruments Incorporated
  *
  *  Redistribution and use in source and binary forms, with or without
  *  modification, are permitted provided that the following conditions
@@ -39,6 +39,7 @@
 
 #define CSL_MSS_TOP_PBIST_RINFOL_OFFSET    (0x000000C8U)
 #define CSL_MSS_TOP_PBIST_RINFOU_OFFSET    (0x000000CCU)
+#define BOOTLOADER_SOC_APP_CERT_SIZE (0x1000)
 
 Bootloader_resMemSections gResMemSection =
 {
@@ -154,6 +155,7 @@ int32_t Bootloader_socCpuSetClock(uint32_t cpuId, uint32_t cpuHz)
     }
     return SystemP_SUCCESS;
 }
+CSL_top_ctrlRegs * ptrTopCtrlRegs = (CSL_top_ctrlRegs *)CSL_TOP_CTRL_U_BASE;
 
 int32_t Bootloader_socCpuPowerOnReset(uint32_t cpuId,void *socCoreOpMode)
 {
@@ -415,10 +417,33 @@ Bootloader_resMemSections* Bootloader_socGetSBLMem(void)
 
 int32_t Bootloader_socAuthImage(uint32_t certLoadAddr)
 {
-    return SystemP_SUCCESS;
+    int32_t status = SystemP_FAILURE;
+    HsmClient_t client ;
+    status = HsmClient_register(&client, BOOTLOADER_CLIENT_ID);
+
+    /* Request TIFS-MCU to authenticate (and decrypt if mentioned in the x509 cert) the image */
+    status = HsmClient_procAuthBoot(&client, (uint8_t *)certLoadAddr, BOOTLOADER_SOC_APP_CERT_SIZE, SystemP_WAIT_FOREVER);
+
+    return status;
 }
 
 uint32_t Bootloader_socIsAuthRequired(void)
 {
-    return FALSE;
+    uint32_t isAuthRequired = TRUE;
+
+    if(ptrTopCtrlRegs->EFUSE_DEVICE_TYPE == BOOTLOADER_DEVTYPE_HSSE)
+    {
+        isAuthRequired = TRUE;
+    }
+    else
+    {
+        isAuthRequired = FALSE;
+    }
+
+    return isAuthRequired;
+}
+
+void Bootloader_socGetBootSeqOid(uint8_t* boot_seq_oid){
+    uint8_t boot_seq[] = {0x06, 0x09, 0x2B, 0x06, 0x01, 0x04, 0x01, 0x82, 0x26, 0x01, 0x01};
+    memcpy(boot_seq_oid, boot_seq, sizeof(boot_seq));
 }
diff --git a/source/drivers/bootloader/soc/awr294x/bootloader_soc.h b/source/drivers/bootloader/soc/awr294x/bootloader_soc.h
index 6d08ba10f3..0bf4ced951 100644
--- a/source/drivers/bootloader/soc/awr294x/bootloader_soc.h
+++ b/source/drivers/bootloader/soc/awr294x/bootloader_soc.h
@@ -1,5 +1,5 @@
 /*
- *  Copyright (C) 2021 Texas Instruments Incorporated
+ *  Copyright (C) 2021-2023 Texas Instruments Incorporated
  *
  *  Redistribution and use in source and binary forms, with or without
  *  modification, are permitted provided that the following conditions
@@ -30,8 +30,8 @@
  *  OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
  */
 
-#ifndef BOOTLOADER_SOC_AM273X_H_
-#define BOOTLOADER_SOC_AM273X_H_
+#ifndef BOOTLOADER_SOC_AWR294X_H_
+#define BOOTLOADER_SOC_AWR294X_H_
 
 #ifdef __cplusplus
 extern "C"
@@ -40,9 +40,27 @@ extern "C"
 
 
 #include <drivers/hw_include/cslr_soc.h>
+#include <drivers/hsmclient.h>
+/* ========================================================================== */
+/*                           Macros & Typedefs                                */
+/* ========================================================================== */
 
 /**
- * \brief Data structure containing information about a core specific to the AM64x SOC
+ *  \anchor DevTypes
+ *  \name Device Types
+ *  @{
+ */
+/** \brief device type HSSE */
+#define BOOTLOADER_DEVTYPE_HSSE         (0x0AU)
+/** \brief device type HSFS */
+#define BOOTLOADER_DEVTYPE_HSFS         (0xAAU)
+/** \brief device type GP   */
+#define BOOTLOADER_DEVTYPE_GP           (0x03U)
+/** \brief hsmclient ID for bootloader */
+#define BOOTLOADER_CLIENT_ID            (0x02)
+/** @} */
+/**
+ * \brief Data structure containing information about a core specific to the AWR294x SOC
  *
  * This structure is used to store the data about cores in the SoC in the form of a lookup table which will be
  * used by various APIs.
@@ -233,6 +251,18 @@ int32_t Bootloader_socAuthImage(uint32_t certLoadAddr);
  */
 uint32_t Bootloader_socIsAuthRequired(void);
 
+/**
+ * \brief API to load hsm runtime firmware
+ */
+void Bootloader_socLoadHsmRtFw(const uint8_t *HsmRtFw, uint32_t hsmRTSize);
+
+/**
+ * \brief API to get boot sequence oid
+ *
+ * \param boot_seq_oid [in] pointer to integer array for populating boot sequence oid
+ *
+ */
+void Bootloader_socGetBootSeqOid(uint8_t* boot_seq_oid);
 
 #ifdef __cplusplus
 }